Z-Stack API Reference  8.31.00.00
_zstack_secapsremovereq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t parentAddr
 Parent's Short Address.
 
uint16_t nwkAddr
 Device's NWK Address.
 
zstack_LongAddr_t extAddr
 Device's Extended IEEE Address.
 

Detailed Description

Structure to send a Security APS Remove Request.


The documentation for this struct was generated from the following file: