![]() |
![]() |
|
Z-Stack API Reference
8.31.00.00
|
#include <zstack.h>
Data Fields | |
| zstack_ZdpStatus | status |
| zstack_LongAddr_t | ieeeAddr |
| uint16_t | nwkAddr |
| uint8_t | startIndex |
| uint8_t | n_assocDevList |
| uint16_t * | pAssocDevList |
Structure to send a ZDO IEEE Address Response Indication.
| zstack_LongAddr_t ieeeAddr |
64 bit IEEE address of source device
| uint8_t n_assocDevList |
Number of associated devices in the list
| uint16_t nwkAddr |
Network address of the responding device
| uint16_t* pAssocDevList |
Array of (uint16_t) associated devices
| uint8_t startIndex |
Starting index into the list of associated devices
| zstack_ZdpStatus status |
Response status