Z-Stack API Reference  8.31.00.00
_zstack_zdonodedescreq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t dstAddr
 
uint16_t nwkAddrOfInterest
 

Detailed Description

Structure to send a ZDO Node Descriptor Request.

Field Documentation

§ dstAddr

uint16_t dstAddr

Destination address

§ nwkAddrOfInterest

uint16_t nwkAddrOfInterest

The network address of the destination device being queried.


The documentation for this struct was generated from the following file: