![]() |
![]() |
|
Z-Stack API Reference
8.31.00.00
|
Data Fields | |
| uint8_t | actions |
| Configuration command. More... | |
| uint16_t | options |
| Configuration command. More... | |
| uint32_t | gpdId |
| ID of the GPD. | |
| uint8_t | gpdIEEE [Z_EXTADDR_LEN] |
| 0b010. More... | |
| uint8_t | ep |
| is 0b010. More... | |
| uint8_t | deviceId |
| The DeviceID for GPD. | |
| uint8_t | groupEntriesCount |
| Number of groups. | |
| uint8_t * | pGroupList |
| group communication. More... | |
| uint16_t | gpdAssignedAlias |
| The commissioned alias for this GPD. | |
| uint8_t | forwardingRadius |
| To limit the range of the groupcast. | |
| uint8_t | securityOptions |
| The security options. | |
| uint32_t | gpdSecurityFrameCounter |
| The incoming security frame counter. | |
| uint8_t | gpdSecurityKey [SEC_KEY_LEN] |
| The security key for the GPD. | |
| uint8_t | numOfPairedEndpoints |
| Indicates the number of endpoints. | |
| uint8_t * | pPairedEndpoints |
| List of paired endpoints. | |
| uint8_t | appInfo |
| Application information bitfield. | |
| uint16_t | manufacturerId |
| ManufacturerID value. | |
| uint16_t | modeId |
| ModelID value. | |
| uint8_t | numberOfGpdCmd |
| of items in the GP command list field. More... | |
| uint8_t | pGpdCmdList |
| Commmand list. | |
| uint8_t * | pClusterList |
| Cluster list. | |
| uint8_t actions |
Configuration command.
Actions field of the GP Pairing
| uint8_t ep |
is 0b010.
Endpoint of the GP if application ID
| uint8_t gpdIEEE[Z_EXTADDR_LEN] |
0b010.
IEEE of the GPD if application ID is
| uint8_t numberOfGpdCmd |
of items in the GP command list field.
Number of GP commands defines the number
| uint16_t options |
Configuration command.
Options parameter of the GP Pairing
| uint8_t* pGroupList |
group communication.
The 16-bit GroupID and alias for the