|
|
uint8_t | options |
| | Options field of the GP Response command.
|
| |
| uint16_t | tempMasterShortAddr |
| | will transmit the response GPDF to the GPD. More...
|
| |
|
uint8_t | tempMasterChannel |
| | indicates the channel the Response GPDF will be sent on.
|
| |
|
uint32_t | gpdSrcId |
| | ID of the GPD.
|
| |
|
uint8_t | gpdIEEE [Z_EXTADDR_LEN] |
| | IEEE of the GPD if application ID is 0b010.
|
| |
|
uint8_t | ep |
| | Endpoint of the GP if application ID is 0b010.
|
| |
|
uint8_t | cmdId |
| | Command ID.
|
| |
|
uint8_t | payloadLen |
| | Command payload length.
|
| |
|
uint8_t * | cmdPayload |
| | Command payolad.
|
| |
§ tempMasterShortAddr
| uint16_t tempMasterShortAddr |
will transmit the response GPDF to the GPD.
indicates the address of the proxy which
The documentation for this struct was generated from the following file: