Z-Stack API Reference  8.31.00.00
zclLCStep_t Struct Reference

Data Fields

uint8_t stepMode
 LEVEL_STEP_DOWN, or LEVEL_STEP_DOWN_AND_OFF. More...
 
uint8_t amount
 number of levels to step
 
uint16_t transitionTime
 time, in 1/10ths of a second, to take to perform the step
 
uint8_t withOnOff
 with On/off command
 

Field Documentation

§ stepMode

uint8_t stepMode

LEVEL_STEP_DOWN, or LEVEL_STEP_DOWN_AND_OFF.

step mode which is either LEVEL_STEP_UP, LEVEL_STEP_ON_AND_UP,


The documentation for this struct was generated from the following file: