Z-Stack API Reference
8.31.00.00
Data Fields
zclOTA_QuerySpecificFileReqParams_t Struct Reference
ZCL OTA Cluster
»
ZCL OTA Cluster Typedefs
Data Fields
uint8_t
nodeAddr
[Z_EXTADDR_LEN]
This is the IEEE address of the client device.
zclOTA_FileID_t
fileId
File Id structure.
uint16_t
stackVersion
Stack version value.
The documentation for this struct was generated from the following file:
zcl_ota.h
zclOTA_QuerySpecificFileReqParams_t