![]() |
![]() |
|
Z-Stack API Reference
8.31.00.00
|
Data Fields | |
| uint8_t | testModeDuration |
| uint8_t | currZoneSensitivityLevel |
| uint8_t currZoneSensitivityLevel |
Specifies the sensitivity level the IAS Zone server SHALL use for the duration of the Test Mode and with which it must update its CurrentZoneSensitivityLevel attribute.
| uint8_t testModeDuration |
Specifies the duration, in seconds, for which the IAS Zone server SHALL operate in its test mode.