TI BLE-Stack for Bluetooth API Documentation  3.03.00.00
comdef.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  Group: WCS, LPC, BTS
4  $Target Device: DEVICES $
5 
6  ******************************************************************************
7  $License: BSD3 2004 $
8  ******************************************************************************
9  $Release Name: PACKAGE NAME $
10  $Release Date: PACKAGE RELEASE DATE $
11  *****************************************************************************/
12 
18 #ifndef COMDEF_H
19 #define COMDEF_H
20 
21 #ifdef __cplusplus
22 extern "C"
23 {
24 #endif
25 
26 
27 /*********************************************************************
28  * INCLUDES
29  */
30 
31 /* HAL */
32 #include "hal_types.h"
33 #include "hal_defs.h"
34 
36 
37 /*********************************************************************
38  * Lint Keywords
39  */
40 #define VOID (void)
41 
42 #define NULL_OK
43 #define INP
44 #define OUTP
45 #define UNUSED
46 #define ONLY
47 #define READONLY
48 #define SHARED
49 #define KEEP
50 #define RELAX
51 
52 /*********************************************************************
53  * CONSTANTS
54  */
55 
56 #ifndef false
57  #define false 0
58 #endif
59 
60 #ifndef true
61  #define true 1
62 #endif
63 
64 #ifndef CONST
65  #define CONST const
66 #endif
67 
68 #ifndef GENERIC
69  #define GENERIC
70 #endif
71 
73 
74 /*** Generic Status Return Values ***/
75 #define SUCCESS 0x00
76 #define FAILURE 0x01
77 #define INVALIDPARAMETER 0x02
78 #define INVALID_TASK 0x03
79 #define MSG_BUFFER_NOT_AVAIL 0x04
80 #define INVALID_MSG_POINTER 0x05
81 #define INVALID_EVENT_ID 0x06
82 #define INVALID_INTERRUPT_ID 0x07
83 #define NO_TIMER_AVAIL 0x08
84 #define NV_ITEM_UNINIT 0x09
85 #define NV_OPER_FAILED 0x0A
86 #define INVALID_MEM_SIZE 0x0B
87 #define NV_BAD_ITEM_LEN 0x0C
88 
89 /*********************************************************************
90  * TYPEDEFS
91  */
92 
94 
95 // Generic Status return
96 typedef uint8 Status_t;
97 
98 // Data types
99 typedef int32 int24;
100 typedef uint32 uint24;
101 
103 
104 /*********************************************************************
105  * Global System Events
106  */
107 
108 #define SYS_EVENT_MSG 0x8000
109 
110 /*********************************************************************
111  * Global Generic System Messages
112  */
113 
114 #define KEY_CHANGE 0xC0
115 
116 // OSAL System Message IDs/Events Reserved for applications (user applications)
117 // 0xE0 - 0xFC
118 
119 /*********************************************************************
120  * MACROS
121  */
122 
123 /*********************************************************************
124  * GLOBAL VARIABLES
125  */
126 
127 /*********************************************************************
128  * FUNCTIONS
129  */
130 
131 /*********************************************************************
132 *********************************************************************/
133 
134 #ifdef __cplusplus
135 }
136 #endif
137 
138 #endif /* COMDEF_H */
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale