TI BLE-Stack for Bluetooth API Documentation
3.03.00.00
|
HCI layer interface.
End HCI_Function_Maps
Go to the source code of this file.
Data Structures | |
union | _hciEvt_BLEConnComplete_u_ |
LE Connection Complete Event. More... | |
struct | hciDataPacket_t |
HCI Data Packet. More... | |
struct | hciEvt_AptoExpired_t |
Authenticated Payload Timeout Expired Event. More... | |
struct | hciEvt_BLEAdvPktReport_t |
LE Advertising Packet Report Event. More... | |
struct | hciEvt_BLEChanMapUpdate_t |
VS LE Channel Map Update Event. More... | |
struct | hciEvt_BLEConnComplete_t |
LE Connection Complete Event. More... | |
struct | hciEvt_BLEConnUpdateComplete_t |
LE Connection Update Complete Event. More... | |
struct | hciEvt_BLEDataLengthChange_t |
LE Data Length Change Event. More... | |
struct | hciEvt_BLEEnhConnComplete_t |
LE Enhanced Connection Complete Event. More... | |
struct | hciEvt_BLEGenDHKeyComplete_t |
LE Generate DHKey Complete Event. More... | |
struct | hciEvt_BLELTKReq_t |
LE Long Term Key Requested Event. More... | |
struct | hciEvt_BLEPhyUpdateComplete_t |
LE Phy Update Complete Event. More... | |
struct | hciEvt_BLEReadP256PublicKeyComplete_t |
LE Read P256 Public Key Complete Event. More... | |
struct | hciEvt_BLEReadRemoteFeatureComplete_t |
LE Read Remote Used Features Complete Event. More... | |
struct | hciEvt_BLERemoteConnParamReq_t |
LE Remote Connection Parameter Request Event. More... | |
struct | hciEvt_BLEScanReqReport_t |
VS LE Scan Request Report Event. More... | |
struct | hciEvt_BufferOverflow_t |
Data Buffer Overflow Event. More... | |
struct | hciEvt_CmdComplete_t |
Command Complete Event. More... | |
struct | hciEvt_CommandStatus_t |
Command Status Event. More... | |
struct | hciEvt_DevInfo_t |
LE Advertising Report Event. More... | |
struct | hciEvt_DisconnComplete_t |
Disconnection Complete Event. More... | |
struct | hciEvt_EncryptChange_t |
LE Encryption Change Event. More... | |
struct | hciEvt_HardwareError_t |
Hardware Error Event. More... | |
struct | hciEvt_NumCompletedPkt_t |
Number of Completed Packets Event. More... | |
struct | hciEvt_VSCmdComplete_t |
Vendor Specific Command Complete Event. More... | |
struct | hciPacket_t |
HCI Packet event. More... | |
struct | hciRetParam_LeReadBufSize_t |
Data structure for HCI Command Complete Event Return Parameter. More... | |
Macros | |
#define | CONTINUING_PKT LL_DATA_CONTINUATION_PKT |
Continuing Packet. | |
#define | FIRST_PKT_CTRL_TO_HOST LL_DATA_FIRST_PKT_CTRL_TO_HOST |
First Packet Controller to Host. | |
#define | FIRST_PKT_HOST_TO_CTRL LL_DATA_FIRST_PKT_HOST_TO_CTRL |
First Host to Controller Packet. | |
#define | HCI_ADV_CHAN_37 LL_ADV_CHAN_37 |
Channel 37. | |
#define | HCI_ADV_CHAN_38 LL_ADV_CHAN_38 |
Channel 38. | |
#define | HCI_ADV_CHAN_39 LL_ADV_CHAN_39 |
Channel 39. | |
#define | HCI_ADV_CHAN_ALL (LL_ADV_CHAN_37 | LL_ADV_CHAN_38 | LL_ADV_CHAN_39) |
All Channels. | |
#define | HCI_ADV_WL_POLICY_ANY_REQ LL_ADV_WL_POLICY_ANY_REQ |
Any Request. | |
#define | HCI_ADV_WL_POLICY_WL_ALL_REQ LL_ADV_WL_POLICY_WL_ALL_REQ |
All Requests. | |
#define | HCI_ADV_WL_POLICY_WL_CONNECT_REQ LL_ADV_WL_POLICY_WL_CONNECT_REQ |
Connection Requests. | |
#define | HCI_ADV_WL_POLICY_WL_SCAN_REQ LL_ADV_WL_POLICY_WL_SCAN_REQ |
Scan Requests. | |
#define | HCI_CONNECTABLE_DIRECTED_HDC_ADV LL_ADV_CONNECTABLE_DIRECTED_HDC_EVT |
Connectable Directed High Duty Cycle Advertising. | |
#define | HCI_CONNECTABLE_DIRECTED_LDC_ADV LL_ADV_CONNECTABLE_DIRECTED_LDC_EVT |
Connectable Directed Low Duty Cycle Advertising. | |
#define | HCI_CONNECTABLE_UNDIRECTED_ADV LL_ADV_CONNECTABLE_UNDIRECTED_EVT |
Connectable Undirected Advertising. | |
#define | HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_OFF_SYNCH_ON 2 |
ACL Off, Synchronous On. | |
#define | HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_OFF 1 |
ACL On, Synchronous Off. | |
#define | HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_ON 3 |
ACL On, Synchronous On. | |
#define | HCI_CTRL_TO_HOST_FLOW_CTRL_OFF 0 |
Controller to Host Flow Controll Off. | |
#define | HCI_DIRECT_TEST_PAYLOAD_0x00 LL_DIRECT_TEST_PAYLOAD_0x00 |
0x00 | |
#define | HCI_DIRECT_TEST_PAYLOAD_0x0F LL_DIRECT_TEST_PAYLOAD_0x0F |
0x0F | |
#define | HCI_DIRECT_TEST_PAYLOAD_0x55 LL_DIRECT_TEST_PAYLOAD_0x55 |
0x55 | |
#define | HCI_DIRECT_TEST_PAYLOAD_0xAA LL_DIRECT_TEST_PAYLOAD_0xAA |
0xAA | |
#define | HCI_DIRECT_TEST_PAYLOAD_0xF0 LL_DIRECT_TEST_PAYLOAD_0xF0 |
0xF0 | |
#define | HCI_DIRECT_TEST_PAYLOAD_0xFF LL_DIRECT_TEST_PAYLOAD_0xFF |
0xFF | |
#define | HCI_DIRECT_TEST_PAYLOAD_PRBS15 LL_DIRECT_TEST_PAYLOAD_PRBS15 |
PRBS15. | |
#define | HCI_DIRECT_TEST_PAYLOAD_PRBS9 LL_DIRECT_TEST_PAYLOAD_PRBS9 |
PRBS9. | |
#define | HCI_DISABLE_ADDR_RESOLUTION LL_DISABLE_ADDR_RESOLUTION |
Disable. | |
#define | HCI_DISABLE_ADV LL_ADV_MODE_OFF |
Advertising Disable. | |
#define | HCI_DISCONNECT_AUTH_FAILURE HCI_ERROR_CODE_AUTH_FAILURE |
Authentication Failure. | |
#define | HCI_DISCONNECT_KEY_PAIRING_NOT_SUPPORTED HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED |
Key Paring Not Supported. | |
#define | HCI_DISCONNECT_REMOTE_DEV_LOW_RESOURCES HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES |
Remote Device Low Resources. | |
#define | HCI_DISCONNECT_REMOTE_DEV_POWER_OFF HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF |
Remote Device Power Off. | |
#define | HCI_DISCONNECT_REMOTE_USER_TERM HCI_ERROR_CODE_REMOTE_USER_TERM_CONN |
Remote User Terminated. | |
#define | HCI_DISCONNECT_UNACCEPTABLE_CONN_INTERVAL HCI_ERROR_CODE_UNACCEPTABLE_CONN_INTERVAL |
Unnaceptable Connection Interval. | |
#define | HCI_DISCONNECT_UNSUPPORTED_REMOTE_FEATURE HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE |
Unsupported Remote Feature. | |
#define | HCI_DTM_STABLE_MODULATION_INDEX LL_DTM_STABLE_MODULATION_INDEX |
Stable Modulation. | |
#define | HCI_DTM_STANDARD_MODULATION_INDEX LL_DTM_STANDARD_MODULATION_INDEX |
Standard Modulation. | |
#define | HCI_ENABLE_ADDR_RESOLUTION LL_ENABLE_ADDR_RESOLUTION |
Enable. | |
#define | HCI_ENABLE_ADV LL_ADV_MODE_ON |
Advertising Enable. | |
#define | HCI_ENCRYPTION_OFF LL_ENCRYPTION_OFF |
Off. | |
#define | HCI_ENCRYPTION_ON LL_ENCRYPTION_ON |
On. | |
#define | HCI_ERROR_CODE_ACL_CONN_ALREADY_EXISTS 0x0B |
ACL Connection Already Exists. | |
#define | HCI_ERROR_CODE_AUTH_FAILURE 0x05 |
Authentication Fialure. | |
#define | HCI_ERROR_CODE_CHAN_ASSESSMENT_NOT_SUPPORTED 0x2E |
Channel Assessment Not Supported. | |
#define | HCI_ERROR_CODE_CMD_DISALLOWED 0x0C |
Command Disallowed. | |
#define | HCI_ERROR_CODE_COARSE_CLOCK_ADJUST_REJECTED 0x40 |
Coarse Clock Adjust Rejected. | |
#define | HCI_ERROR_CODE_CONN_ACCEPT_TIMEOUT_EXCEEDED 0x10 |
Connection Acceptance Timeout Exceeded. | |
#define | HCI_ERROR_CODE_CONN_FAILED_TO_ESTABLISH 0x3E |
Connection Failued to Establish. | |
#define | HCI_ERROR_CODE_CONN_LIMIT_EXCEEDED 0x09 |
Connection Limit Exceeded. | |
#define | HCI_ERROR_CODE_CONN_REJ_LIMITED_RESOURCES 0x0D |
Connection Rejected due to Limited Resources. | |
#define | HCI_ERROR_CODE_CONN_REJ_NO_SUITABLE_CHAN_FOUND 0x39 |
Connection Rejected No Suitable Channel Found. | |
#define | HCI_ERROR_CODE_CONN_REJECTED_SECURITY_REASONS 0x0E |
Connection Rejected for Security Reasons. | |
#define | HCI_ERROR_CODE_CONN_REJECTED_UNACCEPTABLE_BDADDR 0x0F |
Connection Rejected due to Unacceptable BDADDR. | |
#define | HCI_ERROR_CODE_CONN_TERM_BY_LOCAL_HOST 0x16 |
Connection Terminated by Local Host. | |
#define | HCI_ERROR_CODE_CONN_TERM_MIC_FAILURE 0x3D |
Connection Terminated due to MIC Failure. | |
#define | HCI_ERROR_CODE_CONN_TIMEOUT 0x08 |
Connection Timeout. | |
#define | HCI_ERROR_CODE_CONTROLLER_BUSY 0x3A |
Controller Busy. | |
#define | HCI_ERROR_CODE_DIFFERENT_TRANSACTION_COLLISION 0x2A |
Different Transaction Collision. | |
#define | HCI_ERROR_CODE_DIRECTED_ADV_TIMEOUT 0x3C |
Directed Advertising Timeout. | |
#define | HCI_ERROR_CODE_ENCRYPT_MODE_NOT_ACCEPTABLE 0x25 |
Encrypt Mode not Acceptable. | |
#define | HCI_ERROR_CODE_EXTENDED_INQUIRY_RESP_TOO_LARGE 0x36 |
Extended Inquiry Response too Large. | |
#define | HCI_ERROR_CODE_HOST_BUSY_PAIRING 0x38 |
Host Busy Pairing. | |
#define | HCI_ERROR_CODE_HW_FAILURE 0x03 |
Hardware Failure. | |
#define | HCI_ERROR_CODE_INSTANT_PASSED 0x28 |
Instant Passed. | |
#define | HCI_ERROR_CODE_INSUFFICIENT_SECURITY 0x2F |
Insufficient Security. | |
#define | HCI_ERROR_CODE_INVALID_HCI_CMD_PARAMS 0x12 |
Invalid HCI Command Parameters. | |
#define | HCI_ERROR_CODE_INVALID_LMP_PARAMS 0x1E |
Invalid LMP Paramaters. | |
#define | HCI_ERROR_CODE_LINK_KEY_CAN_NOT_BE_CHANGED 0x26 |
Link Key Can Not Be Changed. | |
#define | HCI_ERROR_CODE_LMP_ERR_TRANSACTION_COLLISION 0x23 |
LMP Error Transaction Collision. | |
#define | HCI_ERROR_CODE_LMP_LL_RESP_TIMEOUT 0x22 |
LMP LL Response Timeout. | |
#define | HCI_ERROR_CODE_LMP_PDU_NOT_ALLOWED 0x24 |
LMP DU Not Allowed. | |
#define | HCI_ERROR_CODE_MAC_CONN_FAILED 0x3F |
MAC Connection Failed. | |
#define | HCI_ERROR_CODE_MEM_CAP_EXCEEDED 0x07 |
Memory Capability Exceeded. | |
#define | HCI_ERROR_CODE_PAGE_TIMEOUT 0x04 |
Page Timeout. | |
#define | HCI_ERROR_CODE_PAIRING_NOT_ALLOWED 0x18 |
Pairing Not Allowed. | |
#define | HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED 0x29 |
Pairing with Unit Key Not Supported. | |
#define | HCI_ERROR_CODE_PARAM_OUT_OF_MANDATORY_RANGE 0x30 |
Paramater out of Mandatory Range. | |
#define | HCI_ERROR_CODE_PIN_KEY_MISSING 0x06 |
Pin Key Missing. | |
#define | HCI_ERROR_CODE_QOS_REJ 0x2D |
QOS Reject. | |
#define | HCI_ERROR_CODE_QOS_UNACCEPTABLE_PARAM 0x2C |
QOS Unacceptable Parameter. | |
#define | HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES 0x14 |
Remote Device Terminated Connection due to Low Resources. | |
#define | HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF 0x15 |
Remote Device Terminated Connection due to Power Off. | |
#define | HCI_ERROR_CODE_REMOTE_USER_TERM_CONN 0x13 |
Remote User Terminated Connection. | |
#define | HCI_ERROR_CODE_REPEATED_ATTEMPTS 0x17 |
Repeated Attempts. | |
#define | HCI_ERROR_CODE_REQ_QOS_NOT_SUPPORTED 0x27 |
Request QOS Not Supported. | |
#define | HCI_ERROR_CODE_RESERVED1 0x2B |
Reserved. | |
#define | HCI_ERROR_CODE_RESERVED2 0x31 |
Reserved. | |
#define | HCI_ERROR_CODE_RESERVED3 0x33 |
Reserved. | |
#define | HCI_ERROR_CODE_RESERVED_SLOT_VIOLATION 0x34 |
Reserved Slot Violation. | |
#define | HCI_ERROR_CODE_ROLE_CHANGE_NOT_ALLOWED 0x21 |
Role Change Not Allowed. | |
#define | HCI_ERROR_CODE_ROLE_SWITCH_FAILED 0x35 |
Role Switch Failed. | |
#define | HCI_ERROR_CODE_ROLE_SWITCH_PENDING 0x32 |
Role Switch Pending. | |
#define | HCI_ERROR_CODE_SCO_AIR_MODE_REJ 0x1D |
SCO Air Mode Rejected. | |
#define | HCI_ERROR_CODE_SCO_INTERVAL_REJ 0x1C |
SCO Interval Rejected. | |
#define | HCI_ERROR_CODE_SCO_OFFSET_REJ 0x1B |
SCO Offset Rejected. | |
#define | HCI_ERROR_CODE_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST 0x37 |
Simple Pairing Not Supported by Host. | |
#define | HCI_ERROR_CODE_SYNCH_CONN_LIMIT_EXCEEDED 0x0A |
Synchonous Connection Limit Exceeded. | |
#define | HCI_ERROR_CODE_UNACCEPTABLE_CONN_PARAMETERS 0x3B |
Unacceptable Connection Parameters. | |
#define | HCI_ERROR_CODE_UNKNOWN_CONN_ID 0x02 |
Unknown Connection ID. | |
#define | HCI_ERROR_CODE_UNKNOWN_HCI_CMD 0x01 |
Unknown HCI Command. | |
#define | HCI_ERROR_CODE_UNKNOWN_LMP_PDU 0x19 |
Unknown LMP PDU. | |
#define | HCI_ERROR_CODE_UNSPECIFIED_ERROR 0x1F |
Unspecified Error. | |
#define | HCI_ERROR_CODE_UNSUPPORTED_FEATURE_PARAM_VALUE 0x11 |
Unsupported Paramter. | |
#define | HCI_ERROR_CODE_UNSUPPORTED_LMP_PARAM_VAL 0x20 |
Unsupported LMP Parameter Value. | |
#define | HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE 0x1A |
Unsupported Remote Feature. | |
#define | HCI_EXT_DISABLE_FAST_TX_RESP_TIME LL_EXT_DISABLE_FAST_TX_RESP_TIME |
Disable. | |
#define | HCI_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT |
Disable. | |
#define | HCI_EXT_DISABLE_ONE_PKT_PER_EVT LL_EXT_DISABLE_ONE_PKT_PER_EVT |
Disable. | |
#define | HCI_EXT_DISABLE_SCAN_REQUEST_REPORT LL_EXT_DISABLE_SCAN_REQUEST_REPORT |
Disable. | |
#define | HCI_EXT_DISABLE_SL_OVERRIDE LL_EXT_DISABLE_SL_OVERRIDE |
Disable. | |
#define | HCI_EXT_ENABLE_FAST_TX_RESP_TIME LL_EXT_ENABLE_FAST_TX_RESP_TIME |
Enable. | |
#define | HCI_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT |
Enable. | |
#define | HCI_EXT_ENABLE_ONE_PKT_PER_EVT LL_EXT_ENABLE_ONE_PKT_PER_EVT |
Enable. | |
#define | HCI_EXT_ENABLE_SCAN_REQUEST_REPORT LL_EXT_ENABLE_SCAN_REQUEST_REPORT |
Enable. | |
#define | HCI_EXT_ENABLE_SL_OVERRIDE LL_EXT_ENABLE_SL_OVERRIDE |
Enable. | |
#define | HCI_EXT_NV_IN_USE LL_EXT_NV_IN_USE |
NV in Use. | |
#define | HCI_EXT_NV_NOT_IN_USE LL_EXT_NV_NOT_IN_USE |
NV Not in Use. | |
#define | HCI_EXT_PER_READ LL_EXT_PER_READ |
Read. | |
#define | HCI_EXT_PER_RESET LL_EXT_PER_RESET |
Reset. | |
#define | HCI_EXT_READ_BUILD_REVISION LL_EXT_READ_BUILD_REVISION |
Read. | |
#define | HCI_EXT_RESET_SYSTEM_HARD LL_EXT_RESET_SYSTEM_HARD |
Hard Reset. | |
#define | HCI_EXT_RESET_SYSTEM_SOFT LL_EXT_RESET_SYSTEM_SOFT |
Soft Reset. | |
#define | HCI_EXT_RX_GAIN_HIGH LL_EXT_RX_GAIN_HIGH |
High Gain. | |
#define | HCI_EXT_RX_GAIN_STD LL_EXT_RX_GAIN_STD |
Standard Gain. | |
#define | HCI_EXT_SET_USER_REVISION LL_EXT_SET_USER_REVISION |
Set. | |
#define | HCI_EXT_TX_MODULATED_CARRIER LL_EXT_TX_MODULATED_CARRIER |
Modulated. | |
#define | HCI_EXT_TX_POWER_0_DBM LL_EXT_TX_POWER_0_DBM |
0 dBm | |
#define | HCI_EXT_TX_POWER_1_DBM LL_EXT_TX_POWER_1_DBM |
1 dBm | |
#define | HCI_EXT_TX_POWER_2_DBM LL_EXT_TX_POWER_2_DBM |
2 dBm | |
#define | HCI_EXT_TX_POWER_3_DBM LL_EXT_TX_POWER_3_DBM |
3 dBm | |
#define | HCI_EXT_TX_POWER_4_DBM LL_EXT_TX_POWER_4_DBM |
4 dBm | |
#define | HCI_EXT_TX_POWER_5_DBM LL_EXT_TX_POWER_5_DBM |
5 dBm | |
#define | HCI_EXT_TX_POWER_MINUS_12_DBM LL_EXT_TX_POWER_MINUS_12_DBM |
-12 dBm | |
#define | HCI_EXT_TX_POWER_MINUS_15_DBM LL_EXT_TX_POWER_MINUS_15_DBM |
-15 dBm | |
#define | HCI_EXT_TX_POWER_MINUS_18_DBM LL_EXT_TX_POWER_MINUS_18_DBM |
-18 dBm | |
#define | HCI_EXT_TX_POWER_MINUS_21_DBM LL_EXT_TX_POWER_MINUS_21_DBM |
-21 dBm | |
#define | HCI_EXT_TX_POWER_MINUS_3_DBM LL_EXT_TX_POWER_MINUS_3_DBM |
3 dBm | |
#define | HCI_EXT_TX_POWER_MINUS_6_DBM LL_EXT_TX_POWER_MINUS_6_DBM |
6 dBm | |
#define | HCI_EXT_TX_POWER_MINUS_9_DBM LL_EXT_TX_POWER_MINUS_9_DBM |
9 dBm | |
#define | HCI_EXT_TX_UNMODULATED_CARRIER LL_EXT_TX_UNMODULATED_CARRIER |
Unmodulated. | |
#define | HCI_FILTER_REPORTS_DISABLE LL_FILTER_REPORTS_DISABLE |
Disable. | |
#define | HCI_FILTER_REPORTS_ENABLE LL_FILTER_REPORTS_ENABLE |
Enable. | |
#define | HCI_INIT_WL_POLICY_USE_PEER_ADDR LL_INIT_WL_POLICY_USE_PEER_ADDR |
Use Peer Address. | |
#define | HCI_INIT_WL_POLICY_USE_WHITE_LIST LL_INIT_WL_POLICY_USE_WHITE_LIST |
Use Whitelist. | |
#define | HCI_LINK_TYPE_ACL_BUFFER_OVERFLOW 1 |
ACL Buffer Overflow. | |
#define | HCI_LINK_TYPE_SCO_BUFFER_OVERFLOW 0 |
SCO Buffer Overflow. | |
#define | HCI_MAX_NUM_CMD_BUFFERS LL_MAX_NUM_CMD_BUFFERS |
Max Num Command Buffer. | |
#define | HCI_NONCONNECTABLE_UNDIRECTED_ADV LL_ADV_NONCONNECTABLE_UNDIRECTED_EVT |
Nonconnectable Undirected Advertising. | |
#define | HCI_PHY_1_MBPS LL_PHY_1_MBPS |
1 Mbps | |
#define | HCI_PHY_2_MBPS LL_PHY_2_MBPS |
2 Mbps | |
#define | HCI_PHY_USE_ANY_PHY LL_PHY_USE_ANY_PHY |
Use any PHY. | |
#define | HCI_PHY_USE_PHY_PARAM LL_PHY_USE_PHY_PARAM |
Use PHY specified by Phy Types. | |
#define | HCI_PTM_SET_FREQ_TUNE_DOWN LL_EXT_SET_FREQ_TUNE_DOWN |
Tune Down. | |
#define | HCI_PTM_SET_FREQ_TUNE_UP LL_EXT_SET_FREQ_TUNE_UP |
Tune Up. | |
#define | HCI_PUBLIC_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_PUBLIC |
Public Device Address. | |
#define | HCI_RANDOM_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_RANDOM |
Random Device Address. | |
#define | HCI_READ_CURRENT_TX_POWER_LEVEL LL_READ_CURRENT_TX_POWER_LEVEL |
Read Current TX Power Level. | |
#define | HCI_READ_MAX_TX_POWER_LEVEL LL_READ_MAX_TX_POWER_LEVEL |
Read Max TX Power Level. | |
#define | HCI_RSSI_NOT_AVAILABLE LL_RSSI_NOT_AVAILABLE |
Invalid RSSI. | |
#define | HCI_SCAN_ACTIVE LL_SCAN_ACTIVE |
Active Scan. | |
#define | HCI_SCAN_PASSIVE LL_SCAN_PASSIVE |
Passive Scan. | |
#define | HCI_SCAN_START LL_SCAN_START |
Scan Start. | |
#define | HCI_SCAN_STOP LL_SCAN_STOP |
Scan Stop. | |
#define | HCI_SCAN_WL_POLICY_ANY_ADV_PKTS LL_SCAN_WL_POLICY_ANY_ADV_PKTS |
Any Advertising Packets. | |
#define | HCI_SCAN_WL_POLICY_USE_WHITE_LIST LL_SCAN_WL_POLICY_USE_WHITE_LIST |
Use Whitelist. | |
#define | HCI_SCANNABLE_UNDIRECTED LL_ADV_SCANNABLE_UNDIRECTED_EVT |
Scannable Undirected Advertising. | |
#define | HCI_SUCCESS 0x00 |
Success. | |
Typedefs | |
typedef union _hciEvt_BLEConnComplete_u_ | hciEvt_BLEConnComplete_u |
LE Connection Complete Event. | |
Functions | |
hciStatus_t | HCI_DisconnectCmd (uint16 connHandle, uint8 reason) |
Terminate a connection. More... | |
hciStatus_t | HCI_EXT_AdvEventNoticeCmd (uint8 taskID, uint16 taskEvent) |
Advertising Event Notice Command. More... | |
hciStatus_t | HCI_EXT_BuildRevisionCmd (uint8 mode, uint16 userRevNum) |
Set a user revision number or read the build revision number. More... | |
hciStatus_t | HCI_EXT_DecryptCmd (uint8 *key, uint8 *encText) |
Decrypt encrypted data using AES128. More... | |
hciStatus_t | HCI_EXT_DisconnectImmedCmd (uint16 connHandle) |
Disconnect the connection immediately. More... | |
hciStatus_t | HCI_EXT_EnablePTMCmd (void) |
Enable Production Test Mode. More... | |
hciStatus_t | HCI_EXT_EndModemTestCmd (void) |
Shutdown a modem test. More... | |
hciStatus_t | HCI_EXT_GetActiveConnInfoCmd (uint8 connId, hciActiveConnInfo_t *activeConnInfo) |
This API is used to get connection related information required to follow the target connection with a BLE conneciton monitor. More... | |
hciStatus_t | HCI_EXT_GetConnInfoCmd (uint8 *numAllocConns, uint8 *numActiveConns, hciConnInfo_t *activeConnInfo) |
Get Connection Info. More... | |
hciStatus_t | HCI_EXT_ModemHopTestTxCmd (void) |
Start Modem Hop Tx Test. More... | |
hciStatus_t | HCI_EXT_ModemTestRxCmd (uint8 rxChan) |
Start Modem Hop RX Test. More... | |
hciStatus_t | HCI_EXT_ModemTestTxCmd (uint8 cwMode, uint8 txChan) |
Start Modem TX Test. More... | |
hciStatus_t | HCI_EXT_NumComplPktsLimitCmd (uint8 limit, uint8 flushOnEvt) |
Set the Number of Completed Packets Limit. More... | |
hciStatus_t | HCI_EXT_OnePktPerEvtCmd (uint8 control) |
Set whether a connection will be limited to one packet per event. More... | |
hciStatus_t | HCI_EXT_PacketErrorRateCmd (uint16 connHandle, uint8 command) |
Packet Error Rate Command. More... | |
hciStatus_t | HCI_EXT_PERbyChanCmd (uint16 connHandle, perByChan_t *perByChan) |
Packet Error Rate by Channel Command. More... | |
hciStatus_t | HCI_EXT_ResetSystemCmd (uint8 mode) |
Issue a soft or hard system reset. More... | |
hciStatus_t | HCI_EXT_SaveFreqTuneCmd (void) |
Save the frequency tuning value to non-volatile memory. More... | |
hciStatus_t | HCI_EXT_ScanEventNoticeCmd (uint8 taskID, uint16 taskEvent) |
Scan Event Notice Command. More... | |
hciStatus_t | HCI_EXT_ScanReqRptCmd (uint8 mode) |
Enable/disable Scan Request Reports. More... | |
hciStatus_t | HCI_EXT_SetBDADDRCmd (uint8 *bdAddr) |
Set this device's BLE address (BDADDR). More... | |
hciStatus_t | HCI_EXT_SetFastTxResponseTimeCmd (uint8 control) |
Set Fast TX Response Time. More... | |
hciStatus_t | HCI_EXT_SetFreqTuneCmd (uint8 step) |
Set Frequency Tuning. More... | |
hciStatus_t | HCI_EXT_SetLocalSupportedFeaturesCmd (uint8 *localFeatures) |
Write this device's supported features. More... | |
hciStatus_t | HCI_EXT_SetMaxDataLenCmd (uint16 txOctets, uint16 txTime, uint16 rxOctets, uint16 rxTime) |
Set the maximum Rx and Tx Octets (in bytes) and Time (in us). More... | |
hciStatus_t | HCI_EXT_SetMaxDtmTxPowerCmd (uint8 txPower) |
Set the maximum transmit output power for DTM. More... | |
hciStatus_t | HCI_EXT_SetRxGainCmd (uint8 rxGain) |
Set the receiver gain. More... | |
hciStatus_t | HCI_EXT_SetSCACmd (uint16 scaInPPM) |
Set this device's Sleep Clock Accuracy. More... | |
hciStatus_t | HCI_EXT_SetSlaveLatencyOverrideCmd (uint8 control) |
Enable or disable suspending slave latency. More... | |
hciStatus_t | HCI_EXT_SetTxPowerCmd (uint8 txPower) |
Set the transmit power. More... | |
void | HCI_ExtTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host extended commands. More... | |
void | HCI_GAPTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host GAP. More... | |
hciStatus_t | HCI_HostNumCompletedPktCmd (uint8 numHandles, uint16 *connHandles, uint16 *numCompletedPkts) |
Set the number of HCI daata packets completed per connection handle. More... | |
void | HCI_L2CAPTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host L2CAP. More... | |
hciStatus_t | HCI_LE_AddDeviceToResolvingListCmd (uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 *peerIRK, uint8 *localIRK) |
Add a device to the resolving list. More... | |
hciStatus_t | HCI_LE_AddWhiteListCmd (uint8 addrType, uint8 *devAddr) |
Add a white list entry. More... | |
hciStatus_t | HCI_LE_ClearResolvingListCmd (void) |
Remove all devices from the whitelist. More... | |
hciStatus_t | HCI_LE_ClearWhiteListCmd (void) |
Clear the white list. More... | |
hciStatus_t | HCI_LE_ConnUpdateCmd (uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
Update the connection parameters. More... | |
hciStatus_t | HCI_LE_CreateConnCancelCmd (void) |
Cancel connection. More... | |
hciStatus_t | HCI_LE_CreateConnCmd (uint16 scanInterval, uint16 scanWindow, uint8 initFilterPolicy, uint8 addrTypePeer, uint8 *peerAddr, uint8 ownAddrType, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
Create a connection. More... | |
hciStatus_t | HCI_LE_EncryptCmd (uint8 *key, uint8 *plainText) |
Perform an encryption using AES128. More... | |
hciStatus_t | HCI_LE_GenerateDHKeyCmd (uint8 *publicKey) |
Generate Diffie-Hellman Key. More... | |
hciStatus_t | HCI_LE_LtkReqNegReplyCmd (uint16 connHandle) |
Send a negative LTK reply to the Controller. More... | |
hciStatus_t | HCI_LE_LtkReqReplyCmd (uint16 connHandle, uint8 *ltk) |
Send a positive LTK reply to the controller. More... | |
hciStatus_t | HCI_LE_RandCmd (void) |
Generate a random number. More... | |
hciStatus_t | HCI_LE_ReadAdvChanTxPowerCmd (void) |
Read transmit power when Advertising. More... | |
hciStatus_t | HCI_LE_ReadBufSizeCmd (void) |
Determine the maximum ACL data packet size allowed by the Controller. More... | |
hciStatus_t | HCI_LE_ReadChannelMapCmd (uint16 connHandle) |
Read a connection's data channel map. More... | |
hciStatus_t | HCI_LE_ReadLocalP256PublicKeyCmd (void) |
Read local P-256 Public Key. More... | |
hciStatus_t | HCI_LE_ReadLocalResolvableAddressCmd (uint8 localIdAddrType, uint8 *localIdAddr) |
Read Local Resolvable Private Address. More... | |
hciStatus_t | HCI_LE_ReadLocalSupportedFeaturesCmd (void) |
Read the LE locally supported features. More... | |
hciStatus_t | HCI_LE_ReadMaxDataLenCmd (void) |
Read max data length. More... | |
hciStatus_t | HCI_LE_ReadPeerResolvableAddressCmd (uint8 peerIdAddrType, uint8 *peerIdAddr) |
Read the Peer Resolvable Address. More... | |
hciStatus_t | HCI_LE_ReadRemoteUsedFeaturesCmd (uint16 connHandle) |
Read the remote device's used features. More... | |
hciStatus_t | HCI_LE_ReadResolvingListSizeCmd (void) |
Read Resolving List Size. More... | |
hciStatus_t | HCI_LE_ReadSuggestedDefaultDataLenCmd (void) |
Read Suggested Default Data Length. More... | |
hciStatus_t | HCI_LE_ReadSupportedStatesCmd (void) |
TRead the Controller's supported states. More... | |
hciStatus_t | HCI_LE_ReadWhiteListSizeCmd (void) |
Read the white list. More... | |
hciStatus_t | HCI_LE_ReceiverTestCmd (uint8 rxChan) |
Start the receiver Direct Test Mode test. More... | |
hciStatus_t | HCI_LE_RemoteConnParamReqNegReplyCmd (uint16 connHandle, uint8 reason) |
Negatively reply to the Conneciton Parameter Update Request. More... | |
hciStatus_t | HCI_LE_RemoteConnParamReqReplyCmd (uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
Positively reply to the Conneciton Parameter Update Request. More... | |
hciStatus_t | HCI_LE_RemoveDeviceFromResolvingListCmd (uint8 peerIdAddrType, uint8 *peerIdAddr) |
Remove a device from the whitelist. More... | |
hciStatus_t | HCI_LE_RemoveWhiteListCmd (uint8 addrType, uint8 *devAddr) |
Remove a white list entry. More... | |
hciStatus_t | HCI_LE_SetAddressResolutionEnableCmd (uint8 addrResolutionEnable) |
Disable / Enable Address Resolution. More... | |
hciStatus_t | HCI_LE_SetAdvDataCmd (uint8 dataLen, uint8 *pData) |
Set the Advertising data. More... | |
hciStatus_t | HCI_LE_SetAdvEnableCmd (uint8 advEnable) |
Turn Advertising on or off. More... | |
hciStatus_t | HCI_LE_SetAdvParamCmd (uint16 advIntervalMin, uint16 advIntervalMax, uint8 advType, uint8 ownAddrType, uint8 directAddrType, uint8 *directAddr, uint8 advChannelMap, uint8 advFilterPolicy) |
Set the Advertising parameters. More... | |
hciStatus_t | HCI_LE_SetDataLenCmd (uint16 connHandle, uint16 txOctets, uint16 txTime) |
Set Data Length. More... | |
hciStatus_t | HCI_LE_SetEventMaskCmd (uint8 *pEventMask) |
Set the HCI LE event mask. More... | |
hciStatus_t | HCI_LE_SetHostChanClassificationCmd (uint8 *chanMap) |
Update the current data channel map. More... | |
hciStatus_t | HCI_LE_SetRandomAddressCmd (uint8 *pRandAddr) |
Set this device's Random address. More... | |
hciStatus_t | HCI_LE_SetResolvablePrivateAddressTimeoutCmd (uint16 rpaTimeout) |
Set Resolvable Private Address Timeout. More... | |
hciStatus_t | HCI_LE_SetScanEnableCmd (uint8 scanEnable, uint8 filterDuplicates) |
Turn Scanning on or off. More... | |
hciStatus_t | HCI_LE_SetScanParamCmd (uint8 scanType, uint16 scanInterval, uint16 scanWindow, uint8 ownAddrType, uint8 filterPolicy) |
Set the Scan parameters. More... | |
hciStatus_t | HCI_LE_SetScanRspDataCmd (uint8 dataLen, uint8 *pData) |
Set the Advertising Scan Response data. More... | |
hciStatus_t | HCI_LE_StartEncyptCmd (uint16 connHandle, uint8 *random, uint8 *encDiv, uint8 *ltk) |
Start encryption in a connection. More... | |
hciStatus_t | HCI_LE_TestEndCmd (void) |
End the Direct Test Mode test. More... | |
hciStatus_t | HCI_LE_TransmitterTestCmd (uint8 txChan, uint8 dataLen, uint8 pktPayload) |
This LE API is used to start the transmit Direct Test Mode test. More... | |
hciStatus_t | HCI_LE_WriteSuggestedDefaultDataLenCmd (uint16 txOctets, uint16 txTime) |
Write Suggested Default Data Length. More... | |
hciStatus_t | HCI_ReadAuthPayloadTimeoutCmd (uint16 connHandle, uint16 *aptoValue) |
Read the connection's Authenticated Payload Timeout value. More... | |
hciStatus_t | HCI_ReadBDADDRCmd (void) |
Read this device's BLE address (BDADDR). More... | |
hciStatus_t | HCI_ReadLocalSupportedCommandsCmd (void) |
Read the locally supported commands. More... | |
hciStatus_t | HCI_ReadLocalSupportedFeaturesCmd (void) |
Read the locally supported features. More... | |
hciStatus_t | HCI_ReadLocalVersionInfoCmd (void) |
Read the local version information. More... | |
hciStatus_t | HCI_ReadRemoteVersionInfoCmd (uint16 connHandle) |
Request version information from the remote device in a connection. More... | |
hciStatus_t | HCI_ReadRssiCmd (uint16 connHandle) |
Read RSSI of last packet. More... | |
hciStatus_t | HCI_ReadTransmitPowerLevelCmd (uint16 connHandle, uint8 txPwrType) |
Read the transmit power level. More... | |
hciStatus_t | HCI_ResetCmd (void) |
Reset the Link Layer. More... | |
hciStatus_t | HCI_SendDataPkt (uint16 connHandle, uint8 pbFlag, uint16 pktLen, uint8 *pData) |
Send an ACL data packet over a connection. More... | |
hciStatus_t | HCI_SetEventMaskCmd (uint8 *pMask) |
Set the HCI event mask. More... | |
hciStatus_t | HCI_SetEventMaskPage2Cmd (uint8 *pMask) |
Set the HCI event mask page 2. More... | |
void | HCI_SMPTaskRegister (uint8 taskID) |
HCI vendor specific registration for Host SMP. More... | |
void | HCI_TestAppTaskRegister (uint8 taskID) |
HCI vendor specific registration for HCI Test Application. More... | |
uint8 | HCI_ValidConnTimeParams (uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout) |
Checks that the connection time parameter ranges are valid. More... | |
hciStatus_t | HCI_WriteAuthPayloadTimeoutCmd (uint16 connHandle, uint16 aptoValue) |
Used to write the connection's Authenticated Payload Timeout value. More... | |