Here is a list of all documented files with brief descriptions:
att.h | ATT layer interface |
bcomdef.h | Type definitions and macros for BLE stack |
central.h | Central layer interface |
comdef.h | Common Defines |
ECCROMCC26XX.h | ECC ROM driver implementation for a CC26XX device |
ext_flash_layout.h | Contains common structures and defines related to external flash layout as it for the OAD usecase |
flash_interface.h | An interface that abstracts flash operations for OAD this allows on-chip and off-chip OAD to use the same flash APIs |
gap.h | GAP layer interface |
gapbondmgr.h | GAPBondMgr layer interface |
gatt.h | GATT layer interface |
gattservapp.h | GATTServApp layer interface |
hci.h | HCI layer interface |
hci_tl.h | Types, constants, external functions etc. for the BLE HCI Transport Layer |
icall.h | ICall layer interface |
icall_addrs.h | Stack image address information specific to build |
icall_cc26xx_defs.h | Indirect function Call dispatcher constant definitions specific to CC26xx platform |
l2cap.h | L2CAP layer interface |
linkdb.h | LinkDB layer interface |
multi.h | Multi layer interface |
oad.h | This file contains OAD Profile header file |
oad_image_header.h | Structure definition for image header and segments, these are prepended to the over the air images |
osal.h | This API allows the software components in the Z-Stack to be written independently of the specifics of the operating system, kernel, or tasking environment (including control loops or connect-to-interrupt systems) |
osal_memory.h | His module defines the OSAL memory control functions |
peripheral.h | Peripheral layer interface |
simple_np.h | |
simple_np_dev.h | SNP Device API |
simple_np_gap.h | SNP GAP Layer API |
simple_np_gatt.h | SNP GATT Layer API |
sm.h | This file contains the interface to the SM |
snp.h | Simple Network Processor API |
SNP_doc.h | |
TRNGCC26XX.h | TRNG driver implementation for a CC26XX device |
uble.h | This file contains configuration, initialization, and parameter management of Micro BLE Stack. It also contains interfacing between Micro BLE Stack and the application |
ugap.h | Micro BLE GAP API |
urfc.h | This file contains configurable variables for the Micro BLE Stack radio |
util.h | Util layer interface |