Network Processor Interface (NPI)

TI’s Network Processor Interface (NPI) is used for establishing a serial data link between a TI SoC and external MCUs or PCs. It is an abstraction layer above the serial interface (UART or SPI) that handles sending / receiving data power management, and data parsing It is mainly used by TI’s network processor solutions. There are two types of NPI used by BLE and they are described in the following sections.

Legacy NPI

Anything that is not specifically “Unified NPI” is Legacy NPI. For example, the hostTest project uses Legacy NPI. For the remainder of this section, NPI will always refer to Legacy NPI

TI provides the source code for NPI and it can be found in the following files at $SDK_INSTALL$sourcetiblestacknpisrc:

  • npi_client_mt.c
  • npi_frame_hci.c
  • npi_fram_mt.c
  • npi_rxbuf.c
  • npi_task.c
  • npi_tl.c
  • npi_tl_spi.c or npi_tl_uart.c

Signaling Protocol

Each processor in an NPI solution must occupy either the master or slave role. The TI wireless SoC generally occupies the slave role in the network processor examples included in the SDK.

NPI Signaling

In order to properly manage the power domains of the device, there must be a way for an external host to wake the network processor from low power modes. This is done through the inclusion of the following pins:

  • Master Ready (MRDY): A GPIO pin whose logic level indicates the state of the master processor. MRDY is an active low (low true) signal. An MRDY event indicates that the master processor is ready to send or receive data.
  • Slave Ready (SRDY): A GPIO pin whose logic level indicates the state of the slave processor. SRDY is an active low (low true) signal. An SRDY event indicates that the slave processor is ready to send or receive data.

In the slave role, MRDY is an input pin and SRDY is an output in. In the master role, MRDY is an output pin and SRDY is an input pin.

NPI Handshake

In order to start an NPI transaction, there first must occur a handshake sequence using the MRDY and SRDY pins. This handshake is required in order to guarantee that both devices are awake and ready to send and/or receive data. Whichever device first starts the handshake sequence is termed the “initiator”. Either the slave or the master may may be the imitator. The NPI transaction is completed by the master raising MRDY followed by the slave raising SRDY.

The figures below illustrate both master and slave-initiated NPI transactions

../_images/legacy_npi_timing_master_initiates.png

Figure 82. Timing for Master-Initiated NPI Transaction

../_images/legacy_npi_timing_slave_initiates.png

Figure 83. Timing for Slave-Initiated NPI Transaction

Packet Format

The NPI module handles the serial driver-level packet formatting, stripping of the NPI, header and FCS when unpacking. This section will describe the packet format to be used with NPI.

Note

This section does not consider the packet format of the data payload section of the NPI packet format as this is dependent on the NPI use case (i.e. HCI packet format for BLE).

The packet format is dependent on the serial protocol being used and described in the following sections.

SPI

In order to understand the structure of the TL packet format, it is necessary to understand the complications inherent in the SPI protocol. The first limitation is that the SPI master must trigger the clock signal (SCLK) in order to receive bytes from the slave. If the slave is sending a message, then the master must know how long this message is in order to receive the complete message. The other limitation of SPI is that if the clock signal is triggered, the master or slave must transmit empty bytes if they have nothing to send. The simple scenario when this occurs is during either a communication sequence where either the master or slave receives only empty bytes. These messages of strictly empty bytes could be easily ignored but the bidirectional message scenario requires more complex handling. If the slave and master are both transmitting non-empty bytes then the shorter message will have to be padded with empty bytes so that the longer message can be fully transmitted. Determining which bytes of message bytes versus empty bytes in this scenario requires message delimitation. In order to handle these limitations of SPI, the NPI SPI Frame is used for all NPI messages sent over SPI.

The NPI SPI Frame has four fields described thus and pictured below:

  • 1 byte Start of Frame (SOF): always 0xFE
  • 1 byte length: length of the data payload field (must be between 0-255 bytes)
  • 0-255 byte Data Payload
  • 1 byte Frame Check Sequence (FCS): calculated by doing a XOR on each byte of the frame in the order they are sent/received on the bus. The SOF byte shall not be included in the FCS calculation.
../_images/legacy_npi_spi_protocol.png

Figure 84. NPI SPI Packet Format

This NPI SPI Frame handles both the delimitation of empty vs non empty data bytes as well as having a fixed length field allowing the SPI master to know how many times the SCLK signal must be toggled to receive a complete message from the SPI slave.

UART

Since UART does not have the same inherent complication as SPI, a much simpler frame format can be used. Because UART RX and TX channels are independent of each other, there is no need for a predefined fixed length field, Furthermore, since there are no empty bytes that must be transmitted, each frame does not need to be delimited. Therefore, every byte received over UART RX or TX channels can be treated as a valid byte of data payload. This allows the NPI UART Frame to consist of only a data payload field:

../_images/legacy_npi_uart_protocol.png

Figure 85. NPI UART Packet Format

Message Types

Both synchronous and asynchronous messages can be supported by NPI. By default, only asynchronous messages are supported. Support for synchronous messages can be compiled into NPI using the compiler define NPI_SREQRSP.

Asynchronous

There are two types of asynchronous messages: asynchronous request ((AREQ)) and asynchronous indication ((AIND)). These messages have the same frame, but the difference lies in whether the transfer was initiated by the network processor (AIND) or the host/application processor (AREQ).

Synchronous

Synchronous messages are blocking in that once a synchronous request ((SREQ)) is sent over NPI all other NPI transmissions are blocked until a corresponding synchronous response ((SRESP)) is returned.

Unified NPI

If Unified NPI is being referenced, it will be specifically referred to as “Unified NPI” or (UNPI). Anything that is not specifically called “Unified NPI” is Legacy NPI. However, the API’s and source files of the UNPI implementation will still always be called “NPI”.

Unified NPI offers some improvements over NPI in that it offers a unified frame format that is used by all transport layers.

For a UNPI example, see the Simple Network Processor project.

TI provides the source code for UNPI and it can be found in the following files at <SDK_INSTALL_DIR>\source\tiblstacknpi\src\unified

  • npi_task.c
  • npi_tl.c
  • npi_tl_spi.c or npi_tl_uart.c
  • npi_util.c

UNPI Architecture

UNPI is implemented as its own TI-RTOS task, and supports inter task communication and routing to the underlying serial interface drivers. See the diagram below for details:

../_images/unified_npi_block_diagram.png

Figure 86. Block Diagram for UNPI

UNPI Signaling

Each processor in an UNPI solution must occupy either the master or slave role. The TI wireless SoC generally occupies the slave role in the network processor examples included in the SDK.

For the remainder of this section, the following terms will be used:

  • Application Processor ((AP): UNPI Master (the host MCU)
  • Network Processor ((NP)): UNPI Slave (the TI network processor)

In order to properly manage the power domains of the device, there must be a way for an external host to wake the network processor from low power modes. This is done through the inclusion of the following pins:

  • Master Ready (MRDY): A GPIO pin whose logic level indicates the state of the master processor. MRDY is an active low (low true) signal. An MRDY event indicates that the master processor is ready to send or receive data.
  • Slave Ready (SRDY): A GPIO pin whose logic level indicates the state of the slave processor. SRDY is an active low (low true) signal. An SRDY event indicates that the slave processor is ready to send or receive data.

In the slave role, MRDY is an input pin and SRDY is an output in. In the master role, MRDY is an output pin and SRDY is an input pin.

UNPI Handshake

In order to start an UNPI transaction, there first must occur a handshake sequence using the MRDY and SRDY pins. This handshake is required in order to guarantee that both devices are awake and ready to send and/or receive data. Whichever device first starts the handshake sequence is termed the “initiator”. Either the slave or the master may may be the imitator. The UNPI transaction is completed by the master raising MRDY followed by the slave raising SRDY.

The figures below illustrate both master and slave-initiated UNPI transactions

../_images/unified_npi_timing_master_initiates.png

Figure 87. Timing for Master-Initiated UNPI Transaction

../_images/unified_npi_timing_slave_initiates.png

Figure 88. Timing for Slave-Initiated UNPI Transaction

Note

Bidirectional (full-duplex) messaging is also possible with UNPI. See the section below for more details.

Packet Format

The Unified NPI packet format consists of the following fields and is pictured below:

  • 1 byte Start of Frame (SOF): always 0xFE
  • 2 byte Length field in little-endian format (so LSB first)
  • 1 byte Type / Subsystem: that contains both message type and subsystem information as such:
    • Bits[7:5]: Message type, see the message type section for more info
    • Bits[4:0]: Subsystem ID field, used to help UNPI route the message to the appropriate place.
  • 1 byte command ID: opcode of the command being sent
  • variable length Payload: the length of the payload is defined by the length field.
  • 1 byte Frame Check Sequence (FCS): calculated by doing a XOR on each byte of the frame in the order they are sent / received on the bus. The SOF byte is always excluded from the FCS calculation.
../_images/unified_npi_packet_format.png

Figure 89. UNPI Packet Format

Message Types

There are three message types supported by Unified NPI. The type of message being sent is often dependent on which processor initiated the transaction. The message types are described below.

Code Message Type
0x01 Synchronous Request (SREQ)
0x02 Asynchronous Request/Indication (AREQ/AIND)
0x03 Synchronous Response (SRESP)

Synchronous Messages

A Synchronous Request ((SREQ)) is a frame, defined by data content instead of the ordering of events of the physical interface, which is sent from the Host to NP where the next frame sent from NP to Host must be the Synchronous Response ((SRESP)) to that SREQ. Once a SREQ is sent, the UNPI interface blocks until a corresponding response (SRESP) is received.

Asynchronous Messages

There are two types of asynchronous messages: asynchronous request ((AREQ)) and asynchronous indication ((AIND)). These messages have the same frame, but the difference lies in whether the transfer was initiated by the network processor (AIND) or the host/application processor (AREQ).

Bidirectional Messaging

There are inherently collisions between messages in any protocol that allows asynchronous messaging (where a signal transition denotes the start of a message as with MRDY and SRDY). Instead of requiring intricate collision handling, the UNPI framework allows for bidirectional messaging to occur. This means that data can be sent from the AP to NP and from NP to the AP in the same message window regardless of the handshake order.

While reducing collision handling, bidirectional messaging adds some complexity to what operations must be performed or initiated by each device. For every AIND the NP initiates, it must prepare to both read and write when MRDY is asserted. For every REQ, the AP must prepare to both read and write once SRDY is asserted. Each device will also need to handle any FIFOs that could potentially be overrun during a message and check at the end of every message to see what, if anything, has been received.

The flow chart for bidirectional message is shown here:

../_images/unified_npi_bidirection.png

Figure 90. UNPI Bidirectional Flow Chart

Note

Bidirectional messaging is enabled regardless of power savings options

UNPI Usage

Currently, the UNPI protocol has been implemented using the UART and SPI drivers on CC26xx devices. There are certain driver specific settings that should be configured which are defined in the following sections.

Initially, the UNPI task doesn’t initiate the MRDY and SRDY pins; it will let the pins default to IOID_UNUSED. It is application’s responsibility to define these pins as such:

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
#define MDRY_PIN        Board_PIN_BUTTON0
#define SDRY_PIN        Board_PIN_BUTTON1
...
// NP Parameters for opening serial port to NP
static NPI_Params portParams;
...
#ifdef NPI_USE_UART
  NPITask_Params_init(NPI_SERIAL_TYPE_UART, &portParams);
#elif defined(NPI_USE_SPI)
  NPITask_Params_init(NPI_SERIAL_TYPE_SPI, &portParams);
#else
#error "Must define NPI_USE_UART or NPI_USE_SPI for any project including NPI"
#endif //NPI_USE_UART
  portParams.stackSize = NPI_TASK_STACK_SIZE;
  portParams.mrdyPinID = MDRY_PIN;
  portParams.srdyPinID = SDRY_PIN;
  portParams.bufSize   = 530;

  // Kick off NPI
  NPITask_open(&portParams);

UART

To use this configuration, the UART project configuration should be selected (if available). This configuration allows low power modes through the inclusion of the MRDY and SRDY signals. If a pre-made project configuration is not included in the SDK, then NPI_USE_UART must be defined as well as including the CC26xx UART drivers. If power management is needed, be sure to define POWER_SAVING and use the MRDY/SRDY signals. The NPI task sets up the UART port with the following settings:

Parameter Default Value
Baud Rate 115200
Data Length 8
Parity None
Stop Bits 1
Flow Control None

Changing the baud rate can be done in the NPITask_Params_init() function as below:

1
2
3
4
5
6
7
UART_Params_init(&params->portParams.uartParams);
params->portParams.uartParams.readDataMode = UART_DATA_BINARY;
params->portParams.uartParams.writeDataMode = UART_DATA_BINARY;
params->portParams.uartParams.readMode = UART_MODE_CALLBACK;
params->portParams.uartParams.writeMode = UART_MODE_CALLBACK;
params->portParams.uartParams.readEcho = UART_ECHO_OFF;
params->portParams.uartParams.baudRate= 460800;

SPI

In order to allow full duplex communication, the SPI configuration requires the use of MRDY and SRDY regardless of whether or not power management is enabled. In order to use SPI, use the project configuration included in the SDK (if applicable). If a project configuration is unavailable, then NPI_USE_SPI should be defined as well as including the CC26xx SPI drivers. If power savings is needed, be sure to define POWER_SAVINGS.

The NPI task will initialize the SPI with the following parameters

Parameter Default Value
Bit Rate 800000
Data Length 8

Changing the bit rate can be done in the NPITask_Params_init() function as below:

1
2
3
4
SPI_Params_init(&params->portParams.spiParams);
params->portParams.spiParams.mode = SPI_SLAVE;
params->portParams.spiParams.bitRate = 8000000;
params->portParams.spiParams.frameFormat = SPI_POL1_PHA1;

Implementing An NPI Master

As stated above, the TI device operates as an NPI slave in the network processor use case. This means the external MCU must implement the master UNPI role. When developing the NPI master role on an external MCU, there are a couple things to keep in mind:

  • The NPI master controls MRDY and thus controls when the NPI frame has completed.
  • Even when the slave is sending data, the master must use the payload format to determine how many bytes it expects and raise MRDY when it has received them.
  • Since all packets use the same frame format regardless of protocol, the NPI master can use the frame format to determine when to raise MRDY.

An example of an NPI master implementation for UART can be found at <SDK_INSTALL_DIR>\source\tiblstacknpi\src\unified\npi_tl_uart_m.c

Note

NPI_MASTER must be defined as a preprocessor symbol to use the above file.

When toggling MRDY / SRDY it is important to remember the following rules:

  • Each device must always initiate a read prior to asserting its respective output pin (MRDY with respect to the AP) regardless of the state of the its respective input pin (SRDY with respect to the AP).
  • Each device can only begin to write (or clock data in the case of SPI) once both MRDY and SRDY are asserted.