simple_np (SNP)

Introduction

The simple_np project implements the TI Simple Network Processor Bluetooth low energy device configuration. In this configuration, the CC2640R2 LaunchPad operates as a Bluetooth low energy network processor incorporating the TI BLE Host and Controller components of the protocol stack while the application and profiles execute off-chip on an external MCU. The simple_np (SNP) is used in designs that require adding Bluetooth low energy capability to an existing embedded system with a host MCU or application processor. The BLE-Stack User's Guide for Bluetooth 4.2 provides further details on the serial remote procedure call (RPC) interface to the SNP.

The supported serial transports are UART and SPI, which can be selected via build configurations.

This project uses stack and app configurations that are summarized in the table below:

App Build Configuration Compatible Stack Configuration Description
FlashROM_StackLibrary FlashROM_Library Application build configuration linked to Stack library (fully executable) for UART transport
FlashROM_SPI_StackLibrary_RCOSC FlashROM_Library Application build configuration linked to Stack library (fully executable) for SPI transport

FlashROM_Library configurations use the stack library configuration, which is explained here.

Hardware Prerequisites

The default simple_np configuration uses the LAUNCHXL-CC2640R2. This hardware configuration is shown in the below image:

For custom hardware, see the Running the SDK on Custom Boards section of the BLE-Stack User's Guide for Bluetooth 4.2.

An additional device will also be needed to act as the application processor.

Software Prerequisites

For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes located in the docs/blestack folder. For information on how to import this project into your IDE workspace and build/run, please refer to The CC2640R2F Platform section in the BLE-Stack User's Guide for Bluetooth 4.2.

SNP Functional Overview

This section will provide an architectural overview of the simple_np.

Architecture Overview

The SNP is a dual-device solution that requires an external MCU application processor (AP) to control the CC2640R2F simple network processor. The SNP was designed to simplify the complexity of the AP application by:

Almost the entire BLE stack is implemented on the SNP. This is shown below:

As indicated above and described throughout this document, the AP (external MCU) is responsible for the initial configuration of the GAP and GATT services. It will also be notified of asynchronous events relating to these services, such as connection establishments, attribute value updates, etc. Using the APIs provided, the AP can then proceed accordingly after receiving these events.

The general procedure is:

  1. Initialize GATT (add services, characteristics, CCCD’s, etc.).
  2. Initialize GAP (advertisement data, connection parameters, etc.).
  3. Advertise and optionally wait for a connection.
  4. Respond to GATT requests and send notifications/indications as desired.

As shown in the figure above, TI-RTOS compatible processors can use the SAP library to further simplify application processor development. The SAP library is out of the scope of this document. More information and an example can be found in the MSP432 Bluetooth plugin document.

Default GATT Services

In order to comply with the Bluetooth spec and communicate with central devices such as mobile phones, there are two services which must be included in any BLE device:

Therefore, these services are included by default in the SNP and are managed by the GATT server on the SNP. It is possible for the AP to modify and interact with these services via the commands and events described in the BLE-Stack User's Guide for Bluetooth 4.2.

The figure below depicts how these services are initialized by default in the SNP including what handle each attribute resides at. The Generic Access Service is assigned the value 0x1800 and the Device Information Service is assigned 0x180A.

Any custom services and characteristics that the AP adds to the attribute table will always be added after these initial two services. Any other services that are added by the AP at run-time are managed by the AP. That is, the AP will manage the characteristic value. It will be notified when a read/write of the characteristic occurs and can respond (or not) with the value as it chooses.

Limitations

The SNP will be configured by default to act only as a peripheral and/or broadcaster device. This cannot be modified. This implies that the device can only advertise and accept/reject connection. It cannot discover devices or initiate a connection. Also, the SNP will only be configured as a GATT server; it cannot be a GATT client. The standard use case is for the SNP (peripheral GATT server) to connect to a central GATT client such as a smartphone.

Furthermore, while additional features will be added for future releases, the following limitations currently exist:

Compiling the SNP

The BLE-Stack ships pre-built hexfiles for the SNP in most common configurations. These files can be found at /examples/rtos/CC2640R2_LAUNCHXL/blestack/hexfiles.

For the majority of users it is acceptable to use the SNP as a black box. Further customizations can be made by building the project using IAR or CCS.

The SNP can be configured to support one of two serial interfaces: SPI and UART. The interface can be selected by choosing the relevant project configuration in the IDE. The FlashROM_StackLibrary configuration uses UART, and the FlashROM_SPI_StackLibrary configuration uses SPI.

Furthermore, power management can be enabled/disabled by including/excluding the POWER_SAVING preprocessor definition. This option will be described in more detail in the Unified Network Processor Interface section.

Unified Network Processor Interface

This section will describe TI's Unified Network Processor Interface (NPI). NPI implements the serial link between the application and network processor, and it supports UART or SPI. The Unified NPI Wiki Page contains a full description of the protocol and its inner workings, and it is highly recommended that the user read this page. Only NPI details specific to the NPI BLE Subsystem are covered here.

BLE SNP Subsystem

Unified NPI supports automatically routing messages from the serial port to various software subsystems within the device. This allows the application and network processor to easily exchange different types of messages on the same serial bus without collision. Examples of subsystems include a peripheral subsystem and a debug system. The SNP has its own subsystem. All commands and APIs described in this document use the BLE SNP subsystem. A message’s subsystem is set through its CMD0 field (described below).

The Unified NPI frame format is explained in detail at the Unified NPI Wiki Page, but is copied here for simplicity in explaining the BLE SNP Subsystem.

SOF Length Cmd0 Cmd1 Data Payload FCS
1 Byte (0xFE) 2 bytes 1 byte (bits 5-7: type, bits 0-4: subsystem) 1 Byte 0-4096 bytes 1 Byte

SOF:

Start of Frame (1 byte). This byte must be 0xFE to indicate a start of frame.

Length:

Length of the data payload field (2 bytes). This length does not consider any other fields besides the data payload field. The largest acceptable length is 4095. This field is little endian

Cmd0:

One byte split in 2 fields:

Type Description
0x01 Synchronous Request
0x02 Asynchronous Request
0x03 Synchronous Response

More information about the type and subsystems can be found here.

Cmd1:

opcode of the command / event (1 byte):

Opcode Subgroup Description
0 SNP Device Subgroup
1 SNP GAP Subgroup
2 SNP GATT Subgroup
3 Reserved Subgroup

Payload:

The parameters of the command/event.

FCS:

Frame check sequence, calculated by an exclusive OR on all fields except SOF.

Example SNP BLE Subsystem NPI Frame

The following table shows an example of the SNP Add Service (0x81) command to send to SNP, with service type of primary service (0x01) and UUID 0xFFF0. The SNP frame will be the following:

SOF Length Cmd0 Cmd1 Data Payload FCS
0xFE 0x03 0x00 0x35 0x81 0x01 0xF0 0xFF 0xB9

Note that all multi-byte fields need to be in little endian format (except for variable length data payload field where they are read in the order they arrive on the bus).

Setting MRDY/SRDY Pins

As described on the Unified NPI Wiki Page, MRDY and SRDY are configurable GPIO pins. They can be changed and set by the application. The SNP task (simple_np.c) sets these pins based on defines in the device’s board file. The table below shows the defaults for the projects within the SDK. See the Unified NPI wiki page for an example of how to change these pins.

The following table shows the default pins for serial communication:

PIN CC2640R2F Pins
MRDY IOID_23
SRDY IOID_12
UART_RX IOID_2
UART_TX IOID_3
SPI_MISO IOID_8
SPI_MOSI IOID_9
SPI_CLK IOID_10

Interfacing to the SNP

The SNP can be interfaced to using serial commands. The MSP432 document described in the Architecture Overview section is one example of the Simple Application Processor communicating with the SNP.

The commands that can be used in this serial interface are detailed in the SNP API References section of the BLE-Stack User's Guide for Bluetooth 4.2

See the message sequence chart below for a sample initialization of the SNP.

Note: The chart below uses general terms to describe the payloads sent over the wire, these commands can be found in detail in the API reference above