Simple Peripheral OAD On-chip
Table of Contents
Introduction
The simple_peripheral_oad_onchip project demonstrates on-chip OAD functionality with the simple_peripheral application. The application behavior is the same as the stock simple_peripheral project, with the exception that OAD is added.
OAD security has now been enabled by default. Non secure OAD can be switched to
by using the _unsecure
build configuration below
On-chip OAD employs a dual image architecture. This means that two images share the same BLE-Stack. This project implements the user app application in the OAD on-chip demo. The user app is intended to be the end application image. The persistent app is also included in the project and is intended to be a lightweight implementation of the OAD profile.
FlashROM configurations use the split image configuration, which is explained here. FlashROM/split image configurations are required by OAD on-chip where two applications must share the same BLE-Stack.
Note: This application implements the user app cc2640r2lp_app
and includes the following
projects: The persistent app is implemented by cc2640r2lp_persistent_app
along with the
stack image cc2640r2lp_stack
shared with the user app.
Additionally you will have to load the cc2640r2lp_bim_onchip
for the device to function properly.
Be sure that all build configurations are aligned to use security or
not. If security is to be enabled the BIM project, app project, persistent app,
and stack project must use a secure configuration. The same is true for non
secure configurations
App Build Configuration | Compatible Stack Configuration | Description |
---|---|---|
cc2640r2lp_app | FlashROM | OAD on-chip application FlashROM configuration with security |
cc2640r2lp_app | FlashROM_unsecure | OAD on-chip application FlashROM configuration without security |
Following #define macros are used in BIM project.
BIM #defines | Description |
---|---|
SECURITY | BIM configuration with security,removing this defines removes all the image authentication code |
CACHE_AS_RAM | This define can be used for enabling GPRAM as cache to create more RAM for application use |
DEBUG | This define can be used for debugging. When image is downloaded to the internal flash via JTAG the |
| CRC and/or image signature is not available in the OAD binary image header. As the calculation of | CRC and image signing is done at post build step. The debug mode mode allows skipping of CRC and/or | authentication check. The LED indications are also available for visual feedback.
Following #define macro are used in Application and stack projects.
Stack & App #defines | Description |
---|---|
SECURITY | Application configuration with security, removing this defines removes all the image authentication |
| code CACHE_AS_RAM | This define can be used for enabling GPRAM as cache to create more RAM for application use
This document seeks to extend the simple_peripheral project documentation that is already in place, and explain how simple_peripheral can be used to demonstrate on-chip OAD. For an advanced discussion of OAD, and an in-depth explanation of this project, please see:
OAD Chapter of BLE-Stack User's Guide
Hardware Prerequisites
The default Simple Peripheral OAD on-chip configuration uses the LAUNCHXL-CC2640R2. This hardware configuration is shown in the below image:
For custom hardware, see the Running the SDK on Custom Boards section of the BLE-Stack User's Guide for Bluetooth 4.2..
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes located in the docs/blestack folder. For information on how to import this project into your IDE workspace and build/run, please refer to the BLE-Stack User's Guide.
Service/Profile Table
This project contains the simple service, which has 5 characteristics.
Note that BLE Scanner may report 128 bit UUIDs, but the project is generating 16 bit UUIDs.
Characterisitic | UUID | Format | Properties | Profile Source |
---|---|---|---|---|
1 | FFF1 | 1 Byte Integer | Read/Write | simple_gatt_profile.c |
2 | FFF2 | 1 Byte Integer | Read | simple_gatt_profile.c |
3 | FFF3 | 1 Byte Integer | Write | simple_gatt_profile.c |
4 | FFF4 | 1 Byte Integer | Notify | simple_gatt_profile.c |
5 | FFF5 | 5 Byte Integer | Read | simple_gatt_profile.c |
Additionally this project contains the OAD Reset service, which has 1 characteristic.
See the OAD Chapter of the BLE-Stack User's Guide for more information on the OAD service
Usage
This application uses the UART peripheral to provide an interface for the application. The UART is only used for display messages.
This document will use PuTTY to serve as the display for the output of the CC2640R2 LaunchPad, and it will use BLE Scanner as the phone app that will act as the central device that will connect to the Simple Peripheral device. Note that any other serial terminal and smart phone BLE application can be used. The following default parameters are used for the UART peripheral for display:
UART Param | Default Values |
---|---|
Baud Rate | 115200 |
Data length | 8 bits |
Parity | None |
Stop bits | 1 bit |
Flow Control | None |
For further guidance refer to * On-chip OAD User's Guide Section*