TI BLE-Stack for Bluetooth API Documentation
3.03.07.00
|
HCI Function Mapping
This section lists the mapping between stack APIs and function names, as described in the BT core spec. The App column indicates if the command can be called by the application where Y means yes and N means no.
Stack API | BT Function | App |
---|---|---|
HCI_DisconnectCmd | Disconnect Command | N |
HCI_HostNumCompletedPktCmd | Host Number Of Completed Packets Command | N |
HCI_LE_AddDeviceToResolvingListCmd | LE Add Device to Resolving List Command | N |
HCI_LE_AddWhiteListCmd | LE Add Device To White List Command | Y |
HCI_LE_ClearWhiteListCmd | LE Clear White List Command | Y |
HCI_LE_ConnUpdateCmd | LE Connection Update Command | N |
HCI_LE_CreateConnCancelCmd | LE Create Connection Cancel Command | N |
HCI_LE_CreateConnCmd | LE Create Connection Command | N |
HCI_LE_EncryptCmd | LE Encrypt Command | Y |
HCI_LE_GenerateDHKeyCmd | LE Generate DHKey Command | N |
HCI_LE_LtkReqNegReplyCmd | LE Long Term Key Request Negative Reply Command | N |
HCI_LE_LtkReqReplyCmd | LE Long Term Key Request Reply Command | N |
HCI_LE_RandCmd | LE Rand Command | N |
HCI_LE_ReadAdvChanTxPowerCmd | Read Transmit Power Level Command | Y |
HCI_LE_ReadBufSizeCmd | LE Read Buffer Size Command | N |
HCI_LE_ReadChannelMapCmd | LE Read Channel Map Command | Y |
HCI_LE_ReadLocalP256PublicKeyCmd | LE Read Local P-256 Public Key Command | N |
HCI_LE_ReadLocalResolvableAddressCmd | LE Read Local Resolvable Address Command | N |
HCI_LE_ReadLocalSupportedFeaturesCmd | Read Local Supported Commands Command | Y |
HCI_LE_ReadMaxDataLenCmd | Set Event Mask Command | Y |
HCI_LE_ReadPeerResolvableAddressCmd | LE Read Peer Resolvable Address Command | N |
HCI_LE_ReadRemoteUsedFeaturesCmd | LE Read Remote Used Features Command | Y |
HCI_LE_ReadResolvingListSizeCmd | LE Read Resolving List Size Command | N |
HCI_LE_ReadSuggestedDefaultDataLenCmd | LE Read Suggested Default Data Length Command | Y |
HCI_LE_ReadSupportedStatesCmd | LE Read Supported States Command | Y |
HCI_LE_ReadWhiteListSizeCmd | LE Read White List Size Command | Y |
HCI_LE_RemoteConnParamReqNegReplyCmd | LE Remote Connection Parameter Request Negative Reply Command | N |
HCI_LE_RemoteConnParamReqReplyCmd | LE Remote Connection Parameter Request Reply Command | N |
HCI_LE_RemoveDeviceFromResolvingListCmd | LE Remove Device From Resolving List Command | N |
HCI_LE_RemoveWhiteListCmd | LE Remove Device From White List Command | Y |
HCI_LE_SetAddressResolutionEnableCmd | LE Set Address Resolution Enable Command | N |
HCI_LE_SetAdvDataCmd | LE Set Advertising Data Command | N |
HCI_LE_SetAdvEnableCmd | LE Set Advertise Enable Command | N |
HCI_LE_SetDataLenCmd | LE Set Data Length Command | Y |
HCI_LE_SetEventMaskCmd | LE Set Event Mask Command | Y |
HCI_LE_SetHostChanClassificationCmd | LE Set Host Channel Classification Command | Y |
HCI_LE_SetRandomAddressCmd | LE Set Random Address Command | N |
HCI_LE_SetResolvablePrivateAddressTimeoutCmd | LE Set Resolvable Private Address Timeout Command | N |
HCI_LE_SetScanEnableCmd | LE Set Scan Enable Command | N |
HCI_LE_SetScanParamCmd | LE Set Scan Parameters Command | N |
HCI_LE_SetAdvDataCmd | LE Set Advertising Data Command | N |
HCI_LE_SetAdvEnableCmd | LE Set Advertise Enable Command | N |
HCI_LE_SetAdvParamCmd | LE Set Advertising Parameters Command | N |
HCI_LE_SetScanRspDataCmd | LE Set Scan Response Data Command | N |
HCI_LE_StartEncyptCmd | LE Start Encryption Command | N |
HCI_LE_TestEndCmd | LE Test End Command | Y |
HCI_LE_TransmitterTestCmd | LE Transmitter Test Command | Y |
HCI_LE_WriteSuggestedDefaultDataLenCmd | LE Write Suggested Default Data Length Command | Y |
HCI_ReadAuthPayloadTimeoutCmd | Read Authenticated Payload Timeout Command | N |
HCI_ReadBDADDRCmd | Read BD_ADDR Command | Y |
HCI_ReadLocalSupportedCommandsCmd | Read Local Supported Commands Command | Y |
HCI_ReadLocalSupportedFeaturesCmd | Read Local Supported Features Command | Y |
HCI_ReadLocalVersionInfoCmd | Read Local Version Information Command | Y |
HCI_ReadRemoteVersionInfoCmd | Read Remote Version Information Command | Y |
HCI_ReadRssiCmd | Read RSSI Command | Y |
HCI_ReadTransmitPowerLevelCmd | Read Transmit Power Level Command | Y |
HCI_ResetCmd | Reset Command | Y |
HCI_SetEventMaskCmd | Set Event Mask Command | Y |
HCI_SetEventMaskPage2Cmd | Set Event Mask Page 2 Command | Y |
This section lists the mapping between stack APIs and function names, as described in the Vendor Specific API guide included with the installer.
Stack API | Vendor Specific Function |
---|---|
HCI_EXT_AdvEventNoticeCmd | HCI Extension Advertiser Event Notice |
HCI_EXT_BuildRevisionCmd | HCI Extension Build Revision |
HCI_EXT_DecryptCmd | HCI Extension Decrypt |
HCI_EXT_DisconnectImmedCmd | HCI Extension Disconnect Immediate |
HCI_EXT_EnablePTMCmd | HCI Extension Enable PTM |
HCI_EXT_EndModemTestCmd | Set Event Mask Command |
HCI_EXT_EndModemTestCmd | HCI Extension End Modem Test |
HCI_EXT_ModemHopTestTxCmd | HCI Extension Modem Hop Test Transmit |
HCI_EXT_ModemTestRxCmd | HCI Extension Modem Test Receive |
HCI_EXT_ModemTestTxCmd | HCI Extension Modem Test Transmit |
HCI_EXT_NumComplPktsLimitCmd | HCI Extension Number Completed Packets Limit |
HCI_EXT_OnePktPerEvtCmd | HCI Extension One Packet Per Event |
HCI_EXT_PacketErrorRateCmd | HCI Extension Packet Error Rate |
HCI_EXT_PERbyChanCmd | HCI Extension Packet Error Rate By Channel |
HCI_EXT_SaveFreqTuneCmd | HCI Extension Save Frequency Tuning |
HCI_EXT_ScanEventNoticeCmd | HCI Extension Scan Event Notice |
HCI_EXT_ScanReqRptCmd | HCI Extension Scan Request Report |
HCI_EXT_SetBDADDRCmd | HCI Extension Set BDADDR |
HCI_EXT_SetFastTxResponseTimeCmd | HCI Extension Set Fast Transmit Response Time |
HCI_EXT_SetFreqTuneCmd | HCI Extension Set Frequency Tuning |
HCI_EXT_SetLocalSupportedFeaturesCmd | HCI Extension Set Local Supported Features |
HCI_EXT_SetMaxDataLenCmd | HCI Extension Set Max Data Length |
HCI_EXT_SetMaxDtmTxPowerCmd | HCI Extension Set Max DTM Transmitter Power |
HCI_EXT_SetRxGainCmd | HCI Extension Set Receiver Gain |
HCI_EXT_SetSCACmd | HCI Extension Set SCA |
HCI_EXT_SetTxPowerCmd | HCI Extension Set Transmitter Power |
HCI_EXT_SetScanChannels | HCI Extension Set Scan Channels |