Instance: AON_RTC
Component: AON_RTC
Base address: 0x40092000
This component control the Real Time Clock residing in AON
Note: This module is only supporting 32 bit ReadWrite access.
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x4009 2000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4009 2004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x4009 2008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x4009 200C |
|
RO |
32 |
0x0080 0000 |
0x0000 0010 |
0x4009 2010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x4009 2014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x4009 2018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x4009 201C |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x4009 2020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x4009 2024 |
|
RO |
32 |
0x0000 0000 |
0x0000 0028 |
0x4009 2028 |
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x4009 202C |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x4009 2000 | Instance | 0x4009 2000 |
Description | Control This register contains various bitfields for configuration of RTC |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||||||||||||||||||||
31:19 | RESERVED19 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 | |||||||||||||||||||||||||||||||||||||||||||||||
18:16 | COMB_EV_MASK | Eventmask selecting which delayed events that form the combined event.
|
RW | 0b000 | |||||||||||||||||||||||||||||||||||||||||||||||
15:12 | RESERVED12 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | |||||||||||||||||||||||||||||||||||||||||||||||
11:8 | EV_DELAY | Number of SCLK_LF clock cycles waited before generating delayed events. (Common setting for all RTC cannels) the delayed event is delayed
|
RW | 0x0 | |||||||||||||||||||||||||||||||||||||||||||||||
7 | RESET | RTC Counter reset. Writing 1 to this bit will reset the RTC counter. This bit is cleared when reset takes effect |
WO | 0 | |||||||||||||||||||||||||||||||||||||||||||||||
6:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | |||||||||||||||||||||||||||||||||||||||||||||||
2 | RTC_4KHZ_EN | RTC_4KHZ is a 4 KHz reference output, tapped from SUBSEC.VALUE bit 19 which is used by AUX timer. 0: RTC_4KHZ signal is forced to 0 1: RTC_4KHZ is enabled ( provied that RTC is enabled EN) |
RW | 0 | |||||||||||||||||||||||||||||||||||||||||||||||
1 | RTC_UPD_EN | RTC_UPD is a 16 KHz signal used to sync up the radio timer. The 16 Khz is SCLK_LF divided by 2 0: RTC_UPD signal is forced to 0 1: RTC_UPD signal is toggling @16 kHz |
RW | 0 | |||||||||||||||||||||||||||||||||||||||||||||||
0 | EN | Enable RTC counter 0: Halted (frozen) 1: Running |
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4009 2004 | Instance | 0x4009 2004 |
Description | Event Flags, RTC Status This register contains event flags from the 3 RTC channels. Each flag will be cleared when writing a '1' to the corresponding bitfield. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 | ||
16 | CH2 | Channel 2 event flag, set when CHCTL.CH2_EN = 1 and the RTC value matches or passes the CH2CMP value. An event will be scheduled to occur as soon as possible when writing to CH2CMP provided that the channel is enabled and the new value matches any time between next RTC value and 1 second in the past Writing 1 clears this flag. Note that a new event can not occur on this channel in first 2 SCLK_LF cycles after a clearance. AUX_SCE can read the flag through AUX_WUC:WUEVFLAGS.AON_RTC_CH2 and clear it using AUX_WUC:WUEVCLR.AON_RTC_CH2. |
RW | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | CH1 | Channel 1 event flag, set when CHCTL.CH1_EN = 1 and one of the following: - CHCTL.CH1_CAPT_EN = 0 and the RTC value matches or passes the CH1CMP value. - CHCTL.CH1_CAPT_EN = 1 and capture occurs. An event will be scheduled to occur as soon as possible when writing to CH1CMP provided that the channel is enabled, in compare mode and the new value matches any time between next RTC value and 1 second in the past. Writing 1 clears this flag. Note that a new event can not occur on this channel in first 2 SCLK_LF cycles after a clearance. |
RW | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | CH0 | Channel 0 event flag, set when CHCTL.CH0_EN = 1 and the RTC value matches or passes the CH0CMP value. An event will be scheduled to occur as soon as possible when writing to CH0CMP provided that the channels is enabled and the new value matches any time between next RTC value and 1 second in the past. Writing 1 clears this flag. Note that a new event can not occur on this channel in first 2 SCLK_LF cycles after a clearance. |
RW | 0 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x4009 2008 | Instance | 0x4009 2008 |
Description | Second Counter Value, Integer Part | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VALUE | Unsigned integer representing Real Time Clock in seconds. When reading this register the content of SUBSEC.VALUE is simultaneously latched. A consistent reading of the combined Real Time Clock can be obtained by first reading this register, then reading SUBSEC register. |
RW | 0x0000 0000 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x4009 200C | Instance | 0x4009 200C |
Description | Second Counter Value, Fractional Part | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VALUE | Unsigned integer representing Real Time Clock in fractions of a second (VALUE/2^32 seconds) at the time when SEC register was read. Examples : - 0x0000_0000 = 0.0 sec - 0x4000_0000 = 0.25 sec - 0x8000_0000 = 0.5 sec - 0xC000_0000 = 0.75 sec |
RW | 0x0000 0000 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x4009 2010 | Instance | 0x4009 2010 |
Description | Subseconds Increment Value added to SUBSEC.VALUE on every SCLK_LFclock cycle. |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:24 | RESERVED24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 | ||
23:0 | VALUEINC | This value compensates for a SCLK_LF clock which has an offset from 32768 Hz. The compensation value can be found as 2^38 / freq, where freq is SCLK_LF clock frequency in Hertz This value is added to SUBSEC.VALUE on every cycle, and carry of this is added to SEC.VALUE. To perform the addition, bits [23:6] are aligned with SUBSEC.VALUE bits [17:0]. The remaining bits [5:0] are accumulated in a hidden 6-bit register that generates a carry into the above mentioned addition on overflow. The default value corresponds to incrementing by precisely 1/32768 of a second. NOTE: This register is read only. Modification of the register value must be done using registers AUX_WUC:RTCSUBSECINC1 , AUX_WUC:RTCSUBSECINC0 and AUX_WUC:RTCSUBSECINCCTL |
RO | 0x80 0000 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x4009 2014 | Instance | 0x4009 2014 |
Description | Channel Configuration | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:19 | RESERVED19 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 | ||
18 | CH2_CONT_EN | Set to enable continuous operation of Channel 2 | RW | 0 | ||
17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||
16 | CH2_EN | RTC Channel 2 Enable 0: Disable RTC Channel 2 1: Enable RTC Channel 2 |
RW | 0 | ||
15:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 | ||
9 | CH1_CAPT_EN | Set Channel 1 mode 0: Compare mode (default) 1: Capture mode |
RW | 0 | ||
8 | CH1_EN | RTC Channel 1 Enable 0: Disable RTC Channel 1 1: Enable RTC Channel 1 |
RW | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | CH0_EN | RTC Channel 0 Enable 0: Disable RTC Channel 0 1: Enable RTC Channel 0 |
RW | 0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x4009 2018 | Instance | 0x4009 2018 |
Description | Channel 0 Compare Value | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VALUE | RTC Channel 0 compare value. Bit 31 to 16 represents seconds and bits 15 to 0 represents subseconds of the compare value. The compare value is compared against SEC.VALUE (15:0) and SUBSEC.VALUE (31:16) values of the Real Time Clock register. A Cannel 0 event is generated when {SEC.VALUE(15:0),SUBSEC.VALUE (31:16)} is reaching or exciting the compare value. Writing to this register can trigger an immediate*) event in case the new compare value matches a Real Time Clock value from 1 second in the past up till current Real Time Clock value. Example: To generate a compare 5.5 seconds RTC start,- set this value = 0x0005_8000 *) It can take up to 2 SCLK_LF clock cycles before event occurs due to synchronization. |
RW | 0x0000 0000 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x4009 201C | Instance | 0x4009 201C |
Description | Channel 1 Compare Value | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VALUE | RTC Channel 1 compare value. Bit 31 to 16 represents seconds and bits 15 to 0 represents subseconds of the compare value. The compare value is compared against SEC.VALUE (15:0) and SUBSEC.VALUE (31:16) values of the Real Time Clock register. A Cannel 0 event is generated when {SEC.VALUE(15:0),SUBSEC.VALUE (31:16)} is reaching or exciting the compare value. Writing to this register can trigger an immediate*) event in case the new compare value matches a Real Time Clock value from 1 second in the past up till current Real Time Clock value. Example: To generate a compare 5.5 seconds RTC start,- set this value = 0x0005_8000 *) It can take up to 2 SCLK_LF clock cycles before event occurs due to synchronization. |
RW | 0x0000 0000 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0x4009 2020 | Instance | 0x4009 2020 |
Description | Channel 2 Compare Value | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VALUE | RTC Channel 2 compare value. Bit 31 to 16 represents seconds and bits 15 to 0 represents subseconds of the compare value. The compare value is compared against SEC.VALUE (15:0) and SUBSEC.VALUE (31:16) values of the Real Time Clock register. A Cannel 0 event is generated when {SEC.VALUE(15:0),SUBSEC.VALUE (31:16)} is reaching or exciting the compare value. Writing to this register can trigger an immediate*) event in case the new compare value matches a Real Time Clock value from 1 second in the past up till current Real Time Clock value. Example: To generate a compare 5.5 seconds RTC start,- set this value = 0x0005_8000 *) It can take up to 2 SCLK_LF clock cycles before event occurs due to synchronization. |
RW | 0x0000 0000 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x4009 2024 | Instance | 0x4009 2024 |
Description | Channel 2 Compare Value Auto-increment This register is primarily used to generate periodical wake-up for the AUX_SCE module, through the [AUX_EVCTL.EVSTAT0.AON_RTC] event. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | VALUE | If CHCTL.CH2_CONT_EN is set, this value is added to CH2CMP.VALUE on every channel 2 compare event. | RW | 0x0000 0000 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x4009 2028 | Instance | 0x4009 2028 |
Description | Channel 1 Capture Value If CHCTL.CH1_EN = 1and CHCTL.CH1_CAPT_EN = 1, capture occurs on each rising edge of the event selected in AON_EVENT:RTCSEL. |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:16 | SEC | Value of SEC.VALUE bits 15:0 at capture time. | RO | 0x0000 | ||
15:0 | SUBSEC | Value of SUBSEC.VALUE bits 31:16 at capture time. | RO | 0x0000 |
Address Offset | 0x0000 002C | ||
Physical Address | 0x4009 202C | Instance | 0x4009 202C |
Description | AON Synchronization This register is used for synchronizing between MCU and entire AON domain. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | WBUSY | This register will always return 0,- however it will not return the value until there are no outstanding write requests between MCU and AON Note: Writing to this register prior to reading will force a wait until next SCLK_LF edge. This is recommended for syncing read registers from AON when waking up from sleep Failure to do so may result in reading AON values from prior to going to sleep |
RW | 0 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |