TI Logo
SimpleLink™ CC2640R2 SDK Proprietary RF User's Guide
2.70.0
  • Proprietary RF Quick Start Guide
  • The SimpleLink CC2640R2 SDK Platform
  • Examples User’s Guide
  • Custom hardware
  • TI-RTOS (RTOS Kernel) Overview
  • noRTOS Overview
  • RF Core
  • Proprietary Physical Layer
  • EasyLink Layer
    • Overview
    • General Behavior
    • Error Handling
    • Supported Functions
    • EZLINKPROP-890 Workaround
      • 1) Exporting Commands from SmartRF Studio
      • 2) Update Project to use Exported Settings
      • 3) Update EasyLink
    • Frame Structure
  • Debugging
  • Memory overview
  • Over the Air Download (OAD)
  • Migration Guides
  • API References
  • Terms and acronyms




SimpleLink™ CC2640R2 SDK Proprietary RF User's Guide
  • »
  • EasyLink Layer

EasyLink Layer¶

Overview¶

The EasyLink API is a simple abstraction layer on top of the RF Driver and is intended as a starting point for customers creating a proprietary Sub-1 GHz protocol. The EasyLink layer does not support any regional RF conformance such as Listen Before Talk required for the license free frequency band. Customers need to add support for the regional conformance that their product requires under the EasyLink API.

The EasyLink Example can be found in the examples/{rtos or nortos}/{development board}/easylink folder. You can find descriptions of the examples in the Examples User’s Guide.

The EasyLink layer also supports a simple network processor configuration. This is showcased in the EasyLink Network Processor (NP) example project. Here, the EasyLink API has been exposed over an AT Command Interface such that it can be used by Host SW (running on a PC, MPU or MCU), or by using a serial terminal emulator over a UART. The specific commands can be found in the rfEasyLinkNp.

The EasyLink API should be used in application code. The EasyLink API is intended to abstract the RF Driver in order to give a simple API for customers to use as is or extend to suit their application use cases.

For API descriptions, see the EasyLink API Reference.

General Behavior¶

Before using the EasyLink API the EasyLink Layer is initialized by calling EasyLink_init(). This initializes and opens the RF driver and configures the modulation scheme passed to EasyLink_init.

RX is enabled by calling EasyLink_receive() or EasyLink_receiveAsync(). Entering RX can be immediate or scheduled by using the EasyLink_RxPacket::absTime field. EasyLink_receive() is blocking and EasyLink_receiveAsync() is nonblocking. The EasyLink API does not queue messages so calling another API function while in EasyLink_receiveAsync() will return EasyLink_Status_Busy_Error. An Asynchronous Rx operation can be canceled with EasyLink_abort().

TX is enabled by calling EasyLink_transmit() or EasyLink_transmitAsync(). TX can be immediate or scheduled by using the EasyLink_TxPacket::absTime field. EasyLink_transmit() is blocking and EasyLink_transmitAsync() is nonblocking. The EasyLink API does not queue messages so calling another API function while in EasyLink_transmitAsync() will return EasyLink_Status_Busy_Error An Asynchronous operation can be canceled with EasyLink_abort().

Error Handling¶

The EasyLink API will return EasyLink_Status containing success or error code.

The EasyLink_Status code are:

EasyLink_Status_Success
EasyLink_Status_Config_Error
EasyLink_Status_Param_Error
EasyLink_Status_Mem_Error
EasyLink_Status_Cmd_Error
EasyLink_Status_Tx_Error
EasyLink_Status_Rx_Error
EasyLink_Status_Rx_Timeout
EasyLink_Status_Busy_Error
EasyLink_Status_Aborted

Supported Functions¶

Generic API function Description
EasyLink_init() Inits and opens the RF driver and configures the specified modulation
EasyLink_transmit() Blocking Transmit
EasyLink_transmitAsync() Nonblocking Transmit
EasyLink_receive() Blocking Receive
EasyLink_receiveAsync() Nonblocking Receive
EasyLink_abort() Aborts a non blocking call
EasyLink_EnableRxAddrFilter() Enables/Disables RX filtering on the Addr
EasyLink_GetIeeeAddr() Gets the IEEE Address
EasyLink_SetFreq() Sets the frequency
EasyLink_GetFreq() Gets the frequency
EasyLink_SetRfPwr() Sets the Tx Power
EasyLink_GetRfPwr() Gets the Tx Power

EZLINKPROP-890 Workaround¶

Currently there is a known issue (EZLINKPROP-890) that causes all existing PHYs to be affected when exporting custom settings using SmartRF Studio. The custom settings are only meant to affect the “Custom” EasyLink PHY however, each pre-defined PHY currently shares TX and advanced RX commands with the custom settings. A three step workaround to this issue follows below.

1) Exporting Commands from SmartRF Studio¶

EasyLink requires an advanced RX command to support address filtering and clear channel assessment. This command is not exported by default for EasyLink supported PHYs via SmartRF Studio. To export the command:

  1. After selecting and modifying a desired PHY in SmartRF Studio, click “Code Export”.
  2. Select the “Command” view from the upper left corner of the pane that pops-up.
  3. Check the “Select commands individually” checkbox.
  4. Select CMD_PROP_RX_ADV and click the “>” arrow to add it to the list of exported commands.
  5. Save the generated files.

2) Update Project to use Exported Settings¶

In your project there will be two sets of SmartRF Settings; smartrf_settings_predefined.c/h and smartrf_settings.c/h. The pre-defined settings are used for all PHYs except the “Custom” EasyLink PHY whereas the non-prefined settings are used for the “Custom” PHY. The following modifications are needed to these files:

  1. Open the contents of the original smartrf_settings.c and copy the entirety of the rfc_CMD_PROP_TX_t command.
  2. Open the smartrf_settings_predefined.c file and paste the copied rfc_CMD_PROP_TX_t command at the bottom of the file.
  3. Rename the pasted rfc_CMD_PROP_TX_t command to from RF_cmdPropTx to RF_cmdPropTx_preDef.
  4. Open smartrf_settings_predefined.h and add extern rfc_CMD_PROP_TX_t RF_cmdPropTx_preDef; to the list of extern variables.
  5. Overwrite the contents of the original smartrf_settings.c/h files with the recently exported SmartRF Studio files.

3) Update EasyLink¶

EasyLink uses an array of “EasyLink_RfSetting” to access the individual RF commands for each PHY. This needs to be updated to use the recent changes made to the smartrf_settings files. In addition, the EasyLink source code needs to be modified for the recently exported advanced rx command to use the correct sync word:

  1. Open easylink_config.c and locate the EasyLink_supportedPhys array. Each individual PHY is surrounded by a guard macro indicating the PHY type.
  2. Locate the Custom PHY and modify the RF_pCmdPropRxAdv element to: .RF_pCmdPropRxAdv = &RF_cmdPropRxAdv,.
  3. Update all other RF_pCmdPropTx elements to RF_cmdPropTx_preDef except the Custom PHY: .RF_pCmdPropTx = &RF_cmdPropTx_preDef,.
  4. Open EasyLink.c or EasyLink_nortos.c depending on the projects RTOS support.
  5. Find the EasyLink_init() function implementation and the lines of code modifying elements of the EasyLink_cmdPropRxAdv structure.
  6. After the last line modifying this structure add the code snippet below. This will force the advanced RX command to use the same sync word as the TX command that was recently exported from SmartRF Studio:
if(EasyLink_Phy_Custom == EasyLink_params.ui32ModType)
{
   EasyLink_cmdPropRxAdv.syncWord0 = EasyLink_cmdPropTxAdv.syncWord;
}

Frame Structure¶

The EasyLink implements a basic header for transmitting and receiving data. This header supports addressing for a star or point-to-point network with acknowledgments.

Packet structure:

1B Length 1-64b Dst Address Payload
Next Previous

2016-2020, Texas Instruments, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale