GPIO.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2020, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!****************************************************************************
33  * @file GPIO.h
34  *
35  * @brief General Purpose I/O driver interface.
36  *
37  * The GPIO header file should be included in an application as follows:
38  * @code
39  * #include <ti/drivers/GPIO.h>
40  * @endcode
41  *
42  * # Overview #
43  * The GPIO module allows you to manage General Purpose I/O pins via simple
44  * and portable APIs. GPIO pin behavior is usually configured statically,
45  * but can also be configured or reconfigured at runtime.
46  *
47  * Because of its simplicity, the GPIO driver does not follow the model of
48  * other TI-RTOS drivers in which a driver application interface has
49  * separate device-specific implementations. This difference is most
50  * apparent in the GPIOxxx_Config structure, which does not require you to
51  * specify a particular function table or object.
52  *
53  * # Usage #
54  * This section provides a basic \ref ti_drivers_GPIO_Synopsis
55  * "usage summary" and a set of \ref ti_drivers_GPIO_Examples "examples"
56  * in the form of commented code fragments. Detailed descriptions of the
57  * GPIO APIs and their effect are provided in subsequent sections.
58  *
59  * @anchor ti_drivers_GPIO_Synopsis
60  * ### Synopsis #
61  * @anchor ti_drivers_GPIO_Synopsis_Code
62  * @code
63  * // Import GPIO Driver definitions
64  * #include <ti/drivers/GPIO.h>
65  *
66  * // Define names for GPIO pin indexes
67  * #define BUTTON 0
68  * #define LED 1
69  *
70  * // One-time init of GPIO driver
71  * GPIO_init();
72  *
73  * // Read GPIO pin
74  * unsigned int state = GPIO_read(BUTTON);
75  *
76  * // Write to GPIO pin
77  * GPIO_write(LED, state);
78  * @endcode
79  *
80  * @anchor ti_drivers_GPIO_Examples
81  * ### Examples #
82  * * @ref ti_drivers_GPIO_Example_callback "Creating an input callback"
83  * * @ref ti_drivers_GPIO_Example_reconfigure "Runtime pin configuration"
84  *
85  * @anchor ti_drivers_GPIO_Example_callback
86  * **Creating an input callback**: The following example demonstrates how
87  * to configure a GPIO pin to generate an interrupt and how to toggle an
88  * an LED on and off within the registered interrupt callback function.
89  * @code
90  * // Driver header file
91  * #include <ti/drivers/GPIO.h>
92  *
93  * // TI Drivers Configuration
94  * #include "ti_drivers_config.h"
95  * // Board file
96  * #include <ti/drivers/Board.h>
97  *
98  * // GPIO button call back function
99  * void gpioButton0Fxn(uint_least8_t index);
100  *
101  * main()
102  * {
103  * // One-time Board initialization
104  * Board_init();
105  *
106  * // One-time init of GPIO driver
107  * GPIO_init();
108  *
109  * // Turn on user LED
110  * GPIO_write(CONFIG_GPIO_LED0, CONFIG_GPIO_LED_ON);
111  *
112  * // install Button callback
113  * GPIO_setCallback(CONFIG_GPIO_BUTTON0, gpioButton0Fxn);
114  *
115  * // Enable interrupts
116  * GPIO_enableInt(CONFIG_GPIO_BUTTON0);
117  * }
118  *
119  * //
120  * // ======== gpioButton0Fxn ========
121  * // Callback function for the GPIO interrupt on CONFIG_GPIO_BUTTON0
122  * //
123  * // Note: index is the GPIO id for the button which is not used here
124  * //
125  * void gpioButton0Fxn(uint_least8_t index)
126  * {
127  * // Toggle the LED
128  * GPIO_toggle(CONFIG_GPIO_LED0);
129  * }
130  * @endcode
131  *
132  * @anchor ti_drivers_GPIO_Example_reconfigure
133  * **Runtime pin configuration**: The following example demonstrates how
134  * to (re)configure GPIO pins.
135  * @code
136  * // Driver header file
137  * #include <ti/drivers/GPIO.h>
138  *
139  * // TI Driver configuration
140  * #include "ti_drivers_config.h"
141  *
142  * #define LED CONFIG_GPIO_LED0
143  * #define BUTTON CONFIG_GPIO_BUTTON0
144  *
145  * void main()
146  * {
147  * // One-time init of GPIO driver
148  * GPIO_init();
149  *
150  * // Configure a button input pin
151  * GPIO_setConfig(BUTTON, GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING);
152  *
153  * // Configure an LED output pin
154  * GPIO_setConfig(LED, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
155  * }
156  * @endcode
157  *
158  * ### GPIO Driver Configuration #
159  *
160  * In order to use the GPIO APIs, the application is required
161  * to provide 3 structures in the ti_drivers_config.c file:
162  * 1. An array of @ref GPIO_PinConfig elements that defines the
163  * initial configuration of each pin used by the application. A
164  * pin is referenced in the application by its corresponding index in this
165  * array. The pin type (that is, INPUT/OUTPUT), its initial state (that is
166  * OUTPUT_HIGH or LOW), interrupt behavior (RISING/FALLING edge, etc.), and
167  * device specific pin identification are configured in each element
168  * of this array (see @ref GPIO_PinConfigSettings).
169  * Below is an MSP432 device specific example of the GPIO_PinConfig array:
170  * @code
171  * //
172  * // Array of Pin configurations
173  * //
174  * GPIO_PinConfig gpioPinConfigs[] = {
175  * // Input pins
176  * // MSP_EXP432P401R_GPIO_S1
177  * GPIOMSP432_P1_1 | GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING,
178  * // MSP_EXP432P401R_GPIO_S2
179  * GPIOMSP432_P1_4 | GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING,
180  *
181  * // Output pins
182  * // MSP_EXP432P401R_GPIO_LED1
183  * GPIOMSP432_P1_0 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
184  * // MSP_EXP432P401R_GPIO_LED_RED
185  * GPIOMSP432_P2_0 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
186  * };
187  * @endcode
188  *
189  * 2. An array of @ref GPIO_CallbackFxn elements that is used to store
190  * callback function pointers for GPIO pins configured with interrupts.
191  * The indexes for these array elements correspond to the pins defined
192  * in the GPIO_pinConfig array. These function pointers can be defined
193  * statically by referencing the callback function name in the array
194  * element, or dynamically, by setting the array element to NULL and using
195  * GPIO_setCallback() at runtime to plug the callback entry.
196  * Pins not used for interrupts can be omitted from the callback array to
197  * reduce memory usage (if they are placed at the end of GPIO_pinConfig
198  * array). The callback function syntax should match the following:
199  * @code
200  * void (*GPIO_CallbackFxn)(uint_least8_t index);
201  * @endcode
202  * The index parameter is the same index that was passed to
203  * GPIO_setCallback(). This allows the same callback function to be used
204  * for multiple GPIO interrupts, by using the index to identify the GPIO
205  * that caused the interrupt.
206  * @remark Callback functions are called in the context of an interrupt
207  * service routine and should be designed accordingly.
208  *
209  * When an interrupt is triggered, the interrupt status of all
210  * (interrupt enabled) pins on a port will be read, cleared, and the
211  * respective callbacks will be executed. Callbacks will be called in order
212  * from least significant bit to most significant bit.
213  * Below is an MSP432 device specific example of the GPIO_CallbackFxn array:
214  * @code
215  * //
216  * // Array of callback function pointers
217  * //
218  * GPIO_CallbackFxn gpioCallbackFunctions[] = {
219  * // MSP_EXP432P401R_GPIO_S1
220  * NULL,
221  * // MSP_EXP432P401R_GPIO_S2
222  * NULL
223  * };
224  * @endcode
225  *
226  * 3. A device specific GPIOxxx_Config structure that tells the GPIO
227  * driver where the two aforementioned arrays are and the number of elements
228  * in each. The interrupt priority of all pins configured to generate
229  * interrupts is also specified here. Values for the interrupt priority are
230  * device-specific. You should be well-acquainted with the interrupt
231  * controller used in your device before setting this parameter to a
232  * non-default value. The sentinel value of (~0) (the default value) is
233  * used to indicate that the lowest possible priority should be used.
234  * Below is an MSP432 device specific example of a GPIOxxx_Config
235  * structure:
236  * @code
237  * //
238  * // MSP432 specific GPIOxxx_Config structure
239  * //
240  * const GPIOMSP432_Config GPIOMSP432_config = {
241  * .pinConfigs = (GPIO_PinConfig *)gpioPinConfigs,
242  * .callbacks = (GPIO_CallbackFxn *)gpioCallbackFunctions,
243  * .numberOfPinConfigs = sizeof(gpioPinConfigs)/sizeof(GPIO_PinConfig),
244  * .numberOfCallbacks = sizeof(gpioCallbackFunctions)/sizeof(GPIO_CallbackFxn),
245  * .intPriority = (~0)
246  * };
247  * @endcode
248  *
249  * ### Initializing the GPIO Driver #
250  *
251  * GPIO_init() must be called before any other GPIO APIs. This function
252  * configures each GPIO pin in the user-provided @ref GPIO_PinConfig
253  * array according to the defined settings. The user can also reconfigure
254  * a pin dynamically after GPIO_init() is called by using the
255  * GPIO_setConfig(), and GPIO_setCallback() APIs.
256  *
257  * # Implementation #
258  *
259  * Unlike most other TI-RTOS drivers, the GPIO driver has no generic function
260  * table with pointers to device-specific API implementations. All the generic
261  * GPIO APIs are implemented by the device-specific GPIO driver module.
262  * Additionally, there is no notion of an instance 'handle' with the GPIO
263  * driver.
264  *
265  * GPIO pins are referenced by their numeric index in the GPIO_PinConfig
266  * array. This design approach was used to enhance runtime and memory
267  * efficiency.
268  *
269  ******************************************************************************
270  */
271 
272 #ifndef ti_drivers_GPIO__include
273 #define ti_drivers_GPIO__include
274 
275 #include <stdint.h>
276 
277 #ifdef __cplusplus
278 extern "C" {
279 #endif
280 
299 #define GPIO_STATUS_RESERVED (-32)
300 
307 #define GPIO_STATUS_SUCCESS (0)
308 
315 #define GPIO_STATUS_ERROR (-1)
316 
327 typedef uint32_t GPIO_PinConfig;
328 
333 #define GPIO_CFG_IO_MASK 0x00ff0000
334 #define GPIO_CFG_IO_LSB 16
335 #define GPIO_CFG_OUT_TYPE_MASK 0x00060000
336 #define GPIO_CFG_OUT_TYPE_LSB 17
337 #define GPIO_CFG_IN_TYPE_MASK 0x00060000
338 #define GPIO_CFG_IN_TYPE_LSB 17
339 #define GPIO_CFG_OUT_STRENGTH_MASK 0x00f00000
340 #define GPIO_CFG_OUT_STRENGTH_LSB 20
341 #define GPIO_CFG_INT_MASK 0x07000000
342 #define GPIO_CFG_INT_LSB 24
343 #define GPIO_CFG_OUT_BIT 19
344 
353 #define GPIO_CFG_OUTPUT (((uint32_t) 0) << GPIO_CFG_IO_LSB)
354 #define GPIO_CFG_OUT_STD (((uint32_t) 0) << GPIO_CFG_IO_LSB)
355 #define GPIO_CFG_OUT_OD_NOPULL (((uint32_t) 2) << GPIO_CFG_IO_LSB)
356 #define GPIO_CFG_OUT_OD_PU (((uint32_t) 4) << GPIO_CFG_IO_LSB)
357 #define GPIO_CFG_OUT_OD_PD (((uint32_t) 6) << GPIO_CFG_IO_LSB)
359 #define GPIO_CFG_OUT_STR_LOW (((uint32_t) 0) << GPIO_CFG_OUT_STRENGTH_LSB)
360 #define GPIO_CFG_OUT_STR_MED (((uint32_t) 1) << GPIO_CFG_OUT_STRENGTH_LSB)
361 #define GPIO_CFG_OUT_STR_HIGH (((uint32_t) 2) << GPIO_CFG_OUT_STRENGTH_LSB)
363 #define GPIO_CFG_OUT_HIGH (((uint32_t) 1) << GPIO_CFG_OUT_BIT)
364 #define GPIO_CFG_OUT_LOW (((uint32_t) 0) << GPIO_CFG_OUT_BIT)
370 #define GPIO_CFG_INPUT (((uint32_t) 1) << GPIO_CFG_IO_LSB)
371 #define GPIO_CFG_IN_NOPULL (((uint32_t) 1) << GPIO_CFG_IO_LSB)
372 #define GPIO_CFG_IN_PU (((uint32_t) 3) << GPIO_CFG_IO_LSB)
373 #define GPIO_CFG_IN_PD (((uint32_t) 5) << GPIO_CFG_IO_LSB)
379 #define GPIO_CFG_IN_INT_NONE (((uint32_t) 0) << GPIO_CFG_INT_LSB)
380 #define GPIO_CFG_IN_INT_FALLING (((uint32_t) 1) << GPIO_CFG_INT_LSB)
381 #define GPIO_CFG_IN_INT_RISING (((uint32_t) 2) << GPIO_CFG_INT_LSB)
382 #define GPIO_CFG_IN_INT_BOTH_EDGES (((uint32_t) 3) << GPIO_CFG_INT_LSB)
383 #define GPIO_CFG_IN_INT_LOW (((uint32_t) 4) << GPIO_CFG_INT_LSB)
384 #define GPIO_CFG_IN_INT_HIGH (((uint32_t) 5) << GPIO_CFG_INT_LSB)
395 #define GPIO_CFG_IN_INT_ONLY (((uint32_t) 1) << 27)
401 #define GPIO_DO_NOT_CONFIG 0x40000000
415 typedef void (*GPIO_CallbackFxn)(uint_least8_t index);
416 
427 extern void GPIO_clearInt(uint_least8_t index);
428 
436 extern void GPIO_disableInt(uint_least8_t index);
437 
451 extern void GPIO_enableInt(uint_least8_t index);
452 
464 extern void GPIO_getConfig(uint_least8_t index, GPIO_PinConfig *pinConfig);
465 
476 extern void GPIO_init();
477 
488 extern uint_fast8_t GPIO_read(uint_least8_t index);
489 
511 extern void GPIO_setCallback(uint_least8_t index, GPIO_CallbackFxn callback);
512 
526 extern int_fast16_t GPIO_setConfig(uint_least8_t index,
527  GPIO_PinConfig pinConfig);
528 
534 extern void GPIO_toggle(uint_least8_t index);
535 
542 extern void GPIO_write(uint_least8_t index, unsigned int value);
543 
544 #ifdef __cplusplus
545 }
546 #endif
547 
548 #endif /* ti_drivers_GPIO__include */
void GPIO_write(uint_least8_t index, unsigned int value)
Writes the value to a GPIO pin.
void GPIO_clearInt(uint_least8_t index)
Clear a GPIO pin interrupt flag.
void GPIO_toggle(uint_least8_t index)
Toggles the current state of a GPIO.
void GPIO_enableInt(uint_least8_t index)
Enable a GPIO pin interrupt.
uint32_t GPIO_PinConfig
GPIO pin configuration settings.
Definition: GPIO.h:327
void GPIO_getConfig(uint_least8_t index, GPIO_PinConfig *pinConfig)
Get the current configuration for a gpio pin.
void GPIO_init()
Initializes the GPIO module.
int_fast16_t GPIO_setConfig(uint_least8_t index, GPIO_PinConfig pinConfig)
Configure the gpio pin.
void GPIO_setCallback(uint_least8_t index, GPIO_CallbackFxn callback)
Bind a callback function to a GPIO pin interrupt.
uint_fast8_t GPIO_read(uint_least8_t index)
Reads the value of a GPIO pin.
void GPIO_disableInt(uint_least8_t index)
Disable a GPIO pin interrupt.
void(* GPIO_CallbackFxn)(uint_least8_t index)
GPIO callback function type.
Definition: GPIO.h:415
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale