22 #ifndef GAP_ADVERTISER_H 23 #define GAP_ADVERTISER_H 52 #define GAPADV_PARAMS_LEGACY_SCANN_CONN { \ 54 .eventProps = GAP_ADV_PROP_CONNECTABLE | GAP_ADV_PROP_SCANNABLE | \ 55 GAP_ADV_PROP_LEGACY, \ 58 .primChanMap = GAP_ADV_CHAN_ALL, \ 59 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 60 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 61 .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \ 62 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 63 .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \ 64 .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \ 69 #define GAPADV_PARAMS_AE_LONG_RANGE_CONN { \ 71 .eventProps = GAP_ADV_PROP_CONNECTABLE, \ 74 .primChanMap = GAP_ADV_CHAN_ALL, \ 75 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 76 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 77 .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \ 78 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 79 .primPhy = GAP_ADV_PRIM_PHY_CODED_S2, \ 80 .secPhy = GAP_ADV_SEC_PHY_CODED_S2, \ 85 #define GAPADV_PARAMS_AE_NC_NS { \ 89 .primChanMap = GAP_ADV_CHAN_ALL, \ 90 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 91 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 92 .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \ 93 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 94 .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \ 95 .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \ 304 #define GAP_ADV_INVALID_HANDLE 0xFF 395 #define GAP_ADV_TX_POWER_NO_PREFERENCE 127 460 GAP_ADV_EVT_MASK_RESERVED = BV(15)
469 #define GAPADV_PERIODIC_ADV_INTERVAL_MIN 0x0006 471 #define GAPADV_PERIODIC_ADV_INTERVAL_MAX 0xFFFF 473 #define GAPADV_PERIODIC_ADV_ENABLE_TX_POWER 0x0040 475 #define GAPADV_PERIODIC_ADV_DISABLE_TX_POWER 0x0000 477 #define GAPADV_PERIODIC_ADV_DATA_INTERMIDIATE_FRAG 0x00 479 #define GAPADV_PERIODIC_ADV_DATA_FIRST_FRAG 0x01 481 #define GAPADV_PERIODIC_ADV_DATA_LAST_FRAG 0x02 483 #define GAPADV_PERIODIC_ADV_DATA_COMPLETE 0x03 485 #define GAPADV_PERIODIC_ADV_MAX_DATA_LEN 252 559 uint16 periodicAdvIntervalMin;
560 uint16 periodicAdvIntervalMax;
561 uint16 periodicAdvProp;
562 } GapAdv_periodicAdvParams_t;
576 } GapAdv_periodicAdvData_t;
583 } GapAdv_periodicAdvEvt_t;
592 } GapAdv_dataUpdateEvent_t;
598 } GapAv_setAdvStatusDoneEvent_t;
657 GapAdv_freeBufferOptions_t freeOptions);
694 GapAdv_enableOptions_t enableOptions,
695 uint16 durationOrMaxEvents);
775 void *pValue, uint8_t *pLen);
795 uint16 *pLen, uint8 **ppBuf);
856 GapAdv_freeBufferOptions_t freeOptions);
903 uint16 len, uint8 *pBuf);
1026 uint8_t GapAdv_SetPeriodicAdvParams( uint8 advHandle,
1027 GapAdv_periodicAdvParams_t *periodicAdvParams );
1045 bStatus_t GapAdv_SetPeriodicAdvData( uint8 advHandle,
1046 GapAdv_periodicAdvData_t *periodicAdvData );
1064 bStatus_t GapAdv_SetPeriodicAdvEnable( uint8 enable,
Omit advertiser's address from PDU's.
Definition: gap_advertiser.h:315
uint32_t primIntMax
GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
Definition: gap_advertiser.h:512
This API allows the software components in the Z-Stack to be written independently of the specifics o...
All Channels.
Definition: gap_advertiser.h:365
GAP_Peer_Addr_Types_t
Address types used for specifying peer address type.
Definition: gap.h:727
coded-s2
Definition: gap_advertiser.h:402
Channels 37 & 39.
Definition: gap_advertiser.h:361
bStatus_t GapAdv_setParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue)
bStatus_t GapAdv_getParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue, uint8_t *pLen)
Definition: gap_advertiser.h:291
uint32_t primIntMin
GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
Definition: gap_advertiser.h:511
bStatus_t GapAdv_prepareLoadByHandle(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
GapAdv_freeBufferOptions_t
Possible free options for Gap Advertiser API's.
Definition: gap_advertiser.h:328
Definition: gap_advertiser.h:450
1 mbps
Definition: gap_advertiser.h:400
Definition: gap_advertiser.h:223
bStatus_t GapAdv_loadByHandle(uint8 handle, GapAdv_dataTypes_t dataType, uint16 len, uint8 *pBuf)
Definition: gap_advertiser.h:316
Directed advertising.
Definition: gap_advertiser.h:312
bStatus_t GapAdv_abortLoad(void)
bStatus_t GapAdv_setVirtualAdvAddr(uint8 advHandle, uint8 *bdAddr)
Definition: gap_advertiser.h:438
bStatus_t GapAdv_enable(uint8 handle, GapAdv_enableOptions_t enableOptions, uint16 durationOrMaxEvents)
Data type returned with GAP_EVT_ADV_DATA_TRUNCATED event.
Definition: gap_advertiser.h:544
int8 rssi
RSSI of the scan req.
Definition: gap_advertiser.h:540
Scannable advertising.
Definition: gap_advertiser.h:311
uint16_t eventProps
GAP_ADV_PARAM_PROPS
Definition: gap_advertiser.h:510
Free the scan response data.
Definition: gap_advertiser.h:332
uint8 channel
Channel when the scan req was received.
Definition: gap_advertiser.h:539
GapAdv_enableOptions_t
Enable options for GapAdv_enable.
Definition: gap_advertiser.h:336
Definition: gap_advertiser.h:426
GapAdv_ParamId_t
Definition: gap_advertiser.h:159
Definition: gap_advertiser.h:377
1 mbps
Definition: gap_advertiser.h:408
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:527
Don't free anything.
Definition: gap_advertiser.h:330
Definition: gap_advertiser.h:277
Channels 38 & 39.
Definition: gap_advertiser.h:363
bStatus_t GapAdv_disable(uint8 handle)
Disable an active advertising set.
void(* pfnGapCB_t)(uint32_t event, void *pBuf, uintptr_t arg)
Definition: gap.h:1324
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:546
Definition: gap_advertiser.h:232
GapAdv_secondaryPHY_t secPhy
GAP_ADV_PARAM_SECONDARY_PHY
Definition: gap_advertiser.h:519
2 mbps
Definition: gap_advertiser.h:409
Scan response data.
Definition: gap_advertiser.h:324
bStatus_t GapAdv_setEventMask(uint8 handle, GapAdv_eventMaskFlags_t mask)
GapAdv_secondaryPHY_t
Gap Advertiser Options for advertising on the secondary PHY.
Definition: gap_advertiser.h:406
bStatus_t GapAdv_create(pfnGapCB_t *cb, GapAdv_params_t *advParam, uint8 *advHandle)
Definition: gap_advertiser.h:446
Definition: gap_advertiser.h:253
GapAdv_advChannels_t
GAP Advertiser Defines for Advertiser Channels.
Definition: gap_advertiser.h:354
Definition: gap_advertiser.h:193
Channels 37 & 38.
Definition: gap_advertiser.h:359
GAP_Peer_Addr_Types_t peerAddrType
GAP_ADV_PARAM_PEER_ADDRESS_TYPE
Definition: gap_advertiser.h:514
GapAdv_eventMaskFlags_t
Definition: gap_advertiser.h:421
Advertising data.
Definition: gap_advertiser.h:323
GapAdv_primaryPHY_t
Gap Advertiser Options for advertising on the primary PHY.
Definition: gap_advertiser.h:398
Definition: gap_advertiser.h:350
Type definitions and macros for BLE stack.
Channel 37.
Definition: gap_advertiser.h:356
Definition: gap_advertiser.h:179
Connectable advertising.
Definition: gap_advertiser.h:310
Free the advertising data.
Definition: gap_advertiser.h:331
Definition: gap_advertiser.h:346
bStatus_t GapAdv_getBuffer(uint8 handle, GapAdv_dataTypes_t dataType, uint16 *pLen, uint8 **ppBuf)
coded-s2
Definition: gap_advertiser.h:411
Definition: gap_advertiser.h:265
Definition: gap_advertiser.h:387
Definition: gap_advertiser.h:434
uint16 connHandle
Connection handle that ended advertising.
Definition: gap_advertiser.h:529
OSAL Event Header.
Definition: osal.h:92
Definition: gap_advertiser.h:430
coded-s8
Definition: gap_advertiser.h:410
GapAdv_filterPolicy_t filterPolicy
GAP_ADV_PARAM_FILTER_POLICY
Definition: gap_advertiser.h:516
GapAdv_advChannels_t primChanMap
GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP
Definition: gap_advertiser.h:513
Use legacy advertising PDU's.
Definition: gap_advertiser.h:314
GapAdv_dataTypes_t
Gap Advertising Data Types.
Definition: gap_advertiser.h:321
Definition: gap_advertiser.h:342
uint8 scanAddrType
Address type of scanning device.
Definition: gap_advertiser.h:537
uint16 advDataLen
Definition: gap_advertiser.h:551
int8_t txPower
NOT CURRENTLY IMPLEMENTED.
Definition: gap_advertiser.h:517
Data type returned with GAP_EVT_ADV_SET_TERMINATED event.
Definition: gap_advertiser.h:525
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
Definition: gap_advertiser.h:168
Definition: gap_advertiser.h:508
Definition: gap_advertiser.h:442
High Duty Cycle Directed Advertising.
Definition: gap_advertiser.h:313
Definition: gap_advertiser.h:382
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:251
Definition: gap_advertiser.h:391
Definition: gap_advertiser.h:214
GapAdv_filterPolicy_t
GAP Advertiser White List Policy.
Definition: gap_advertiser.h:371
bStatus_t GapAdv_prepareLoadByBuffer(uint8 *pBuf, bool freeOldData)
bStatus_t GapAdv_loadByBuffer(uint16 len, uint8 *pBuf)
Channel 39.
Definition: gap_advertiser.h:358
bStatus_t GapAdv_destroy(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:536
GapAdv_eventProps_t
GAP Advertising Event Param Properties.
Definition: gap_advertiser.h:308
coded-s8
Definition: gap_advertiser.h:401
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.
Definition: gap_advertiser.h:534
Channel 38.
Definition: gap_advertiser.h:357
GapAdv_primaryPHY_t primPhy
GAP_ADV_PARAM_PRIMARY_PHY
Definition: gap_advertiser.h:518
uint8_t sid
GAP_ADV_PARAM_SID
Definition: gap_advertiser.h:520
uint8 status
TODO.
Definition: gap_advertiser.h:528
uint8 numCompAdvEvts
Number of completed advertising events.
Definition: gap_advertiser.h:530
Definition: gap_advertiser.h:205
uint8 availAdvDataLen
How many bytes of the advertising data were sent.
Definition: gap_advertiser.h:547