![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.03.01.00
|
Modules | |
| Micro BLE Stack Callbacks | |
| Micro BLE Stack Constants | |
| Micro BLE Stack Structures | |
Files | |
| file | uble.h |
| This file contains configuration, initialization, and parameter management of Micro BLE Stack. It also contains interfacing between Micro BLE Stack and the application. | |
Macros | |
| #define | BLE_LOG_INT_INT(handle, type, format, param1, param2) |
| #define | BLE_LOG_INT_STR(handle, type, format, param1, param2) |
| #define | BLE_LOG_INT_TIME(handle, type, start_str, param1) |
Functions | |
| bStatus_t | uble_checkAddr (ubleAddrType_t addrType, uint8 *pAddr) |
| Check if the given address is valid. More... | |
| bStatus_t | uble_getAddr (ubleAddrType_t addrType, uint8 *pAddr) |
| Retrieve the address corresponding to the given address type. More... | |
| bStatus_t | uble_getParameter (uint8 param, void *pValue) |
| Get a Micro BLE Stack parameter. More... | |
| void | uble_processMsg (void) |
| Let the Micro Stack process the queued messages. More... | |
| bStatus_t | uble_registerAntSwitchCB (ubleAntSwitchCB_t pfnAntSwitchCB) |
| Register callback for antenna switch. More... | |
| void | uble_resetAddr (void) |
| Make BD Addr revert to Random Static Address if exists or Public Address otherwise. | |
| bStatus_t | uble_setParameter (uint8 param, uint8 len, void *pValue) |
| Set a Micro BLE Stack parameter. More... | |
| bStatus_t | uble_stackInit (ubleAddrType_t addrType, uint8 *pStaticAddr, ublePostEvtProxyCB_t pfnPostEvtProxyCB, uint8 timeCritical) |
| Initialize Micro BLE Stack. More... | |
| uint8 | uble_timeCompare (uint32 time1, uint32 time2) |
| This function determines if the first time parameter is greater than the second time parameter, taking timer counter wrap into account. If so, TRUE is returned. More... | |
| uint32 | uble_timeDelta (uint32 time1, uint32 time2) |
| This function determines the difference between two time parameters, taking timer counter wrap into account. More... | |
| bStatus_t uble_checkAddr | ( | ubleAddrType_t | addrType, |
| uint8 * | pAddr | ||
| ) |
Check if the given address is valid.
| addrType | - UBLE_ADDRTYPE_PUBLIC , UBLE_ADDRTYPE_STATIC , UBLE_ADDRTYPE_NONRESOLVABLE , or UBLE_ADDRTYPE_RESOLVABLE |
| pAddr | - pointer to where the address to check resides |
| bStatus_t uble_getAddr | ( | ubleAddrType_t | addrType, |
| uint8 * | pAddr | ||
| ) |
Retrieve the address corresponding to the given address type.
| addrType | - UBLE_ADDRTYPE_PUBLIC , UBLE_ADDRTYPE_STATIC or UBLE_ADDRTYPE_BD |
| pAddr | pointer to memory location to return address. This should be a uint8_t[6] |
| bStatus_t uble_getParameter | ( | uint8 | param, |
| void * | pValue | ||
| ) |
Get a Micro BLE Stack parameter.
| param | - parameter ID: Micro BLE Stack Parameters |
| pValue | - pointer to location to get the value. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
| void uble_processMsg | ( | void | ) |
Let the Micro Stack process the queued messages.
| bStatus_t uble_registerAntSwitchCB | ( | ubleAntSwitchCB_t | pfnAntSwitchCB | ) |
Register callback for antenna switch.
| pfnAntSwitchCB | - application antenna switch callback |
| bStatus_t uble_setParameter | ( | uint8 | param, |
| uint8 | len, | ||
| void * | pValue | ||
| ) |
Set a Micro BLE Stack parameter.
| param | - parameter ID: Micro BLE Stack Parameters |
| len | - length of data to write |
| pValue | - pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
| bStatus_t uble_stackInit | ( | ubleAddrType_t | addrType, |
| uint8 * | pStaticAddr, | ||
| ublePostEvtProxyCB_t | pfnPostEvtProxyCB, | ||
| uint8 | timeCritical | ||
| ) |
Initialize Micro BLE Stack.
| addrType | - Micro BLE Stack Address Types Type of the address which the device will use initially. Either UBLE_ADDRTYPE_PUBLIC or UBLE_ADDRTYPE_STATIC . If addrType is UBLE_ADDRTYPE_PUBLIC , the public address which is stored in CCFG preferably or in FCFG otherwise will be used for BD Addr. If addrType is UBLE_ADDRTYPE_STATIC , BD Addr will depend on pBDAddr. |
| pStaticAddr | - If this is NULL and addrType is UBLE_ADDRTYPE_STATIC , a random static address will be generated by the stack and will be used for BD Address. If this is not NULL and addrType is UBLE_ADDRTYPE_STATIC , the 6 byte-long data pointed to by pBDAddr will be used for BD Address as the random static address. |
| pfnPostEvtProxyCB | - Callback to trigger a context switch to the application task so that the messages queued by the stack can be processed by uble_processMsg in the application task context. |
| timeCritical | - rf transmit operation. For strict timing on the transmission, set value to RF_TIME_CRITICAL. For relaxed timing on the transmission set value to RF_TIME_RELAXED. |
| uint8 uble_timeCompare | ( | uint32 | time1, |
| uint32 | time2 | ||
| ) |
This function determines if the first time parameter is greater than the second time parameter, taking timer counter wrap into account. If so, TRUE is returned.
| time1 | - First time. |
| time2 | - Second time. |
| uint32 uble_timeDelta | ( | uint32 | time1, |
| uint32 | time2 | ||
| ) |
This function determines the difference between two time parameters, taking timer counter wrap into account.
| time1 | - First time. |
| time2 | - Second time. |