Compiler and Linker Options¶
Compiler Options¶
Tip
More advanced documentation can be found in the compiler’s documentation:
For BLE5-Stack projects, compiler options are generated by SysConfig and stored in
the project’s Debug\syscfg
folder if using Debug version or it can be found in
the project’s Release\syscfg
folder if using Release version. The compiler.opt
file contains a set of options (typically include options and preprocessor defines)
to be passed to the compiler when compiling user source files. In the BLE5-Stack,
SysConfig is used to generate compile time options to configure BLE5-Stack. For
info on configurable SysConfig see BLE5-Stack SysConfig Features.
The .opt
files are generated through SysConfig when the project is built.
All Bluetooth LE example projects included in the SimpleLink Low Power F3 SDK come with SysConfig
enabled by default.
Note
host_test’s SysConfig file is configured such that it cannot be used to make Bluetooth LE configuration modifications. This is because host_test’s Bluetooth LE configuration has been carefully configured to facilitate the intended use-case of host_test.
The predefined symbols in the .opt
files are prefixed with a -D
, which
is standard commandline prefix notation across all the supported toolchains.
Of the predefined symbols in the .opt
files, some of them are configurable
and some are not. .opt
files generated by SysConfig cannot be directly
modified but instead must be modified through SysConfig. See Bluetooth Low Energy Application Configuration Parameters and
Bluetooth Low Energy Application Configuration Parameters for reference as to which options are
configurable.
The convention to disable a symbol in the .opt
files is to put an ‘x’ in
front of the name. For example, to disable power management,
change -DPOWER_SAVING
to -DxPOWER_SAVING
. It is also possible to
disable a symbol by commenting it out via ‘C - style’ syntax
(e.g. /* -DPOWER_SAVING */
).
Warning
Changes in an .opt
file may not be detected by the compiler/toolchain.
It is best to rebuild the entire project when a define is changed.
Linker Options¶
Linker symbols may need to be set or adjusted at the project level in order to control the memory layout of the generated image. The following procedure describes how to access and modify linker symbols.
CCS¶
Open Project Properties
Navigate in CCS to Build -> ARM Linker -> Advanced Options -> Command File Preprocessing
Use the buttons highlighted in Figure 41. to add, delete, or edit a linker symbol.

Figure 41. CCS Linker Symbols¶
IAR¶
Open the Project’s Options and select the Linker Category.
Open the Config tab.
View the Configuration File symbol definitions box (see Figure 43.).
Add or edit the preprocessor symbols.

Figure 43. IAR Defined Symbols Box¶
Linker Command File¶
Linker command files (or linker command scripts) allow to put linker options and directives in a file. These are used to control how the sections in the input files should be mapped into the output file, and to control the memory layout of the output file.
Per convention, the linker command files are named depending on the toolchain used:
xxx.cmd
for TI Clang (for more details, see here)xxx.icf
for IAR