33 #include "ti/ble/controller/ll/ll_common.h"    48 #define linkDB_Up( connectionHandle )  linkDB_State( (connectionHandle), LINK_CONNECTED )    58 #define linkDB_Encrypted( connectionHandle )  linkDB_State( (connectionHandle), LINK_ENCRYPTED )    68 #define linkDB_Authenticated( connectionHandle )  linkDB_State( (connectionHandle), LINK_AUTHENTICATED )    78 #define linkDB_Bonded( connectionHandle )  linkDB_State( (connectionHandle), LINK_BOUND )    95 #define LINKDB_CONNHANDLE_ALL                  LL_CONNHANDLE_ALL    97 #define LINKDB_CONNHANDLE_LOOPBACK             LL_CONNHANDLE_LOOPBACK    99 #define LINKDB_CONNHANDLE_INVALID              LL_CONNHANDLE_INVALID   107 #define LINK_NOT_CONNECTED              0x00       108 #define LINK_CONNECTED                  0x01       109 #define LINK_AUTHENTICATED              0x02       110 #define LINK_BOUND                      0x04       111 #define LINK_ENCRYPTED                  0x10       112 #define LINK_SECURE_CONNECTIONS         0x20       113 #define LINK_IN_UPDATE                  0x40       114 #define LINK_PAIR_TIMEOUT               0x80       121 #define LINKDB_ERR_INSUFFICIENT_AUTHEN      0x05     122 #define LINBDB_ERR_INSUFFICIENT_KEYSIZE     0x0c     123 #define LINKDB_ERR_INSUFFICIENT_ENCRYPTION  0x0f     197   extern uint8 
linkDB_State( uint16 connectionHandle, uint8 state );
 uint16 connTimeout
current connection timeout 
Definition: linkdb.h:150
uint8 addrType
Address type of connected device. 
Definition: linkdb.h:144
uint16 connLatency
current connection latency 
Definition: linkdb.h:151
uint8 linkDB_GetActiveConnInfo(uint8 connectionHandle, hciActiveConnInfo_t *activeConnInfo)
uint16 connInterval
The connection's interval (n * 1.23 ms) 
Definition: linkdb.h:148
uint8 linkDB_NumActive(void)
uint8 stateFlags
LinkDB Connection State Flags 
Definition: linkdb.h:143
uint16 MTU
The connection's MTU size. 
Definition: linkdb.h:149
uint8 linkDB_State(uint16 connectionHandle, uint8 state)
#define B_ADDR_LEN
Default Public and Random Address Length. 
Definition: bcomdef.h:99
uint8 linkDB_GetInfo(uint16 connectionHandle, linkDBInfo_t *pInfo)
Information pertaining to the linklinkDB info. 
Definition: linkdb.h:141
uint8 connRole
Connection formed as Central or Peripheral. 
Definition: linkdb.h:147
uint8 linkDB_NumConns(void)