GPIOLPF3.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2021-2025, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
53 #ifndef ti_drivers_GPIOLPF3__include
54 #define ti_drivers_GPIOLPF3__include
55 
56 #include <ti/drivers/GPIO.h>
57 
58 #include <ti/devices/DeviceFamily.h>
59 #include DeviceFamily_constructPath(inc/hw_ioc.h)
60 
61 #ifdef __cplusplus
62 extern "C" {
63 #endif
64 
65 /* Do not configure this pin. */
66 #define GPIO_CFG_DO_NOT_CONFIG_INTERNAL (0x80000000U)
67 
68 /* Re-map IOC PORTCFG defines from hw_ioc.h to GPIO defines*/
69 #define GPIO_MUX_PORTCFG_PFUNC7 IOC_IOC3_PORTCFG_DTB
70 #define GPIO_MUX_PORTCFG_PFUNC6 IOC_IOC3_PORTCFG_ANA
71 #define GPIO_MUX_PORTCFG_PFUNC5 IOC_IOC3_PORTCFG_PFUNC5
72 #define GPIO_MUX_PORTCFG_PFUNC4 IOC_IOC3_PORTCFG_PFUNC4
73 #define GPIO_MUX_PORTCFG_PFUNC3 IOC_IOC3_PORTCFG_PFUNC3
74 #define GPIO_MUX_PORTCFG_PFUNC2 IOC_IOC3_PORTCFG_PFUNC2
75 #define GPIO_MUX_PORTCFG_PFUNC1 IOC_IOC3_PORTCFG_PFUNC1
76 #define GPIO_MUX_GPIO_INTERNAL IOC_IOC3_PORTCFG_BASE
77 
78 /* We don't define this value on purpose - any unsupported values will cause a
79  * compile-time error. If your compiler tells you that this macro is missing,
80  * you are trying to use an unsupported option.
81  *
82  * See below for which options are unsupported.
83  */
84 #undef GPIOLPF3_CFG_OPTION_NOT_SUPPORTED
85 
86 /* Most configuration values are directly mapped to fields in the IOCn
87  * registers, but the mux bits are reserved for configuration options that
88  * cannot be directly mapped to the IOCn registers. The define below is the
89  * mask used by the GPIO driver to mask off the non-IOC configuration values.
90  */
91 #define GPIOLPF3_CFG_IOC_M (0xFFFFFFF8U)
92 
93 /* Low and high value interrupts are not available on Low Power F3 devices */
94 #define GPIO_CFG_INT_LOW_INTERNAL GPIOLPF3_CFG_OPTION_NOT_SUPPORTED
95 #define GPIO_CFG_INT_HIGH_INTERNAL GPIOLPF3_CFG_OPTION_NOT_SUPPORTED
96 
97 /* General options */
98 #define GPIO_CFG_NO_DIR_INTERNAL (IOC_IOC3_IOMODE_NORMAL | GPIOLPF3_CFG_PIN_IS_INPUT_INTERNAL)
99 /* Hysteresis is enabled by default for all input pins due to hardware changes on these devices.
100  * This may impact pin response by 1-2ns, but creates significantly more stable environments for
101  * high-speed use cases like SPI.
102  */
103 #define GPIO_CFG_INPUT_INTERNAL \
104  (IOC_IOC3_IOMODE_NORMAL | IOC_IOC3_INPEN | IOC_IOC3_WUENSB | IOC_IOC3_HYSTEN | GPIOLPF3_CFG_PIN_IS_INPUT_INTERNAL)
105 #define GPIO_CFG_OUTPUT_INTERNAL (IOC_IOC3_IOMODE_NORMAL | IOC_IOC3_INPEN | GPIOLPF3_CFG_PIN_IS_OUTPUT_INTERNAL)
106 #define GPIO_CFG_OUTPUT_OPEN_DRAIN_INTERNAL \
107  (IOC_IOC3_IOMODE_OPEND | IOC_IOC3_INPEN | GPIOLPF3_CFG_PIN_IS_OUTPUT_INTERNAL)
108 #define GPIO_CFG_OUT_OPEN_SOURCE_INTERNAL (IOC_IOC3_IOMODE_OPENS | IOC_IOC3_INPEN | GPIOLPF3_CFG_PIN_IS_OUTPUT_INTERNAL)
109 
110 #define GPIO_CFG_PULL_NONE_INTERNAL IOC_IOC3_PULLCTL_PULL_DIS
111 #define GPIO_CFG_PULL_UP_INTERNAL IOC_IOC3_PULLCTL_PULL_UP
112 #define GPIO_CFG_PULL_DOWN_INTERNAL IOC_IOC3_PULLCTL_PULL_DOWN
113 
114 #define GPIO_CFG_INT_NONE_INTERNAL IOC_IOC3_EDGEDET_EDGE_DIS
115 #define GPIO_CFG_INT_FALLING_INTERNAL IOC_IOC3_EDGEDET_EDGE_NEG
116 #define GPIO_CFG_INT_RISING_INTERNAL IOC_IOC3_EDGEDET_EDGE_POS
117 #define GPIO_CFG_INT_BOTH_EDGES_INTERNAL IOC_IOC3_EDGEDET_EDGE_BOTH
118 
119 /* We can feed this into the low bit of IOMODE, and it can then be ORed with output/input/OD/OS */
120 #define GPIO_CFG_INVERT_OFF_INTERNAL (0U)
121 #define GPIO_CFG_INVERT_ON_INTERNAL IOC_IOC3_IOMODE_INVERTED
122 
123 #define GPIO_CFG_HYSTERESIS_OFF_INTERNAL (0U)
124 #define GPIO_CFG_HYSTERESIS_ON_INTERNAL IOC_IOC3_HYSTEN
125 
126 #define GPIO_CFG_SHUTDOWN_WAKE_OFF_INTERNAL (0U)
127 #define GPIO_CFG_SHUTDOWN_WAKE_HIGH_INTERNAL IOC_IOC3_WUCFGSD_WAKE_HIGH
128 #define GPIO_CFG_SHUTDOWN_WAKE_LOW_INTERNAL IOC_IOC3_WUCFGSD_WAKE_LOW
129 
130 /* Slew limits and drive strength are only supported on specific pins: pin 12, pins 16-19, and pin 24 */
131 #define GPIO_CFG_SLEW_NORMAL_INTERNAL IOC_IOC17_SLEWRED_NORMAL
132 #define GPIO_CFG_SLEW_REDUCED_INTERNAL IOC_IOC17_SLEWRED_REDUCED
133 
134 #define GPIO_CFG_DRVSTR_LOW_INTERNAL IOC_IOC17_IOCURR_CUR_2MA
135 #define GPIO_CFG_DRVSTR_MED_INTERNAL IOC_IOC17_IOCURR_CUR_4MA
136 #define GPIO_CFG_DRVSTR_HIGH_INTERNAL IOC_IOC17_IOCURR_CUR_8MA
137 
138 /* Configuration values stored in mux bits. Any configuration options not
139  * directly handled by IOC need to be stored inside the mux bits (lowest 3 bits
140  * on Low Power F3 devices). These are masked out by GPIO_init(),
141  * GPIO_setConfig(), GPIO_setConfigAndMux() and GPIO_getConfig() using
142  * GPIOLPF3_CFG_IOC_M.
143  */
144 
145 /* Default output value */
146 #define GPIO_CFG_OUTPUT_DEFAULT_HIGH_INTERNAL (0x1U)
147 #define GPIO_CFG_OUTPUT_DEFAULT_LOW_INTERNAL (0U)
148 
149 /* Whether GPIO hardware should have the output enable bit set for this pin */
150 #define GPIOLPF3_CFG_PIN_IS_INPUT_INTERNAL (0x2U)
151 #define GPIOLPF3_CFG_PIN_IS_OUTPUT_INTERNAL (0U)
152 
153 /* Interrupt enable is in the GPIO module */
154 #define GPIO_CFG_INT_ENABLE_INTERNAL (0x4U)
155 #define GPIO_CFG_INT_DISABLE_INTERNAL (0U)
156 
157 #ifdef __cplusplus
158 }
159 #endif
160 
161 #endif /* ti_drivers_GPIOCC26XX__include */
General Purpose I/O driver interface.
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale