Disable External Flash¶
The external flash consumes energy and can be disabled if not used.
By default, SysConfig generates the code to enable / disable the external
flash at the end of ti_drivers_config.c. The functions available to the
application are: Board_sendExtFlashByte, Board_wakeUpExtFlash, and
Board_shutDownExtFlash.
By default, the Board_init function disables external flash.