Channel Sounding

This chapter serves as a guide to the Texas Instruments Channel Sounding feature including application implementation, drivers, and middle layers of the stack. Bluetooth 6.0 specification Channel Sounding extends the capabilities of Bluetooth-based ranging beyond traditional RSSI and direction finding (DF) methods, enabling more accurate and cost-effective ranging designs.

The guide will cover the main principles of the Channel Sounding process, the process of adding Channel Sounding to a project, and an out of the box example project available within the SimpleLink Low Power F3 SDK.

The Channel Sounding chapters will cover:

The CC23xx or CC27xx LaunchPad allows for quick and easy development of BLE applications, such as Channel Sounding. To run the Channel Sounding example, you will need two TI CC23xx or CC27xx.

Note: To run the CS demo, one must use CC27xx as car node in order to support distance calculation.

Channel Sounding Overview

What is Channel Sounding? Bluetooth Channel Sounding (CS), introduced in the Bluetooth 6.0 specification, enables high-accuracy distance measurement between two BLE devices using phase-based ranging (PBR). This technique estimates the distance by measuring the phase difference between a received unmodulated tone and the device’s local oscillator (LO) across multiple RF frequencies in the 2.4 GHz band. Both devices—the initiator and the reflector—exchange tones and record phase information. These phase differences, when plotted against frequency, yield a curve whose slope directly corresponds to the physical distance between devices. Advanced signal processing helps correct for multipath interference, enhancing precision even in complex radio environments.

Why is Channel Sounding Important? Channel Sounding delivers high-level distance accuracy without needing external infrastructure, making it ideal for real-time location systems (RTLS), car access, and secure proximity-based services. It also introduces built-in security mechanisms like random frequency hopping, Round Trip Time (RTT) validation, and attack detection metrics (NADM) to defend against spoofing or relay attacks. Importantly, it integrates efficiently with existing Bluetooth LE protocols, supporting low-power, low-cost, and scalable deployment across consumer, industrial, and automotive applications.

Two BLE supported devices are needed for Channel Sounding for this version of the SimpleLink Low Power F3 SDK.

  • Car Node

  • Key Node

The car node is the initiator device and the key node is the reflector device. The initiator is the device that is in control of the channel sounding configuration, synchronization, and begins each channel sounding subevent. Firstly, Mode 0 steps are sent from the initiator to the reflector. The Mode 0 steps synchronize the reflector to the initiators configuration and sets up the timing for the unmodulate tones, or subevents. Next, Mode 1, 2, or 3 steps can be completed. These steps include (RTT), (PBR) or a combination of both. Each step is an unmodulated tone sent between the initiator and the reflector device. The phase change or the time of flight of the tone is then used to calculate the distance, and/or detect spoofing, or man in the middle attacks.

How to enable Channel Sounding example

Channel sounding example works using CCS and Python:

  • CCS is used to flash one CC23xx or CC27xx with an initiator code and the second with one with a reflector code.

  • Python is used to control car node and plot results of CS procedure.

The following section will go through the SW flow behind TI’s CS demo.

@startuml

participant PC
participant "Car Node"
participant "Key Node"

group Channel Sounding

    "Key Node" -> "Key Node" : GapAdv_enable()
    PC -> "Car Node" : GapScan_enable()

    "Car Node" -> "Key Node" : Send Connection Indication packet

    "Car Node" -> "Key Node" : Pairing_Request
    "Key Node" -> "Car Node" : Pairing_Response

    rnote over "Car Node"
        GAP_BOND_PAIRING_STATE_STARTED
    end note

    rnote over "Key Node"
        GAP_BOND_PAIRING_STATE_STARTED
    end note

    "Car Node" -> "Key Node" : Encryption_Request
    "Key Node" -> "Car Node" : Encryption_Response

    rnote over "Car Node"
        GAP_BOND_PAIRING_STATE_COMPLETE
    end note

    rnote over "Key Node"
        GAP_BOND_PAIRING_STATE_COMPLETE
    end note

    "Car Node" -> PC : Connection_Data

    PC -> "Car Node" : CS_CMD_READ_LOCAL_CAP

    PC -> "Car Node" : CS_CMD_READ_REMOTE_CAP
    "Car Node" -> "Key Node" : LLCP_CS_Capabilities_Request
    "Key Node" -> "Car Node" : LLCP_CS_Capabilities_Response
    "Car Node" -> PC : NWP_CS_READ_REMOTE_CAPS

    PC -> "Car Node" : CS_CMD_SECURITY_ENABLE
    "Car Node" -> "Key Node" : LLCP_CS_Security_Request
    "Key Node" -> "Car Node" : LLCP_CS_Security_Response
    "Car Node" -> PC : NWP_CS_SECURITY_ENABLE_COMPLETE

    PC -> "Car Node" : CS_CMD_SET_DEFAULT_SETTINGS

    PC -> "Car Node" : CS_CMD_CREATE_CONFIG
    "Car Node" -> "Key Node" : LLCP_CS_Config_Request
    "Key Node" -> "Car Node" : LLCP_CS_Config_Response
    "Car Node" -> PC : NWP_CS_CONFIG_COMPLETE

    PC -> "Car Node" : CS_CMD_PROCEDURE_ENABLE
    "Car Node" -> "Key Node" : LLCP_CS_Request
    "Key Node" -> "Car Node" : LLCP_CS_Response
    "Car Node" -> "Key Node" : LLCP_CS_Indication
    "Car Node" -> PC : NWP_CS_CONFIG_COMPLETE

    rnote over "Car Node"
        Channel Sounding Procedure
    end note

    rnote over "Key Node"
        Channel Sounding Procedure
    end note

    "Car Node" -> PC : NWP_CS_APP_DISTANCE_RESULTS

end

@enduml

Figure 132. Channel Sounding Example Project Software Flow

Prerequisites

Hardware:

  • 2 x SimpleLink CC23xx or CC27xx LaunchPad Target

  • 2 x SimpleLink™ LaunchPad™ XDS110 Debugger

  • 2 x USB cable

  • (Optional) 1 x Battery Pack for Reflector

Software:

Prepare CCS and Python environment

1. For the initiator node, import <SDK>/examples/rtos/LP_EM_CC2745R10/ble/car_node and set the example to initiate a pairing request within Bond Manager. Procedure to do this is described below. Flash the car_node project onto one of the two CC23xx or CC27xx devices and keep it connected to your PC. The COM port of the ble_device_car_node_with_distance.py script should be set to the COM port of the car node.

../_images/ConfigureInitiatePairing_CarNode.png

Figure 133. Configure Car Node to Initiate Pairing

../_images/ConfiguringComPort_CarNode.png

Figure 134. Configure COM Port for Car Node in Python

  1. For reflector node, import <SDK>/examples/rtos/LP_EM_CC2745R10/ble/key_node. Flash the key_node project onto the second CC23xx or CC27xx device. The reflector does not need to remain connected to your PC. It only needs to be powered.

Note: Advertising data in the key node project is used by python. If it is changed in CCS, make sure to change it in python script too.

  1. (Optional) To configure 2x2 antenna setup for both CC23xx or CC27xx:

    • Python:

      • Go to <SDK>/tools/ble/ble_agent/examples/ble_device_car_node_with_distance.py. Change in cs_set_procedure_params and cs_set_procedure_params_repeat “aci” from 0 to 7 and “preferred_peer_antenna” from 0b0001 to 0b0011;

      • To use other antenna configurations, refer to the ACI map below. Additionally, the preferred_peer_antenna bitmap will dictate the number of antennas on the peer (reflector).

    ACI

    Ant Config

    ACI=0

    1x1

    ACI=1

    2x1

    ACI=2

    3x1

    ACI=3

    4x1

    ACI=4

    1x2

    ACI=5

    1x3

    ACI=6

    1x4

    ACI=7

    2x2

    Note: The antenna configurations above are oriented initiator x reflector.

    • CCS:

      • Go to Syscfg -> RF STACKS -> BLE -> Channel sounding configuration -> Number of Antennas. Select 2 antennas, and configure the Antenna Mux Bitmap 0xC6. For different antenna configurations, refer to the note within the Antenna Mux Bitmap section of SysConfig.

      • Syscfg -> TI DRIVERS -> RCL -> RCL Observable -> Additional RF GPIO Signals. Add PBEGPO2 and PBEGPO3.

../_images/ConfigureAdditionalRFGPIOSignals.png

Figure 135. Configure PBEGPOs for Multiple Antennas

4. (Optional) To configure algorithm, max distance, QQ3 threshold, Distance Fusion, antenna path summation, and gap interpolation, navigate to the Car Node project in CCS -> app folder -> inc folder -> app_cs_process.c file -> csProcess_InitConfig.

Note: Max distance measurable = maxDistance / 2

../_images/csProcess_InitConfig.png
  1. Install Python 3.10.11

Note: Python 3.10 should be installed at C:\Python310

  1. During installation select “Add Environment Variable”, otherwise you can add it later, shown in the images below:

../_images/system_properties.png

Figure 136. Open System Properties

../_images/env_variables.jpg

Figure 137. Navigate to Environment Variables

../_images/edit_env_variables.jpg

Figure 138. Edit User Environment Variables

  1. Open a command line tool such as Windows Power Shell and install and activate virtual environment. In case your network is behind a proxy, use the proxy command shown.

Listing 158. Setup virtual environment
1    cd <ble_agent folder (SDK/tools/ble/ble_agent)>
2    c:\Python310\python.exe -m pip install virtualenv [--proxy <www.proxy.com>]
3    c:\Python310\python.exe -m venv .venv
4    .venv\Scripts\activate
  1. Setup external packages in case your network is behind a proxy, use [–proxy]

Listing 159. Upgrade python packages
1    python -m pip install --upgrade pip [--proxy <www.proxy.com>]
2    pip install --upgrade wheel [--proxy <www.proxy.com>]
3    pip install -r requirements.txt [--proxy <www.proxy.com>]

How to run Channel Sounding example

Python

Execute Python Script in the previously configured environment using:

Listing 160. Activate virtual environment
1    cd \simplelink_lowpower_f3_source_sdk_9_10_00_70_eng\tools\ble\ble_agent
2    .venv\Scripts\activate
3    cd examples
4    python ble_device_car_node_with_distance.py

The script will automatically initiate a connection between the car node and key node and start a CS procedure. See an example of the output below:

../_images/DistanceOutput_Terminal.png

Figure 139. Distance Output in Terminal