SYS0

Instance: SYS0
Component: SYS0
Base address: 0x40004000


This is top module of SYS0

TOP:SYS0 Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

DESC

RO

32

0x6B4E 0010

0x0000 0000

0x4000 4000

MUNLOCK

WO

32

0x0000 0000

0x0000 000C

0x4000 400C

ATESTCFG

RW

32

0x0000 000F

0x0000 0100

0x4000 4100

TSENSCFG

RW

32

0x0000 0000

0x0000 0108

0x4000 4108

LPCMPCFG

RW

32

0x0000 0000

0x0000 010C

0x4000 410C

VGMCFG

RW

32

0x0000 0003

0x0000 0110

0x4000 4110

VGMTRIMDBG

RW

32

0x0000 0000

0x0000 0114

0x4000 4114

DEVICEID

RO

32

0x0BB9 802F

0x0000 03FC

0x4000 43FC

DBGAUTH

WO

32

0x0000 0000

0x0000 0410

0x4000 4410

PARTID

RW

32

0x0000 0000

0x0000 07F8

0x4000 47F8

LIFECYC

RW

32

0x0000 0000

0x0000 07FC

0x4000 47FC

TMUTE0

RW

32

0x0000 0000

0x0000 0800

0x4000 4800

TMUTE1

RW

32

0x0000 0000

0x0000 0804

0x4000 4804

TMUTE2

RW

32

0x0080 0000

0x0000 0808

0x4000 4808

TMUTE3

RW

32

0x0000 0000

0x0000 080C

0x4000 480C

TMUTE4

RW

32

0xB02E 603F

0x0000 0810

0x4000 4810

TMUTE5

RW

32

0x0000 0000

0x0000 0814

0x4000 4814

TOP:SYS0 Register Descriptions

TOP:SYS0:DESC

Address Offset 0x0000 0000
Physical Address 0x4000 4000 Instance 0x4000 4000
Description Description Register
This register provides IP module ID, revision information, instance index and standard MMR registers offset.
Type RO
Bits Field Name Description Type Reset
31:16 MODID Module Identifier is used to uniquely identify this IP RO 0x6B4E
15:12 STDIPOFF Standard IP MMR block offset. Standard IP MMRs are the set from aggregated IRQ registers till DTB.

0: Standard IP MMRs do not exist

0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address)
RO 0x0
11:8 INSTIDX IP Instance ID number. If multiple instances of IP exist in the device, this field can identify the instance number (0-15). RO 0x0
7:4 MAJREV Major revision of IP (0-15). RO 0x1
3:0 MINREV Minor revision of IP (0-15). RO 0x0

TOP:SYS0:MUNLOCK

Address Offset 0x0000 000C
Physical Address 0x4000 400C Instance 0x4000 400C
Description Mutable section Unlock
This register unlocks registers in mutable section
Type WO
Bits Field Name Description Type Reset
31:0 KEY Write the unlock key 0xC5AF6927 to temporarily unlock registers in mutable section. The lock is set automatically if no write accesses, to the mutable section, are detected for consecutive 32 CLKULL (24MHz) clock cycles. Writing any value other than that, the unlock key will immediately lock the mutable register space for write access.
Value ENUM Name Description
0x0 LOCK Lock registers in the mutable section
0xC5AF6927 UNLOCK Unlock registers in the mutable section
WO 0x0000 0000

TOP:SYS0:ATESTCFG

Address Offset 0x0000 0100
Physical Address 0x4000 4100 Instance 0x4000 4100
Description ATEST Configuration
This register is used to configure analog switches in ATEST module.
Type RW
Bits Field Name Description Type Reset
31:24 KEY Key must be written with value 0x5A for successful write to ATESTCFG and to unlock register state.
Write with any value other than 0x5A to KEY will be ignored and register content is not updated.
It is recommended to write this register with incorrect KEY to lock back register state after necessary ATESTCFG updates are done.
Read value of KEY is 0x0.
WO 0x00
23:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000
8 VSEL Selects supply for ATEST switches.
Value ENUM Name Description
0x0 VDDBST Selects VDDBOOST
0x1 VDDS Selects VDDS
RW 0
7 VA2VA1 Enables isolation switch between VA_ATEST_A1 and VA_PAD_A1.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 0
6 VA2VA0 Enables isolation switch between VA_ATEST_A0 and VA_PAD_A0.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 0
5 VR2VA1 Enables isolation switch between VR_ATEST_A1 and VA_ATEST_A1.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 0
4 VR2VA0 Enables isolation switch between VR_ATEST_A0 and VA_ATEST_A0.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 0
3 SHTVA1 Shorts VA_ATEST_A1 to ground.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 1
2 SHTVA0 Shorts VA_ATEST_A0 to ground.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 1
1 SHTVR1 Shorts VR_ATEST_A1 to ground.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 1
0 SHTVR0 Shorts VR_ATEST_A0 to ground.
Value ENUM Name Description
0x0 OPEN Switch is open
0x1 CLOSE Switch is closed
RW 1

TOP:SYS0:TSENSCFG

Address Offset 0x0000 0108
Physical Address 0x4000 4108 Instance 0x4000 4108
Description TSENSE Configuration
This register is used to configure temperature sensor module.
Type RW
Bits Field Name Description Type Reset
31:26 RESERVED26 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000
25:12 RESERVED12 Software should not rely on the value of a reserved field. Writing any other value than the reset value may result in undefined behavior RO 0b00 0000 0000 0000
11 TSENS2EN This is the enable bit for the second temperature sensor in AUX.
Value ENUM Name Description
0x0 DIS Second temperature sensor is disabled.
0x1 EN Second temperature sensor is enabled.
RW 0
10:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b0 0000 0000
1:0 SEL Used to enable and configure temperature sensor module. Setting the value to 0x3 will disable the temperature sensor.
Value ENUM Name Description
0x0 DISABLE Temperature sensor is disabled
0x1 VALUE 20uA current is injected on VR_ATEST_A0 and voltage measured on VR_ATEST_A1
0x2 GND 20uA current is injected on VR_ATEST_A0 and ground measured on VR_ATEST_A1
RW 0b00

TOP:SYS0:LPCMPCFG

Address Offset 0x0000 010C
Physical Address 0x4000 410C Instance 0x4000 410C
Description LPCMP configuration
This register is used to configure and check the status of low-power comparator (LPCOMP) module.
Type RW
Bits Field Name Description Type Reset
31 RESERVED31 Software should not rely on the value of a reserved field. Writing any other value than the reset value may result in undefined behavior RO 0
30 HYSPOL Hysteresis polarity
Value ENUM Name Description
0x0 NOINV Not inverted
0x1 INV Inverted
RW 0
29:28 ATESTMUX Used to configure ATEST mux in comparator module and provides chosen output on VA_ATEST_A0.
Note: This bit field is write-protected using global lock indicator on production device.
Value ENUM Name Description
0x0 OFF ATEST mux is off
0x1 COMPOUT Selects comparator output
0x2 COMP_VIN_NEG Selects voltage divider output
0x3 IBIASOUT Selects bias current output
RW 0b00
27:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
24 EVTIFG Event flag

The event flag is set when the comparator output transition is qualified based on the edge polarity configuration in EDGCFG.
Value ENUM Name Description
0x0 CLR Clear
0x1 SET Set
RW 0
23:22 RESERVED22 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
21 COUTEN Enables LPCOMP output on device pin.
Value ENUM Name Description
0x0 DIS Disabled
0x1 EN Enabled
RW 0
20 COUT LPCOMP output status. This bit captures the value LPCOMP raw output.
Value ENUM Name Description
0x0 LOW Output is low
0x1 HIGH Output is high
RO 0
19 RESERVED19 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
18 WUENSB Enables lpcmpcfg output to wake device from standby.
Value ENUM Name Description
0x0 DIS Disable
0x1 EN Enable
RW 0
17 EVTEN Enables event generation. Comparator module will produce event on ULL event fabric when EVTIFG is set.
Value ENUM Name Description
0x0 DIS Disable
0x1 EN Enable
RW 0
16 EDGCFG Selects positive edge or negative edge detection on comparator output to set the event flag
Value ENUM Name Description
0x0 RISE Rise edge detection
0x1 FALL Fall edge detection
RW 0
15 RESERVED15 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
14:12 NSEL Negative input selection. Setting values 0x5-0x7 will open all the switches.
Value ENUM Name Description
0x0 OPEN All switches are open
0x1 VA_PAD_A2 Selects VA_PAD_A2
0x2 VA_PAD_A3 Selects VA_PAD_A3
0x3 VDDS Selects VDDS
0x4 VDDD Selects VDDD
RW 0b000
11:8 PSEL Positive input selection. Setting values 0x9-0xF will open all the switches.
Value ENUM Name Description
0x0 OPEN All switches are open
0x1 VA_PAD_A1 Selects VA_PAD_A1
0x2 VA_PAD_A2 Selects VA_PAD_A2
0x3 VA_PAD_A3 Selects VA_PAD_A3
0x4 VR_ATEST_A0 Selects VR_ATEST_A0
0x5 VR_ATEST_A1 Selects VR_ATEST_A1
0x6 VA_ATEST_A0 Selects VA_ATEST_A0
0x7 VA_ATEST_A1 Selects VA_ATEST_A1
0x8 VDDS Selects VDDS
RW 0x0
7:5 HYSSEL Used to enable and select hysteresis level

Hysteresis is disabled when HYSSEL = 0 and enabled for other values of HYSSEL from 1 to 7. Refer to device specific datasheet for individual hysteresis values.
Value ENUM Name Description
0x0 VAL0 Hysteresis is disabled
0x1 VAL1 Hysteresis value 1
0x2 VAL2 Hysteresis value 2
0x3 VAL3 Hysteresis value 3
0x4 VAL4 Hysteresis value 4
0x5 VAL5 Hysteresis value 5
0x6 VAL6 Hysteresis value 6
0x7 VAL7 Hysteresis value 7
RW 0b000
4 DIVPATH Used to select the path on which voltage divider is applied
Value ENUM Name Description
0x0 NSIDE Divider is applied on N-side
0x1 PSIDE Divider is applied on P-side
RW 0
3:1 DIV Used to configure reference divider. Setting values 0x5-0x7 will set the divide value to 1.
Value ENUM Name Description
0x0 VAL0 Divide value is 1
0x1 VAL1 Divide value is 3/4
0x2 VAL2 Divide value is 1/2
0x3 VAL3 Divide value is 1/3
0x4 VAL4 Divide value is 1/4
RW 0b000
0 EN Used to enable comparator module.
Value ENUM Name Description
0x0 DIS Disable
0x1 EN Enable
RW 0

TOP:SYS0:VGMCFG

Address Offset 0x0000 0110
Physical Address 0x4000 4110 Instance 0x4000 4110
Description This register is used to configure the VGM module.
Type RW
Bits Field Name Description Type Reset
31:24 KEY Key must be written with value 0x5A for successful write to VGMCFG and to unlock register state.
Write with any value other than 0x5A to KEY will be ignored and the register content is not updated.
Read value of KEY is 0x0.
WO 0x00
23:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x000
11:8 ATBMUXSEL These bits are used to generate VGM ATB mux selection control. RW 0x0
7:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000
1 OSHDETDIS Disables overshoot detector in VGM.
Value ENUM Name Description
0x0 EN Enable
0x1 DIS Disable
RW 1
0 USHTDETDIS Disables undershoot detector in VGM.
Value ENUM Name Description
0x0 EN Enable
0x1 DIS Disable
RW 1

TOP:SYS0:VGMTRIMDBG

Address Offset 0x0000 0114
Physical Address 0x4000 4114 Instance 0x4000 4114
Description This register is used to trim and debug VGM module.
Type RW
Bits Field Name Description Type Reset
31 RESERVED31 RESERVED RO 0
30 TMODE5 Test mode bit for glitchy supply mux selection. RW 0
29:27 TMODE4 Test mode bits for VREF mux selection for overshoot detector. RW 0b000
26:24 TMODE3 Test mode bits for VREF mux selection for undershoot detector. RW 0b000
23:22 RESERVED22 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
21:20 TMODE2 Test mode for level shifter isolation. RW 0b00
19:18 TMODE1 Test mode bits for low voltage SR latch reset. RW 0b00
17:16 TMODE0 Test mode bits for 3V SR latch reset. RW 0b00
15:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
11:8 IBPROG These bits are used to program VGM bias current generator. RW 0x0
7:4 OSHDETTRIM These bits are used to trim VGM overshoot detector. RW 0x0
3:0 USHTDETTRIM These bits are used to trim VGM undershoot detector. RW 0x0

TOP:SYS0:DEVICEID

Address Offset 0x0000 03FC
Physical Address 0x4000 43FC Instance 0x4000 43FC
Description Device ID
This register provides Device ID information.
Note: This 32-bit register value is provided as output to DEBUGSS.
Type RO
Bits Field Name Description Type Reset
31:28 VERSION Monotonic increasing value indicating new hardware revision. A newer hardware revision shall never have a lower version than an older revision of hardware. RO 0x0
27:12 DEVICE Value generated by RAMP for the SOC. This value uniquely identifies the die from any other TI device. RO 0xBB98
11:1 MANFACTURER JEP 106 assigned manufacturer ID. This field identifies the device as a Texas Instruments device. RO 0b000 0001 0111
0 ALWAYSONE Value 1 in this bit field means that a 32-bit scan register exists. RO 1

TOP:SYS0:DBGAUTH

Address Offset 0x0000 0410
Physical Address 0x4000 4410 Instance 0x4000 4410
Description Debug Authentication.
This register is used by ROM to store Debug Authnetication Status
Type WO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17:16 CLR Clears Authentication Status WO 0b00
15:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
1:0 SET Sets Authentication Status
Value ENUM Name Description
0x0 UNAUTH Debug Unauthorized
0x1 NONINV Only Non-Invasive Debug Authorized
0x2 NONSEC Non-Secure Debug Authorized
0x3 SEC Secure Debug Authorized
WO 0b00

TOP:SYS0:PARTID

Address Offset 0x0000 07F8
Physical Address 0x4000 47F8 Instance 0x4000 47F8
Description Part ID
This register is programmed by boot code with Part ID information. Note: This 32-bit register value is provided as output to DEBUGSS
Type RW
Bits Field Name Description Type Reset
31 START Start bit
Value ENUM Name Description
0x0 CLR Clear
0x1 SET Set
RW 0
30:28 MAJORREV Monotonic increasing value indicating a new revision of the SKU significant enough that users of the device may have to revise PCB or software design RW 0b000
27:24 MINORREV Monotonic increasing value indicating a new revision of the SKU that preserves compatibility with lesser MINORREV values RW 0x0
23:16 VARIANT Bit pattern uniquely identifying a variant of a part RW 0x00
15:0 PART Bit pattern uniquely identifying a part RW 0x0000

TOP:SYS0:LIFECYC

Address Offset 0x0000 07FC
Physical Address 0x4000 47FC Instance 0x4000 47FC
Description This register is programmed by boot code with device life cycle information
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 RESERVED RO 0x00 0000
7:0 VAL Device life cycle value.
Value ENUM Name Description
0x0 LCYCLE_POSSIBLE_1STBDAY Possible first birthday
0x1 LCYCLE_1STBDAY First birthday
0x2 LCYCLE_TESTPT Test Production Test
0x3 LCYCLE_TESTFT Test Final Test
0x4 LCYCLE_ENGRDEV Engineering device
0x5 LCYCLE_PRODDEV Production device
0x6 LCYCLE_RETEST Re-test
0xFF LCYCLE_ILLEGAL Illegal
RW 0x00

TOP:SYS0:TMUTE0

Address Offset 0x0000 0800
Physical Address 0x4000 4800 Instance 0x4000 4800
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:0 CDACL Internal. Only to be used through TI provided API. RW 0x0000 0000

TOP:SYS0:TMUTE1

Address Offset 0x0000 0804
Physical Address 0x4000 4804 Instance 0x4000 4804
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:0 CDACM Internal. Only to be used through TI provided API. RW 0x0000 0000

TOP:SYS0:TMUTE2

Address Offset 0x0000 0808
Physical Address 0x4000 4808 Instance 0x4000 4808
Description TMUTE2 trim Register
Type RW
Bits Field Name Description Type Reset
31 RESERVED31 RESERVED RO 0
30:26 IBTRIM LPCOMP: Bias current trim, 250nA to be terminated across I2V, 1M ohm setting. Resulting target trim voltage 250mV. RW 0b0 0000
25:23 TRIM ADC REFBUF trim bits. RW 0b001
22:16 LATCH SOC ADC: Latch trim bits. These bits are used in the analog IP. RW 0b000 0000
15:4 OFFSET SOCADC: Offset trim bits. These bits are used in DTC. RW 0x000
3:2 RES SOCADC: Resistor trim bits. These bits are used in the analog IP. RW 0b00
1:0 CDACU SOCADC: Upper 2 bits of CDAC trim. These bits are used in DTC. RW 0b00

TOP:SYS0:TMUTE3

Address Offset 0x0000 080C
Physical Address 0x4000 480C Instance 0x4000 480C
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:26 BATC1 Internal. Only to be used through TI provided API. RW 0b00 0000
25:19 BATC0 Internal. Only to be used through TI provided API. RW 0b000 0000
18:14 TEMPC2 Internal. Only to be used through TI provided API. RW 0b0 0000
13:8 TEMPC1 Internal. Only to be used through TI provided API. RW 0b00 0000
7:0 TEMPC0 Internal. Only to be used through TI provided API. RW 0x00

TOP:SYS0:TMUTE4

Address Offset 0x0000 0810
Physical Address 0x4000 4810 Instance 0x4000 4810
Description TMUTE4 trim Register
Type RW
Bits Field Name Description Type Reset
31:28 RECHCOMPREFLVL Internal. Only to be used through TI provided API. RW 0xB
27:26 IOSTRCFG2 Internal. Only to be used through TI provided API. RW 0b00
25:22 IOSTRCFG1 Internal. Only to be used through TI provided API. RW 0x0
21:19 MAX Internal. Only to be used through TI provided API. RW 0b101
18:16 MED Internal. Only to be used through TI provided API. RW 0b110
15:13 MIN Internal. Only to be used through TI provided API. RW 0b011
12:11 DCDCLOAD Internal. Only to be used through TI provided API. RW 0b00
10:8 IPEAK Internal. Only to be used through TI provided API. RW 0b000
7:6 DTIME Internal. Only to be used through TI provided API. RW 0b00
5:3 LENSEL Internal. Only to be used through TI provided API. RW 0b111
2:0 HENSEL Internal. Only to be used through TI provided API. RW 0b111

TOP:SYS0:TMUTE5

Address Offset 0x0000 0814
Physical Address 0x4000 4814 Instance 0x4000 4814
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:13 RESERVED13 Internal. Only to be used through TI provided API. RO 0b000 0000 0000 0000 0000
12:10 DCDCDRVDS Internal. Only to be used through TI provided API. RW 0b000
9:5 GLDOISCLR Internal. Only to be used through TI provided API. WO 0b0 0000
4:0 GLDOISSET Internal. Only to be used through TI provided API. WO 0b0 0000
4:0 RESERVED0 Internal. Only to be used through TI provided API. RO 0b0 0000