332 #ifndef ti_drivers_can__include   333 #define ti_drivers_can__include   339 #include <ti/devices/DeviceFamily.h>   357 #define CAN_STATUS_SUCCESS ((int_fast16_t)0)   365 #define CAN_STATUS_ERROR ((int_fast16_t)-1)   373 #define CAN_STATUS_NOT_SUPPORTED ((int_fast16_t)-2)   380 #define CAN_STATUS_TX_BUF_FULL ((int_fast16_t)-3)   388 #define CAN_STATUS_NO_RX_MSG_AVAIL ((int_fast16_t)-4)   396 #define CAN_STATUS_NO_TX_EVENT_AVAIL ((int_fast16_t)-5)   413 #define CAN_EVENT_SPI_XFER_ERROR (0x800U)   421 #define CAN_EVENT_BIT_ERR_UNCORRECTED (0x400U)   431 #define CAN_EVENT_RX_RING_BUFFER_FULL (0x200U)   438 #define CAN_EVENT_RX_FIFO_MSG_LOST (0x100U)   443 #define CAN_EVENT_ERR_PASSIVE (0x80U)   448 #define CAN_EVENT_ERR_ACTIVE (0x40U)   453 #define CAN_EVENT_BUS_OFF (0x20U)   458 #define CAN_EVENT_BUS_ON (0x10U)   466 #define CAN_EVENT_TX_EVENT_LOST (0x08U)   475 #define CAN_EVENT_TX_EVENT_AVAIL (0x04U)   480 #define CAN_EVENT_TX_FINISHED (0x02U)   488 #define CAN_EVENT_RX_DATA_AVAIL (0x01U)   497 #define CAN_DLC_0B  ((uint32_t)0U)   498 #define CAN_DLC_1B  ((uint32_t)1U)   499 #define CAN_DLC_2B  ((uint32_t)2U)   500 #define CAN_DLC_3B  ((uint32_t)3U)   501 #define CAN_DLC_4B  ((uint32_t)4U)   502 #define CAN_DLC_5B  ((uint32_t)5U)   503 #define CAN_DLC_6B  ((uint32_t)6U)   504 #define CAN_DLC_7B  ((uint32_t)7U)   505 #define CAN_DLC_8B  ((uint32_t)8U)   506 #define CAN_DLC_12B ((uint32_t)9U)     507 #define CAN_DLC_16B ((uint32_t)10U)    508 #define CAN_DLC_20B ((uint32_t)11U)    509 #define CAN_DLC_24B ((uint32_t)12U)    510 #define CAN_DLC_32B ((uint32_t)13U)    511 #define CAN_DLC_48B ((uint32_t)14U)    512 #define CAN_DLC_64B ((uint32_t)15U)    531 #define CAN_FEC_DISABLE_FILTER         ((uint32_t)0U)   532 #define CAN_FEC_STORE_RXFIFO0          ((uint32_t)1U)   533 #define CAN_FEC_STORE_RXFIFO1          ((uint32_t)2U)   534 #define CAN_FEC_REJECT_ID              ((uint32_t)3U)   535 #define CAN_FEC_SET_PRIO               ((uint32_t)4U)   536 #define CAN_FEC_SET_PRIO_STORE_RXFIFO0 ((uint32_t)5U)   537 #define CAN_FEC_SET_PRIO_STORE_RXFIFO1 ((uint32_t)6U)   538 #define CAN_FEC_STORE_RXBUF            ((uint32_t)7U)   550 #define CAN_FILTER_RANGE     ((uint32_t)0U)   551 #define CAN_FILTER_DUAL_ID   ((uint32_t)1U)   552 #define CAN_FILTER_WITH_MASK ((uint32_t)2U)   553 #define CAN_FILTER_DISABLE   ((uint32_t)3U)   606 typedef void (*
CAN_EventCbk)(CAN_Handle handle, uint32_t event, uint32_t data, 
void *userArg);
   635     uint32_t rxFifoNum[2];
   760     uint32_t rxFifoNum[2];   
   787 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX)   899 int_fast16_t 
CAN_read(CAN_Handle handle, CAN_RxBufElement *elem);
   913 int_fast16_t 
CAN_write(CAN_Handle handle, 
const CAN_TxBufElement *elem);
   941 int_fast16_t 
CAN_writeBuffer(CAN_Handle handle, uint32_t bufIdx, 
const CAN_TxBufElement *elem);
   955 int_fast16_t 
CAN_readTxEvent(CAN_Handle handle, CAN_TxEventElement *elem);
   968 void CAN_getBitTiming(CAN_Handle handle, CAN_BitTimingParams *bitTiming, uint32_t *clkFreq);
 ADC_Params params
Definition: Driver_Init.h:11
uint32_t nbrp
Definition: CAN.h:701
MCAN_TxEventFifoElement CAN_TxEventElement
A CAN Tx Event element struct for CAN_readTxEvent(). 
Definition: CAN.h:569
void(* CAN_EventCbk)(CAN_Handle handle, uint32_t event, uint32_t data, void *userArg)
The definition of a callback function used by the CAN driver. 
Definition: CAN.h:606
CAN Object. 
Definition: CAN.h:749
bool isOpen
Definition: CAN.h:765
uint32_t rxBufNum
Definition: CAN.h:759
void * userArg
Definition: CAN.h:753
Structure for MCAN Standard Message ID Filter Element. 
Definition: MCAN.h:1158
CAN hardware attributes. 
Definition: CAN.h:775
uint_least8_t rxPin
Definition: CAN.h:791
uint32_t eventMask
Definition: CAN.h:752
uint32_t txFifoQNum
Definition: CAN.h:642
void CAN_init(void)
This function initializes the CAN module. 
int_fast16_t CAN_enableLoopbackInt(CAN_Handle handle)
Enables internal loopback test mode. 
uint32_t intPriority
Definition: CAN.h:788
struct CAN_Config_ * CAN_Handle
A handle that is returned from a CAN_open() call. 
Definition: CAN.h:579
uint32_t nsjw
Definition: CAN.h:714
MCAN_StdMsgIDFilterElement * stdMsgIDFilterList
Definition: CAN.h:625
uint32_t txPinMux
Definition: CAN.h:790
uint32_t dtSeg1
Definition: CAN.h:665
Structure for MCAN Extended Message ID Filter Element. 
Definition: MCAN.h:1213
uint32_t tsPrescaler
Definition: CAN.h:738
bool enableCANFD
Definition: CAN.h:777
StructRingBuf_Object txStructRingBuf
Definition: CAN.h:763
uint32_t dbrp
Definition: CAN.h:659
int_fast16_t CAN_write(CAN_Handle handle, const CAN_TxBufElement *elem)
Sends CAN message using the Tx FIFO/Queue. 
uint32_t dtSeg2
Definition: CAN.h:669
size_t txRingBufSize
Definition: CAN.h:786
CAN Message RAM configuration. 
Definition: CAN.h:619
struct CAN_Config_ CAN_Config
CAN Global configuration. 
CAN_Object * object
Definition: CAN.h:806
CAN_Handle CAN_open(uint_least8_t index, CAN_Params *params)
Initializes a CAN driver instance and returns a handle. 
uint32_t txEventFifoNum
Definition: CAN.h:647
const CAN_DataBitRateTimingRaw * dataTiming
Definition: CAN.h:720
uint32_t tdcFilterWinLen
Definition: CAN.h:683
CAN Global configuration. 
Definition: CAN.h:803
uint32_t txFifoQNum
Definition: CAN.h:757
Structure for bit timing parameters. 
Definition: MCAN.h:441
uint32_t ntSeg2
Definition: CAN.h:710
uint32_t extFilterNum
Definition: CAN.h:623
MCAN_TxBufElement CAN_TxBufElement
A CAN Tx buffer element struct for CAN_write() and CAN_writeBuffer(). 
Definition: CAN.h:564
CAN_EventCbk eventCbk
Definition: CAN.h:739
MCAN_RxBufElement CAN_RxBufElement
A CAN Rx buffer element struct for CAN_read(). 
Definition: CAN.h:559
Structure for MCAN Tx Event FIFO element. 
Definition: MCAN.h:1106
Structure defining the raw MCAN CAN FD data phase bit rate configuration. 
Definition: CAN.h:657
uint32_t txFifoQMode
Definition: CAN.h:644
int_fast16_t CAN_enableLoopbackExt(CAN_Handle handle)
Enables external loopback test mode. 
const CAN_BitRateTimingRaw * bitTiming
Definition: CAN.h:737
uint32_t dsjw
Definition: CAN.h:673
uint32_t dataBitRate
Definition: CAN.h:781
uint32_t intMask
Definition: CAN.h:754
uint_least8_t txPin
Definition: CAN.h:792
Definition: StructRingBuf.h:45
const CAN_MsgRamConfig * msgRamConfig
Definition: CAN.h:736
void * rxRingBufPtr
Definition: CAN.h:783
const uint_least8_t CAN_count
size_t rxRingBufSize
Definition: CAN.h:785
MCAN_BitTimingParams CAN_BitTimingParams
A CAN bit timing struct for CAN_getBitTiming(). 
Definition: CAN.h:574
bool enableBRS
Definition: CAN.h:778
uint32_t txBufNum
Definition: CAN.h:756
uint32_t rxPinMux
Definition: CAN.h:789
void CAN_Params_init(CAN_Params *params)
Initializes the CAN_Params struct to its default values. 
MCAN_ExtMsgIDFilterElement * extMsgIDFilterList
Definition: CAN.h:627
bool rejectNonMatchingMsgs
Definition: CAN.h:779
void * txRingBufPtr
Definition: CAN.h:784
uint32_t stdFilterNum
Definition: CAN.h:621
int_fast16_t CAN_read(CAN_Handle handle, CAN_RxBufElement *elem)
Reads a received CAN message. 
uint32_t nominalBitRate
Definition: CAN.h:780
Structure for MCAN Tx Buffer element. 
Definition: MCAN.h:896
uint32_t ntSeg1
Definition: CAN.h:706
uint32_t eventMask
Definition: CAN.h:740
uint32_t txBufNum
Definition: CAN.h:640
uint32_t txEventFifoNum
Definition: CAN.h:758
int_fast16_t CAN_writeBuffer(CAN_Handle handle, uint32_t bufIdx, const CAN_TxBufElement *elem)
Sends CAN message using a dedicated Tx Buffer. 
void * userArg
Definition: CAN.h:741
StructRingBuf_Object rxStructRingBuf
Definition: CAN.h:762
Structure defining the raw MCAN bit rate configuration. 
Definition: CAN.h:699
void CAN_close(CAN_Handle handle)
Closes a CAN peripheral specified by handle. 
int_fast16_t CAN_readTxEvent(CAN_Handle handle, CAN_TxEventElement *elem)
Reads the next available CAN Tx Event FIFO element. 
void CAN_getBitTiming(CAN_Handle handle, CAN_BitTimingParams *bitTiming, uint32_t *clkFreq)
Get the CAN bit timings and functional clock frequency. 
Structure for MCAN Rx Buffer element. 
Definition: MCAN.h:998
Hardware abstraction layer for M_CAN Controller v3.2.1. 
int_fast16_t CAN_disableLoopback(CAN_Handle handle)
Disables loopback test mode. 
uint32_t tdcOffset
Definition: CAN.h:677
CAN_EventCbk eventCbk
Definition: CAN.h:751
const CAN_Config CAN_config[]
const CAN_HWAttrs * hwAttrs
Definition: CAN.h:809
uint32_t rxBufNum
Definition: CAN.h:637
CAN Parameters. 
Definition: CAN.h:734