![]() |
![]() |
LittlevGL
3.30.00.06
|
LittlevGL is an open source project, which provides everything you need to create a Graphical User Interface (GUI) on embedded systems with easy-to-use graphical elements, beautiful visual effects and low memory footprint.
This LittleVGL API Guide is generated from the open source code. For a complete LittlevGL usage documentation, please reference LittlevGL project's own documentation.
Texas Instruments repackages LittlevGL for use in the SimpleLink SDK Software ecosystem and has written some LittlevGL drivers for custom display controllers:
Interfaces | Controllers |
---|---|
SPI | SSD2119 |
LS013B7DH03 |