xWRL684x MMWAVE-L-SDK  06.01.00.05
Code Composer Studio (CCS) Setup and Usage Guide

Introduction

This guide will walk you through:

  1. Downloading and installing Code Composer Studio (CCS)
  2. Configuring CCS for the xWRL684x processor
  3. Creating target configurations
  4. Building examples using CCS
  5. Loading and running applications via CCS

Downloading and Installing CCS

Step 1: Download CCS

  1. Go to the CCS download home page
  2. Download CCS 20.3.1
  3. Extract the downloaded package to a location on your computer

Step 2: Install CCS

  1. Launch the installer by double-clicking the extracted installer file
  2. Follow the installation wizard
  3. Installation Directory: We recommend using the default installation path
  4. Setup Type: Select "Custom" installation type
  5. Component Selection: Make sure to select "mmwave" components to install xWRL684x related emulation and GELs
  6. Complete the installation process
  7. Launch CCS and select a workspace (the default is recommended)
    • You can check "Use this as default and do not ask again" if desired

Verifying Component Installation

To ensure all necessary components are correctly installed and detected by CCS:

Step 1: Check SysConfig Installation

  1. In CCS, go to File > Preferences > Code Composer Studio Settings
    CCS Preferences
  2. Navigate to General > Products
    CCS Products
  3. Verify that SysConfig 1.25.0 is listed

Step 2: Check Compiler Installation

  1. In the Preferences window, navigate to General > Compilers
    CCS Compilers
  2. Verify that TI CLANG 4.0.4.LTS is listed

Creating Target Configuration for xWRL684x

The target configuration connects CCS to your EVM. Follow these steps to create one:

Step 1: Copy Device Configuration File

  1. Delete the existing awrl68xx.xml and iwrl68xx.xml in C:/ti/ccs2031/ccs/ccs_base/common/targetdb/devices
  2. Copy the awrl68xx.xml and iwrl68xx.xml file from ${SDK_INSTALL_PATH}/tools/CCS_SupportFiles
  3. Paste the to C:/ti/ccs2031/ccs/ccs_base/common/targetdb/devices folder

Step 2: Import Target Configuration

  1. In CCS, go to Debug > Target Configuration
    Target Configuration
  2. In the Target Configuration window, click on the   button
  3. Browse to ${SDK_INSTALL_PATH}/tools/CCS_SupportFiles
  4. Select the xwrl68xx_xds110.ccxml file and click "Open"

Alternatively, you can create a new configuration manually:

Step 2 (Alternative): Create New Target Configuration

  1. In CCS, go to Debug > Target Configuration
  2. In the Target Configuration window, click on the "+" button
    Target Configuration
  3. Give your configuration a descriptive name (e.g., "xwrl68xx_xds110")
  4. Select connection as "XDS110 USB Debug Probe"
  5. In "Board or Device" dropdown, select "AWRL68xx" or "IWRL68xx"
  6. Save and close the configuration

UART Terminal Setup

To view debug output from your applications:

  1. In CCS, go to View > Console > Serial Console
  2. Click the   button
  3. In the dialog:
    • Set the serial port to the COM port connected to your EVM
    • Set baud rate to 115200
    • Set Data Size to 8
    • Set Stop bits to 1
    • Set Parity to None
  4. Click "OK" to open the terminal connection

Building Examples

You can build examples using either makefiles (command line) or CCS projects.

Building with Makefiles

  1. Open a command prompt (Windows) or terminal (Linux)
  2. Navigate to the SDK installation directory:
    cd ${SDK_INSTALL_PATH}
  3. Build the example using gmake (Windows) or make (Linux):
    # Windows example:
    gmake -s -C examples/hello_world/xwrL684x-evm/r5fss0-0_freertos/ti-arm-clang
    # Linux example:
    make -s -C examples/hello_world/xwrL684x-evm/r5fss0-0_freertos/ti-arm-clang

Building with CCS Projects

  1. In CCS, go to File > Import Project(s)
    Import Projects
  2. Click "Browse" and navigate to ${SDK_INSTALL_PATH}/examples/hello_world
  3. Select the project hello_world_xwrL684x-evm_r5fss0-0_freertos_ti-arm-clang
  4. Click "Finish" to import the project
  5. Right-click on the imported project and select "Build Project"

For additional details on importing of projects refer to Import a Project in CCS

Building System Projects

System projects combine multiple cores (APPSS, FECSS, C66SS) into a single metaimage:

Using Makefiles:

cd ${SDK_INSTALL_PATH}
gmake -s -C examples/drivers/uart/uart_echo/xwrL684x-evm/system_freertos

Using CCS:

  1. Import the system project from ${SDK_INSTALL_DIR}/examples/uart/uart_echo
  2. Select the project uart_echo_{board}_system_{os}
  3. The individual R5F and C66 projects will be imported automatically
  4. Right-click on the system project and select "Build Project"
    • This will automatically build the individual R5F and C66 projects

Rebuilding Libraries

If you modify source files within libraries:

cd ${SDK_INSTALL_PATH}
gmake -s libs PROFILE=debug # for debug mode libraries
# OR
gmake -s libs PROFILE=release # for release mode libraries

Loading and Running Examples

Step 1: Launch Target Configuration

  1. In CCS, go to Debug > Target Configurations
  2. Right-click your target configuration file (e.g., "xwrl68xx_xds110.ccxml") and select "Start Project-less Debug"
    Project Less Debug
  3. The target will appear in the Threads window

Step 2: Power On and Connect

  1. Power ON the EVM
  2. In the Threads window, right-click on "Cortex_R5_0" / "C66xx_DSP" and select "Connect Target"
    Threads Window

Step 3: Reset and Load Program

  1. Right-click on the connected CPU and select "Reset > CPU Reset"
    CPU RESET
  2. Left-click on the connected CPU and select "Run > Load Load Program"
    Load Program

Step 4: Select the Program

For makefile builds:

  1. Click "Browse" and navigate to your built executable
    • Example: ${SDK_INSTALL_PATH}/examples/hello_world/xwrL684x-evm/r5fss0-0_freertos/ti-arm-clang/hello_world.release.out

Step 5: Run the Program

  1. After loading, the execution will halt at the main() function
  2. Click the   button to run the program
  3. View program output in the Console or Terminal window

Reloading Programs

To reload or run a different program:

  1. Reset the CPU before loading a new program
  2. In most cases, you don't need to power cycle the EVM
  3. If the CPU or device is in an exception state, power cycle the EVM and start over

Troubleshooting

Common Setup & Usage Issues and Solutions

Problem: SysConfig not showing in CCS Products list
Solution: Refer to Check Packages as seen by CCS

Problem: Cannot connect to target
Solution:

  1. Verify power to the EVM
  2. Check JTAG cable connections
  3. Ensure boot mode switches are correctly set
  4. Close and reopen CCS, then try again

Problem: Program fails to execute after loading
Solution:

  1. Check console for error messages
  2. Verify EVM is properly initialized
  3. Reset CPU and reload the program
  4. As a last resort, power cycle the EVM and start over

Next Steps

After successfully setting up CCS and running examples: