Introduction to Safety#

Brief#

Functional Safety is the reduction of unnecessary risk due to hazards caused by malfunctioning behavior of electronic safety systems. The International Electrotechnical Commission (IEC) created the standard IEC 61508 which defines methods on how to create systems which enable functional safety. In addition, the International Organization for Standardization (ISO) created an adaptation of this standard for automotive product development, ISO 26262. In this module, we will discuss how TI AM26x Microcontrollers enable functional safety applications, what resources are provided by TI for functional safety, and additional relevant standards.

As the automotive and industrial markets become more autonomous, they face an increasing need to meet stricter functional safety standards. These standards are designed to minimize equipment failures and physical injury that could result from two types of hardware faults, systematic faults and random hardware faults.

Please refer the device datasheet to read more.

Safety Integration Levels#

Functional safety involves a safety integrity level (SIL) or other similar quantitative metric. A SIL applies to a safety function from start to finish, and affirms that the system reverts to a safe state or performs even during incorrect operation or a loss of functionality (in fault-tolerant architectures). Both the design and process must follow functional safety standards such as IEC 61508 or ISO 26262, and pass independent functional safety audits in order to achieve the corresponding quantitative metrics that assess appropriate safety standards.

TI AM26x Microcontroller sensors are designed according to an extensive hardware and software development process and are supported by device certification from Technischer Überwachungsverein (TÜV) SÜD.

Industrial Portfolio SIL Ratings#

Device

Hardware Capabilities

Systematic Capability

Third Party Assessment + Device Certification

AM263x

SIL-3

SIL-3

(TÜV) SÜD

AM263Px

SIL-3 Targeted

SIL-3 Targeted

(TÜV) SÜD (In Progress)

Automotive Portfolio ASIL Ratings#

Device

Random Hardware Capabilities

Systematic Capability

Third Party Assessment + Device Certification

AM263x

ASIL-D

ASIL-D

(TÜV) SÜD

AM263x

ASIL-D Targeted

ASIL-D Targeted

(TÜV) SÜD (In Progress)

Safety Responsibility: Who does What?#

Texas Instruments, assessors, and system integrators/customers all play a role in safety.

Texas Instruments#

TI has developed Functional Safety rated hardware and software via development processes which are certified by a Functional Safety assessor. Additionally, TI provides documentation, certificates, and relevant support packages to customers.

Below is a list of resources provided with TI Functional Safety compliant microcontrollers, organized by where to find them.

Resource Name

Resource Type

Location

TI Certificate for Functional Safety Hardware Development Process

Document

ti.com Functional Safety Home

TI Certificate for Functional Safety Software Development Process

Document

ti.com Functional Safety Home

Safety Diagnostics Library

Software Package

ti.com Product page (MCU_PLUS_SDK)

References#