Camera#

The Camera module will showcase how you can capture a video using a USB camera, a CSI-2 camera, or an FPD-Link camera.

USB UVC Camera#

Plug in a USB UVC compliant camera and boot the EVM to Linux. Use the v4l2-ctl command to verify the camera is detected:

# v4l2-ctl --list-devices
TI-CSI2RX (platform:30102000.ticsi2rx):
        /dev/media0

wave5-dec (platform:wave5-dec):
        /dev/video0

wave5-enc (platform:wave5-enc):
        /dev/video1

HD Web Camera: HD Web Camera (usb-xhci-hcd.1.auto-1):
        /dev/video2
        /dev/video3
        /dev/media1

GStreamer can be used to capture the video. The captured video can be simultaneously sent to the HDMI display if a display is connected. Below is an example of using GStreamer to stream video (make sure to change videoX to the actual video device number) to a display using kmssink or waylandsink:

# gst-launch-1.0 v4l2src device="/dev/videoX" ! video/x-raw, width=640, height=480, format=UYVY ! kmssink driver-name=tidss force-modesetting=true
# gst-launch-1.0 v4l2src device="/dev/videoX" ! video/x-raw, width=640, height=480 ! waylandsink

The captured video can also be stored to a file and played out on the host PC. Instead of using kmssink as the GStreamer sink, a file sink can be used, for example:

# gst-launch-1.0 v4l2src num-buffers=50 device="/dev/videoX" ! video/x-raw, width=640, height=480 ! filesink location=cam-cap.yuv

Then the captured file can be played out on the host PC using an application such as mplayer:

$ mplayer -demuxer rawvideo -rawvideo w=640:h=480:format=yuy2 cam-cap.yuv

CSI-2 Camera#

AM62Ax supports MIPI CSI-2 compliant cameras. The AM62Ax starter kit (SK) EVM has a CSI-2 camera connector that is compatible with the Raspberry Pi camera interface.

Connect a CSI-2 Camera to the EVM

The CSI-2 camera connector is located at the bottom side of the EVM. A CSI-2 camera can be connected to the EVM as shown below:

../../../_images/Academy_Eval_imx219_am62ax_sk.png

Note

The CSI-2 camera connector on the AM62A SK EVM is a 22-pin FFC connector. For a camera with 15-pin FFC connector, a 15-pin to 22-pin flat flex cable is needed to connect the camera to the EVM.

Apply Device Tree Overlay

Since any camera can be connected to the EVM, the base dtb in the Processor SDK does not include the device tree node for any particular camera sensor. Therefore, the device tree node for a particular sensor should be added in as an overlay. The Processor SDK contains the device tree overlays for a few sensors, as shown below:

root@am62axx-evm:/boot/dtb/ti# ls k3-am62*-sk-csi2*.dtbo
k3-am62a7-sk-csi2-ox05b1s.dtbo  k3-am62x-sk-csi2-imx219.dtbo  k3-am62x-sk-csi2-ov5640.dtbo  k3-am62x-sk-csi2-tevi-ov5640.dtbo

The device tree overlay can be applied in either one of the following two ways:

  1. Open file /run/media/BOOT-mmcblk1p1/uEnv.txt and add the following line at the end of the file, and reboot the EVM:

name_overlays=ti/k3-am62x-sk-csi2-imx219.dtbo
  1. Reboot the EVM and stop at U-Boot prompt, and add the following environment variable:

=>setenv name_overlays ti/k3-am62x-sk-csi2-imx219.dtbo
=>boot

Verify the Camera Is Detected

Boot the EVM to Linux and use the v4l2-ctl --list-devices command to verify the camera is detected. The command should return something similar to below:

# v4l2-ctl --list-devices
j721e-csi2rx (platform:30102000.ticsi2rx):
        /dev/video3
        /dev/video4
        /dev/video5
        /dev/video6
        /dev/video7
        /dev/video8
        /dev/media0

e5010 (platform:e5010):
        /dev/video2

wave5-dec (platform:wave5-dec):
        /dev/video0

wave5-enc (platform:wave5-enc):
        /dev/video1

The above command displays multiple video nodes (/dev/videoX). Each of these video nodes corresponds to a logical stream of data. If the camera is the only connected CSI-2 camera, then the first node under j721e-csi2rx should be used to stream.

For cameras supported by the SDK, script /opt/edgeai-gst-apps/scripts/setup_cameras.sh, which runs automatically after boot, will detect and set up the camera automatically. For example, IMX219 would be detected and configured after boot as below:

IMX219 Camera 0 detected
device = /dev/video-imx219-cam0
name = imx219
format = [fmt:SRGGB8_1X8/1920x1080]
subdev_id = /dev/v4l-imx219-subdev0
isp_required = yes

Both the device alias “/dev/video-imx219-cam0” and subdev_id alias “/dev/v4l-imx219-subdev0” can be used in the Gstreamer pipepline as shown in the below section.

Capture Video

Because the IMX219 is a raw image sensor, the ISP on the SoC needs to be used in order to stream video. Below shows an example of streaming video from an IMX219 camera:

# gst-launch-1.0 v4l2src device=/dev/video-imx219-cam0 io-mode=dmabuf-import ! \
  video/x-bayer, width=1920, height=1080, framerate=30/1, format=rggb ! \
  tiovxisp sink_0::device=/dev/v4l-imx219-subdev0 sensor-name="SENSOR_SONY_IMX219_RPI" \
  dcc-isp-file=/opt/imaging/imx219/linear/dcc_viss.bin \
  sink_0::dcc-2a-file=/opt/imaging/imx219/linear/dcc_2a.bin format-msb=7 ! \
  video/x-raw, format=NV12, width=1920, height=1080, framerate=30/1 ! \
  kmssink driver-name=tidss sync=false

For more details on configuring the sensor to different formats, please refer to Camera Development section.

Tested CSI-2 Cameras#

The following CSI-2 camera modules have been tested with the AM62A starter kit.

OX05B1S

../../../_images/Academy_Eval_ox5b_am62a_sk.png

IMX219

OV5647