Boot Mode#
This module will discuss and reference to different bootmode supported.
As detailed in the AM62Ax Technical Reference Manual (TRM), the ROM bootloader supports several boot modes, which can be broadly classified as:
Memory boot modes
Host boot modes
During a memory boot, the device (AM62Ax) transfers the second bootloader from non-volatile memory, such as, SDCard, eMMC, OSPI/QSPI/SPI flash, or GPMC flash.
During a host boot, the device (AM62Ax) is configured to receive the second bootloader from a host via the selected interface, such as UART or USB(DFU).
The following sections describe the usage of these boot modes in details.
Commonly used boot mode switch settings on the AM62Ax EVM are also listed at the end of the section for quick reference.