EVM Boot Mode Switches#
This section provides the boot mode switch settings for a few commonly used boot modes.
There are multiple ways (boot modes) to boot Linux on an EVM (from a micro SD card, eMMC, UART, etc.). The boot mode is defined by the boot mode switches on the EVM. The supported boot modes and the corresponding boot mode switch settings can be found in the EVM User’s Guide.
Boot Mode |
EVM Boot Mode Switches Setting |
---|---|
SD card boot |
|
eMMC boot |
|
USB Host Boot |
|
USB Peripheral boot |
|
xSPI boot |