SD Card Boot#

This modules explains SD card boot mode.

While it is not used in final products, SD Card boot is often used in EVMs and development platforms. This section demonstrates how to boot TI EVMs to the Linux prompt from an SD card.

In this module, we will be focusing specially for AM62Px.

Bootable SD Card Format

The bootable SD card should have at least two partitions.

  • The first partition holds the U-Boot binaries, and uEnv.txt for customizing the U-Boot environment if needed. This partition should be in FAT format.

  • The second partition holds the contents of the root filesystem. This partition should be in EXT4 format.

Here is an example of bootable SD card partition information:

dev@uda:~$ sudo fdisk -l /dev/sdd

Disk /dev/sdd: 14.9 GiB, 15931539456 bytes, 31116288 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x9dd92e0f

Device     Boot  Start     End Sectors  Size Id Type
/dev/sdd1  *      2048  145407  143360   70M  c W95 FAT32 (LBA)
/dev/sdd2       145408 8032255 7886848  3.8G 83 Linux

Create Bootable SD Card

A bootable SD card can be created manually using fdisk and mkfs commands in Linux based on the format requirement above.

The Processor SDK for AM62Px provides a script bin/create-sdcard.sh, which simplifies this SD card creation process. The script partitions and formats the SD card, and copy the U-Boot binaries and root filesystem content to the corresponding partitions of the SD card.

The Process SDK for AM62Px also provides standalone bootable SD card WIC images which can be downloaded from the Processor SDK release page on ti.com. These WIC images can be flashed to an SD card in Windows or Linux host without installing the entire Processor SDK package. Refer to Create a Linux Bootable SD Card for the flashing details.

SD Card Boot Procedure

Refer to EVM Boot Mode Switches to set the AM62Px EVM boot mode switches to SD Card boot.

Insert the bootable SD card to the EVM SD Card slot, then power on the EVM. Linux will boot from the SD card all the way to the login prompt.