Booting Remote Cores#
This section discusses booting remote cores from Linux, using the standard Linux SDK SPL boot flow.
If using the SBL boot flow that can be found in the MCU+ SDK, then remote cores can be initialized by the SBL boot instead.
Linux can boot remote cores during Linux boot, or during Linux runtime.
Reference section Development & debug through CCS for information about booting remote cores from CCS.
Booting Remote Cores During Linux Boot#
In normal operation, the boot loader (U-Boot) boots and loads Linux onto the A53 cores of the AM62x. If the remote cores are enabled in the Linux devicetree, then Linux will use the RemoteProc driver to boot the remote cores during Linux kernel boot time. Reference section Linux Boot Flow for more information about the Linux boot flow.
The Linux devicetree tells the RemoteProc driver which firmware files to load into the remote cores.
Note
The wakeup R5F core (or DM R5F) is different. That core runs device manager (DM) software which is critical for the rest of the processor to function. Thus, the DM R5F core is not initialized by Linux. Instead, the DM R5F is integrated as a part of the tispl.bin binary, and is started earlier in the boot process.
By default, the Linux RemoteProc looks for these files:
Core Name |
RemoteProc Name |
Description |
Firmware File Name |
|---|---|---|---|
M4F |
5000000.m4f |
M4F core |
am62-mcu-m4f0_0-fw |
DM R5F |
78000000.r5f |
R5F core (wakeup domain) |
not loaded by Linux |
The above files are generally soft linked to the intended firmware on a root file system. For example:
root@am62xx-evm:~# ls -l /lib/firmware
...
lrwxrwxrwx 1 root root 72 Mar 9 2018 am62-mcu-m4f0_0-fw -> /usr/lib/firmware/ti-ipc/am62xx/ipc_echo_test_mcu2_0_release_strip.xer5f
Booting Remote Cores from the Linux Console or User Space#
To reload a remote core with new executables, please follow the below steps.
First, identify the remotproc node associated with the remote core:
# head /sys/class/remoteproc/remoteproc*/name
Then, use the sysfs interface to stop the remote core. For example, to stop the core at remoteproc1:
# echo stop > /sys/class/remoteproc/remoteproc1/state
Note
The RemoteProc driver only supports using “echo stop” to shut down a remote core if graceful shutdown has been enabled in the remote core firmware. The other option to load new binaries into a remote core is to update the symbolic link with the new firmware (if needed), and reboot the board. For more information about graceful shutdown, refer to section Graceful shutdown.
Note that the DM R5F cannot be stopped during runtime. The processor must be rebooted in order to load new firmware into the DM R5F.
If needed, update the symbolic link in the /lib/firmware/ folder to
point to a new firmware:
# ln -sf /full/path/to/firmware_name symbolic_link_name
Finally, use the sysfs interface to start the remote core:
# echo start > /sys/class/remoteproc/remoteproc1/state
The full process on AM62x looks like this:
root@am62xx-evm:~# head /sys/class/remoteproc/remoteproc*/name
==> /sys/class/remoteproc/remoteproc0/name <==
5000000.m4fss
==> /sys/class/remoteproc/remoteproc1/name <==
30074000.pru
==> /sys/class/remoteproc/remoteproc2/name <==
30078000.pru
Let’s load an IPC example onto the M4F core. If the firmware already running on the M4F core has graceful shutdown enabled, then we can use the sysfs interface to restart the remote core:
root@am62xx-evm:~# echo stop > /sys/class/remoteproc/remoteproc0/state
[ 440.832317] remoteproc remoteproc0: stopped remote processor 5000000.m4fss
root@am62xx-evm:~# cd /lib/firmware
root@am62xx-evm:/lib/firmware# ln -sf /usr/lib/firmware/ti-ipc/am62xx/ipc_echo_test_mcu2_0_release_strip.xer5f
root@am62xx-evm:~# echo start > /sys/class/remoteproc/remoteproc0/state
[ 450.930070] remoteproc remoteproc0: powering up 5000000.m4fss
[ 450.936112] remoteproc remoteproc0: Booting fw image am62-mcu-m4f0_0-fw, size 78960
[ 450.960447] remoteproc0#vdev0buffer: assigned reserved memory node m4f-dma-memory@9cb00000
[ 450.969408] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 450.975089] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[ 450.975850] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 450.982840] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[ 450.988824] remoteproc remoteproc0: remote processor 5000000.m4fss is now up