Modify the remote core application to be loaded by Linux#
This module discusses how to modify an MCU+ application, so that the remote core can be initialized by the Linux Remoteproc driver.
Note
There are multiple ways for a remote core to be initialized. For information on other initialization methods, refer to section Booting and Disabling Processor Cores.
Note
The Linux remoteproc driver cannot be used to load firmware into the DM R5F cores. Those cores are loaded by the bootloader before Linux initialization begins.
The MCU+ project can be loaded successfully using CCS. However, if the binary is loaded by the Linux Remoteproc driver, initialization will fail. The Remoteproc driver will fail to initialize the remote core because the MCU+ project does not include a resource table.
Once a resource table has been added and the linker.cmd file has been updated, ensure that Linux and the MCU+ project agree on peripheral and memory allocation.