Build Kernel#

This module explains how to compile kernel.

During Linux development, the kernel source code may need to be modified and recompiled. For example, the kernel needs to be recompiled if:

  • Enabling features which are disabled in the kernel defconfig

  • Disabling features which are enabled in the kernel defconfig

  • Modifying kernel source code to port kernel to a custom board

There are two methods to build the kernel in the Processor SDK:

  • Using the SDK top level Makefile

  • Using the kernel top level Makefile

The first method wraps the build steps in the second method to two commands, which is convenient but has a down side that it reduces the customization capability which the second method has. Therefor, pick the method which fits the use case.

Build Kernel Using the SDK Top Level Makefile#

$ cd <SDK_INSTALL_DIR>/
$ make linux
$ sudo DESTDIR=<sdcard-mounting-point> make linux_install

Build Kernel Using the Kernel Top Level Makefile#

Once the Processor SDK Linux package is installed, the kernel source code is under <SDK_INSTALL_DIR>/board-support/linux-<version>/. Please refer to Processor SDK Documentation Kernel User Guide for how to compile the kernel for AM62x in the kernel source code directory.