How to allocate memory#
Linux and all remote cores must agree on how memory is divided between cores.
Note
The information on this page ONLY applies to SDK 9.1 or later! If you are using AM64x SDK 9.0 or earlier, please refer to the SDK 9.0 version of the AM64x academy. Here are the steps to access the SDK 9.0 version:
On the Left-hand menu, hover your mouse over “AM64x Academy”. Three dots will show up to the right of the label. Click on the 3 dots, and go to “Manage Versions”. Select AM64x Academy, Version 9.00.00.00 v2.
In the Left-hand menu, you should now see “AM64x Academy - 9.00.00.00 v2”