Analog to Digital Converter (ADC) Lab#

Link to share

The objective of this lab is to gain familiarity with the on-chip analog-to-digital converter (ADC) module. The microcontroller (MCU) will be setup to sample a single ADC input channel at a prescribed sampling rate and store the conversion result in a circular memory buffer. In the optional second part of this lab exercise, the digital-to-analog converter (DAC) will be explored. This lab should leave readers more knowledgeable about the capabilities of the ADC and DAC modules, as well as how the analog subsystem commonly interacts with other modules.

Solution#

All C2000 Academy lab software solutions are located in the directory: [C2000Ware_Install_Path]/training/device/[device_name].

Overview#

In this lab, one of the ePWM modules will be set up to trigger a start-of-conversion (SOC) signal for the ADC. The ADC will then start sampling its input at a desired sampling rate. The ADC will use an end-of-conversion (EOC) interrupt to prompt the CPU to copy the results of the ADC conversion into a results buffer in memory. This buffer pointer will be managed in a circular fashion, so that new conversion results will continuously overwrite the oldest conversion results in the buffer. In order to generate an interesting input signal, the code will also toggle a GPIO high and low in the ADC interrupt service routine (ISR). This GPIO pin will be connected to the ADC as the input to be sampled. In an additional optional portion of the lab, the digital-to-analog converter (DAC) can be used to generate a sinusoidal wave which can then be sampled by the ADC.

Lab Objective

Lab Setup#

Hardware Setup#

Required hardware for this lab:

  • A C2000 controlCARD or LaunchPad with the supplied USB cable.

  • Jumper cables (2).

Using the supplied USB cable, connect the USB Micro or Mini Type-B connector into your C2000 board and the USB Standard Type-A connector into your computer’s USB port (please note that controlCARD docking stations may require an additional power supply connection). You should see some LEDs light up on the board. This connection will power the board and provide a JTAG communication link between your device and CCS. Refer to Getting Started module for more details if needed.

Software Setup#

Required computer software installation for this lab:

Note:

This lab requires CCS version 11 or higher as well as a C2000Ware version 4 or higher.

Start a CCS Project#

First, import an empty project from C2000Ware to a CCS workspace:

  1. Open CCS and go to Project→Import CCS Projects. A new window should appear. Ensure that the Select search-directory option is activated.

  2. Click the Browse button and select the [C20000ware_Install_dir]/training/device/[device]/empty_lab directory.
    Note that the default Windows [C20000ware_Install_dir] is C:/ti/c2000/C2000Ware_x_xx_xx_xx.

  3. Under Discovered Projects, you should now see the lab_[board]_[device] project. Select the appropriate project for either the controlCARD or the launchpad.

Discovered_Projects

  1. Click Finish to import and copy the lab_[board]_[device] project into your CCS workspace.

  2. After the project has been imported, the project explorer window should look like below:

Projects_explorer

  1. Rename the project to your liking

    • Right-click on the project in “Project Explorer” pane. Select ‘Rename’ from the drop down menu and rename the project to ‘c2000_adc_lab’ or a name of your choosing.

    • Now click the ‘Down Arrow’ located to the left of the imported project to expand it and select lab_main.c. Right-click on the file, and select ‘Rename’ to rename the file to c2000_adc_lab_main.c or a name of your choosing.

Configure the GPIOs#

We will begin this ADC lab exercise by configuring the three required GPIOs:

  • GPIO 16 will always remain high

  • GPIO 3 will toggle between a high and low state

  • The third GPIO will be used as an LED indicator.

First, configure GPIO16 as an output that is pulled constantly high and is serving as one of the possible ADC inputs. Double click the .syscfg file within the project to open it. Within SysConfig perform the following steps:

  • Add a GPIO by clicking the (+) icon next to ‘GPIO’ on the left pane

  • Set the name of the GPIO as ‘myGPIOHigh’

  • Set the GPIO as an output

  • Set the Pin Type as “Pull-up enabled in input mode”

  • Check the box to enable a write of an initial value

  • Set the initial value as “1: GPIO state is HIGH”

../../../_images/SysConfigGPIO16.png


We have to specify which GPIO we are configuring, in this case GPIO16. Upon expanding the “PinMux” view we can choose the desired GPIO. Follow the steps below:

  • Click on the three dot icon at the top right of the SysConfig window

  • Select “Preferences & Actions”

  • Under preferences, click on the ‘Device Pin Label’ drop down arrow and enable “Device pin name”. This is not part of the default SysConfig settings but allows us to see the pin name along with the pin number

  • Within the GPIO Mux select GPIO16 as the desired GPIO. The device pin number will vary depending on hardware.

../../../_images/SysConfigGPIO_16.png


Next, we can add a second GPIO (GPIO3). GPIO3 will be toggled in the application in order to serve as another possible input to the ADC. Follow the same steps as required to setup GPIO16, but name it “myGPIOToggle”.

../../../_images/SysConfigGPIO3.png

Note:

The device pin numbers on the images above may vary depending on the device used.

Lastly, is the addition of an LED GPIO. This LED will be toggled within the ISR to show that the code is executing properly.

  • In SysConfig, navigate to the “Hardware” tab

  • Click ‘+’ next to ‘LED’ to add an LED (it should be LED4/LED5 if using a LaunchPad, or D1/D2 if using a controlCARD)

  • The parameters should be filled like below. The name will be referenced in the ADC ISR, so make sure the name is ‘myBoardLED0_GPIO’.

../../../_images/sysconfig_led_1.png

Configure the ePWM#

The EPWM module will be used to automatically trigger an ADC SOC. The desired EPWM frequency is 50kHz. For more information on the PWM, please review the Control Peripherals module.

We will start by adding a PWM instance within Sysconfig by clicking on the (+) sign next to ‘EPWM’ within the left pane of Sysconfig. Setup the EPWM module in the following way:

../../../_images/SysConfigEPWMSetup.png


Now that we have added an EPWM instance, we will configure the EPWM ‘Timebase’ submodule as follows:

../../../_images/SysConfigEPWMTimebase.png

Note:

The image above is representative of the F2807x, F28004x, F2837xD, and F2837xS devices. For other devices the “Sync Out Pulse” default option may be different or there might be a “Sync In Pulse” option. For this lab, we are not configuring the “Sync Out Pulse” or “Sync In Pulse” so leaving all synchronization options at the default state is okay.

Secondly, we will enable ADC SOC triggering through the “Event-Trigger’ submodule as follows:

../../../_images/SysConfigEPWMEventTrigger.png

Configure the ADC#

To setup the ADC we need to add an ADC instance within SysConfig by clicking on the plus sign next to ADC on the left most pane of the SysConfig start menu. Setup the ADC in the following way:

../../../_images/SysConfigADCInit.png

Note:

The image above is for devices with an ADC-Type 4, for devices with an ADC Type-5 you will not have the ‘ADC Resolution Mode’ or ‘ADC Signal Mode options’

We will now configure the ADC SOC (start of conversion). The trigger for SOC0 is epwm1

../../../_images/SysConfigADC_SOCSetup.png


Next, we need to setup the ADC interrupt. In this case ADCINT1 will generate an interrupt at the end of the conversions (EOC). This is done in this way so that when we read the ADC results from within the ISR the ADC conversion results are ready.

../../../_images/SysConfigADC_InterruptConfig.png


Lastly, we need to setup the ADC interrupt. This is done by enabling the ADC interrupt and configuring the ADC interrupt handler name.

../../../_images/SysConfigADC_Interrupts.png
ASYSCTL

If your device has an ADC of Type-5 you will also need to configure ASYSCTL as shown below.

ASYSCTL

Program Setup#

Set Up the ADC ISR#

Now that we have configured the ADC and PWM modules within SysConfig, we can switch to the application code portion of this lab. Within the project, click on the .c file under the name you chose.

Within the .c file we need to write the code that will be executed every time there is an ADC interrupt, otherwise known as the ISR (interrupt service routine).

This project requires defining ADCBufPtr (variable used to place ADC results in the buffer). The following code is used to declare the variable within the ISR as well as the variable we will use to change the state of the LED. Copy the following code into your source .c file.

Note: The name of the ISR function is what we defined earlier within the SysConfig configuration for the ADC.

interrupt void INT_myADCA_1_ISR(void)
{
    static uint16_t *AdcBufPtr = AdcBuf;
    static volatile uint16_t LED_count = 0;

The next code is another piece of the ISR which is used to store the ADC results within the buffer. We also need to handle the case where our buffer becomes full. One way to do this is to overwrite previous values. Add the following code into your ISR.

    // Read the ADC Result
    *AdcBufPtr++ = ADC_readResult(myADCA_RESULT_BASE, myADCA_SOC0);
    // Brute Force the circular buffer
    if (AdcBufPtr == (AdcBuf + ADC_BUF_LEN))
    {
        AdcBufPtr = AdcBuf;
    }

The next step is to toggle a GPIO so that we can use this as an ADC input. Add the following code into your ISR.

    // Toggle the pin
    if(DEBUG_TOGGLE == 1)
    {
        GPIO_togglePin(myGPIOToggle);             
    }

Now we have the option to toggle an LED on the device. This will tell us that the program is functioning properly and indeed entering the ISR.

Notice how we toggle the LED whenever LED_count > 25000. This corresponds to ~ 0.5 sec/ toggle. We arrive at this by solving for x.

\((1/50000 \text{ sec/sample})*(1 \text { samples/interrupt})*(25000 \text{ interrupts/toggle}) = (\text{x sec/toggle})\)

\((1/50000 \text{ sec/sample})*(1 \text{ samples/interrupt})*(25000 \text{ interrupts/toggle}) = (0.5 \text{ sec/toggle})\)

Add the following code into your ISR.

    if(LED_count++ > 25000)                      // Toggle slowly to see the LED blink
    {
        GPIO_togglePin(myBoardLED0_GPIO);                   // Toggle the pin
        LED_count = 0;                           // Reset the counter
    }

Lastly, in the ISR, we must acknowledge the PIE group as well as clear the interrupt status flag so that we can continue to service interrupts in the future. Add the following code into your ISR.

    Interrupt_clearACKGroup(INT_myADCA_1_INTERRUPT_ACK_GROUP);
    ADC_clearInterruptStatus(myADCA_BASE, ADC_INT_NUMBER1);
} // End of ADC ISR

Note:

Notice that throughout the .c file, the naming convention generated by SysConfig was followed. Below is a snippet taken from the board.h file located within the project’s Generated Source files. Do not edit board.h directly, as your changes will be overwritten when the file is autogenerated from the .syscfg file.

SysConfig Naming Convention

Define Global Macros and Variables#

The last thing we have to do is define any variables we are using throughout the project and setup the content within main() which includes device initialization. Copy the following code into your source .c file.

We begin by including the sysconfig generated header file board.h. This should already be included by default. Do not edit board.h directly, as your changes will be overwritten when the file is autogenerated from the .syscfg file.

//
// Included Files
//
#include "board.h"

Then we define ADC_BUF_LEN, the length of our ADC value buffer and the buffer itself

//
// Global variables and definitions
//
#define ADC_BUF_LEN         50
uint16_t DEBUG_TOGGLE = 1;    // Used for real-time mode
uint16_t AdcBuf[ADC_BUF_LEN];  // ADC buffer allocation

Next, we need to declare the functions used within the project. In this project, SysConfig is used for all of the ADC/PWM setup so we only need to declare the ISR.

//
// Function Declarations
//
__interrupt void INT_myADCA_1_ISR(void);

Define main()#

Lastly, we define the contents within main() which includes device initialization and peripheral setup:

    void main(void)
    {
        // CPU Initialization
        Device_init();
        Interrupt_initModule();
        Interrupt_initVectorTable();
        // Configure the GPIOs/ADC/PWM through SysConfig generated function found within
        // board.c
        Board_init();
        // Enable global interrupts and real-time debug
        EINT;
        ERTM;
        // Main Loop
        while(1){}
    } 

Build and Run the Project#

Build the Code#

  • Make sure your board is connected to your computer. If you are using a LaunchPad then set the LaunchPad target configuration as the active one within the project. This is done by expanding the TargetConfigs folder within the folder and right-clicking on the LaunchPad ccxml and selecting “Set as Active Target Configuration”.

  • Click the “Build” button and watch the tools run in the Console window. Check for errors in the Problems window, and fix any that may have occurred.

  • Setup a debug and target configuration. For more information on launching a target configuration refer to Getting Started → “Build and Load the Project” → “Setup Target Configuration”.

Run the Code#

  • Press the debug button to transition into the debug perspective.

  • Now that you are in the debug perspective, the program should be paused at the first line of code in main(). Press the resume icon in order for the code to start running.

  • Open a memory browser by going to the top menu and selecting View and then Memory Browser from the drop down list. In memory browser search bar type &AdcBuf and enter. This will allow us to view the contents of the ADC results buffer.

../../../_images/memory_browser1.png

\

  • Using a jumper wire, connect the ADCINA0 pin to GND. Then run the code using the Resume button, and Suspend it after a few seconds. Verify that the ADC results buffer contains the expected value of ~0x0000.

ADCINA0 Pin#

Device

LaunchPad

ControlCARD

F28379D

30

9

F2838x

n/a

9

F28004x

70

9

F28002x

69

9

F28003x

70

9

F280013x

69

9

F280015x

69

9

F28P65x

30

9

F28P55x

70

9

Important

Exercise care when connecting any jumper wires to the LaunchPad or ControlCARD header pins since the power to the USB connector is on!

  • Adjust the jumper wire to connect the ADCINA0 pin to +3.3V or GPIO16 which we set high. Then Resume the code again, and Suspend it after a few seconds. Verify that the ADC results buffer contains the expected value of ~0x0FFF.

LaunchPad#

Device

ADCINA0 Pin

GPIO16 Pin

F28379D

30

33

F2838x

n/a

n/a

F28004x

70

15

F28002x

69

76

F28003x

70

76

F280013x

69

76

F280015x

69

76

F28P65x

30

15

F28P55x

70

51

ControlCARD#

Device

ADCINA0 Pin

GPIO16 Pin

F28379D

9

67

F2838x

9

67

F28004x

9

67

F28002x

9

67

F28003x

9

67

F280013x

9

67

F280015x

9

67

F28P65x

9

67

F28P55x

9

67

  • Adjust the jumper wire to connect the ADCINA0 to GPIO3. Then Resume the code again, and Pause it after a few seconds. Examine the contents of the ADC results buffer (the contents should be alternating ~0x0000 and ~0x0FFF values).

LaunchPad#

Device

ADCINA0 Pin

GPIO3 Pin

F28379D

30

37

F2838x

n/a

n/a

F28004x

70

55

F28002x

69

37

F28003x

70

37

F280013x

69

37

F280015x

69

37

F28P65x

30

79

F28P55x

70

37

ControlCARD#

Device

ADCINA0 Pin

GPIO3 Pin

F28379D

9

55

F2838x

9

55

F28004x

9

55

F28002x

9

55

F28003x

9

55

F280013x

9

55

F280015x

9

55

F28P65x

9

55

F28P55x

9

55

  • Open and set up a graph to plot a 50-point window of the ADC results buffer. Click: Tools → Graph → Single Time and set the following values (then press ok):

    • Acquisition Buffer Size: 50

    • Dsp Data Type: 16 bit unsigned integer

    • Sampling Rate Hz: 50000

    • Start Address: AdcBuf

    • Display Data Size: 50

    • Time Display Unit: us

    • Leave the other settings as their default value. Click OK and you should see the plot window open up.

../../../_images/graph_properties.png

Important

Note: If you do not see CCS menu Tools → Graph, please refer to Getting Started (Setting CCS for graph) to see the instruction on how to enable CCS graphing tool in your perspective.

Why does Code Composer Studio plot resemble a triangle wave? What is the signal processing term for what is happening here?

We are under sampling the signal. If we were to increase our sampling frequency we would see that it is actually a square wave.

  • Activate the Continuous Refresh option in the plot window.

  • You should now see several periods of the PWM waveform in the plot updating in real-time. If desired, you can use the measurement tool to verify that the duty cycle is 25% and the period is 500us. Leave the plot window open.

  • Recall that the code toggled the GPIO3 pin alternately high and low. If you had an oscilloscope available to display GPIO3, you would expect to see a square-wave.

../../../_images/toggled_pin_graph.png

Use Real-Time Emulation#

  • The memory and graph windows displaying AdcBuf should still be open. The jumper wire between ADCINA0 and GPIO3 should still be connected. In real-time mode, we will have our window continuously refresh at the default rate. To view the refresh rate click: Window → Preferences… and in the section on the left select the “Code Composer Studio” category. Click the sign (‘+’ or ‘>’) to the left of “Code Composer Studio” and select “Debug”. In the section on the right notice the default setting. Click Cancel.

Note:

Decreasing the “Continuous refresh interval” causes all enabled continuous refresh windows to refresh at a faster rate. This can be problematic when a large number of windows are enabled, as bandwidth over the emulation link is limited. Updating too many windows can cause the refresh frequency to bog down. In this case you can just selectively enable continuous refresh for the individual windows of interest.

../../../_images/continuous_refresh_rate.png

\

  • Next we need to enable the graph window for continuous refresh. Select the “Single Time” graph. In the graph window toolbar, left-click on the yellow icon with the arrows rotating in a circle over a pause sign. Note when you hover your mouse over the icon, it will show “Enable Continuous Refresh”. This will allow the graph to continuously refresh in real-time while the program is running.

../../../_images/continuous_refresh_button_graph_window.png

\

  • Enable the Memory Browser for continuous refresh using the same procedure as the previous step.

../../../_images/continuous_refresh_membrowser.png

\

  • To enable and run real-time emulation mode, click the “Enable Silicon Real-time Mode” toolbar button. A window may open and if prompted select Yes to the “Do you want to enable real-time mode?” question. This will force the debug enable mask bit (DBGM) in status register ST1 to ‘0’, which will allow the memory and register values to be passed to the host processor for updating (i.e. debug events are enabled).

../../../_images/realtime_enable.png

\

  • While in real-time mode, carefully remove and reconnect the jumper wire. The values should be continuously updating in the memory browser if real-time mode is working properly. Suspend the code.

  • So far, we have seen data flowing from the MCU to the debugger in real-time. Now, we will flow data from the debugger to the MCU.

  • Open and inspect the project’s .c file “lab_main.c”. Notice that the global variable DEBUG_TOGGLE is used to control the toggling of the GPIO3 pin. This is the pin being read with the ADC.

  • Highlight DEBUG_TOGGLE with the mouse, right click and select “Add Watch Expression…” and then select OK. The global variable DEBUG_TOGGLE should now be in the Expressions window with a value of “1”.

  • Enable the Expressions window for continuous refresh.

  • Run the code in real-time mode and change the value to “0”. Are the results shown in the memory and graph window as expected? Change the value back to “1”. As you can see, we are modifying data memory contents while the processor is running in real-time (i.e. we are not halting the MCU nor interfering with its operation in any way)! When done, halt the CPU.

This concludes Part 1: ADC. Terminate the active debug session using the Terminate button. This will close the debugger and return Code Composer Studio to the CCS Edit perspective view.

Optional DAC Addition#

This section is an optional continuation of the ADC lab. The purpose of this part of the lab is to generate a sine wave utilizing the DAC and feed that into the ADC as an input.

Note:

This optional DAC section is only intended for devices which have a buffered DAC. We will be using the same code as before but will add a few lines to support the DAC and enable us to generate a sine wave.

Configure the DAC#

We will start by setting up the configuration for the DAC module. This part will be done through SysConfig. Open the .syscfg file within the project and add a DAC instance by selecting the (+) next to ‘DAC’ on the left side of the SysConfig window.

The key elements of initializing the DAC are to set a reference voltage, determine a load mode (when the DAC converts the value in the shadow register), and enable output.

We will set up our DAC instance (in this device’s example, DACB), use the ADC VREFHI reference voltage, set up the load mode to be “Load on next SYSCLK”, and lastly the shadow value (in this case 800).

For devices with a DAC of Type 2 and above we will also need to set the gain. For more info on DAC types and device peripherals, refer to the Peripherals Reference Guide.

DAC of Type 1:

../../../_images/SysConfig_DACSetup.png


DAC of Type 2:

In order to setup the DAC on a device with DAC Type 2 we need to set the correct ADC reference voltage. This is done through the ‘ASYSCTL’ options within SysConfig. Setup the ADC to have an internal reference voltage of 1.65V (3.3V Conversion Range).

../../../_images/SysConfig_Adc_sysctl.png


Then we setup the DAC with a gain mode of 2.

../../../_images/SysConfig_DACSetupType2.png

Additions to the Program#

Keeping the same .c code as before, go to the global variables section and add the below table as well as a few global variables. The global variables will enable us to change the DAC output in real time and the lookup table will allow us to generate a sine wave.

uint16_t DacOutput;                       
uint16_t DacOffset;                       
uint16_t SINE_ENABLE = 0;                
// quadrature look-up table: contains 4 quadrants of sinusoidal data points
#define SINE_PTS 25
int QuadratureTable[SINE_PTS] = {
        0x0000,         // [0]  0.0
        0x1FD4,         // [1]  14.4
        0x3DA9,         // [2]  28.8
        0x579E,         // [3]  43.2
        0x6C12,         // [4]  57.6
        0x79BB,         // [5]  72.0
        0x7FBE,         // [6]  86.4
        0x7DBA,         // [7]  100.8
        0x73D0,         // [8]  115.2
        0x629F,         // [9]  129.6
        0x4B3B,         // [10] 144.0
        0x2F1E,         // [11] 158.4
        0x100A,         // [12] 172.8
        0xEFF6,         // [13] 187.2
        0xD0E2,         // [14] 201.6
        0xB4C5,         // [15] 216.0
        0x9D61,         // [16] 230.4
        0x8C30,         // [17] 244.8
        0x8246,         // [18] 259.2
        0x8042,         // [19] 273.6
        0x8645,         // [20] 288.0
        0x93EE,         // [21] 302.4
        0xA862,         // [22] 316.8
        0xC257,         // [23] 331.2
        0xE02C          // [24] 345.6
        };

Now navigate to the ADC ISR function and add a static variable that will be used to index the lookup table we recently initialized. We will also add some code to write to the DAC when we are in the ISR. Notice how the most important piece of code here is DAC_setShadowValue() which places the next value to be converted by the DAC into a shadow register.

Add the below code before acknowledging and clearing the interrupt status.

Note:

The specific DAC available depends on the device used. The code below references DACB specifically, but be sure to change the line of code that references ‘DACB’ below to match the name of your device’s available DAC (DACA or DACC).

// Write to DAC-B to create input to ADC-A0
static uint16_t iQuadratureTable = 0;        // Quadrature table index
if(SINE_ENABLE == 1)
{
    DacOutput = DacOffset + ((QuadratureTable[iQuadratureTable++] ^ 0x8000) >> 5);
}
else
{
    DacOutput = DacOffset;
}
if(iQuadratureTable > (SINE_PTS - 1))        // Wrap the index
{
    iQuadratureTable = 0;
}
DAC_setShadowValue(myDACB_BASE, DacOutput);

Build and Run the Project#

  1. Build the code and fix any errors.

  2. Open a debug perspective and add SINE_ENABLE and DacOffset to the expression windows.

  3. Adjust the jumper wire to connect the ADCINA0 pin to the DAC pin.

LaunchPad#

Device

ADCINA0 Pin

DAC Pin

F28379D

30

70 (DACB)

F2838x

n/a

n/a

F28004x

70

30 (DACB)

F28002x

69

n/a

F28003x

70

n/a

F280013x

n/a

n/a

F280015x

n/a

n/a

F28P65x

30

70 (DACC)

F28P55x

70

n/a

ControlCARD#

Device

ADCINA0 Pin

DAC Pin

F28379D

9

11 (DACB)

F2838x

9

11 (DACB)

F28004x

9

11 (DACB)

F28002x

9

n/a

F28003x

9

11 (DACB)

F280013x

9

n/a

F280015x

9

n/a

F28P65x

9

14 (DACC)

F28P55x

9

n/a

  1. Run the code

  2. At this point, the graph should be displaying a DC signal near zero (if you closed the graph, reopen it). Click on the DacOffset variable in the Expressions window and change the value to 800. This changes the DC output of the DAC which is applied to the ADC input. The level of the graph display should be about 800 and this should be reflected in the value shown in the memory buffer (note: 800 decimal = 0x320 hex).

  3. Enable the sine generator by changing the variable SINE_ENABLE in the Expressions window to 1.

  4. You should now see a sine wave in the graph window.

../../../_images/sine_output.png


You have now completed the lab. Terminate the active debug session using theTerminatebutton. This will close the debugger and return Code Composer Studio to the CCS Edit perspective view. Also close the project by right clicking on the project in theProject Explorer.

Full Solution#

The full solution to this lab exercise is included as part of the C2000Ware SDK. Import the project from [C2000Ware_Install_Path]/training/device/[device_name]/analog_subsystems/lab_adc.

Note that the solution includes code for both the ADC and DAC, but it will still compile on devices that do not have a buffered DAC.


Feedback

Please provide any feedback you may have about the content within this Academy to: c2000_academy_feedback@list.ti.com