Real Time Localization System (RTLS) based on Bluetooth® Low Energy#
Error
Note For the past few years, we have been improving our Real Time Localization System (RTLS) toolbox. Today, our SimpleLink CC26x2 Bluetooth LE wireless MCUs and software stack (BLE5-Stack) solution elements enable development of Bluetooth 5.2 compliant direction-finding solutions based on Received Signal Strength Indication (RSSI) and Angle of Arrival (AoA), with each leveraged to assist customers building advanced direction-finding applications in various segments, such as automotive and industrial.
It should be understood that an actual end product implementation incorporating AoA direction finding locator capabilities (1) requires advanced knowledge and further integration by the customer that would not ordinarily be required in a product using Bluetooth LE for communication purposes. Some challenges the customer may be required to address with AoA in their locator product include, but are not limited to, the following:
Embedded or system-level algorithms to achieve desired localization performance/angular accuracy while mitigating the presence of undesired signals (e.g. multi-path reception) in various operating environments
Antenna design to match the end product’s industrial design constraints and/or performance expectations
With Bluetooth-qualified AoA capabilities now included in the SDK, we are making the following modifications in our support for AoA:
The BOOSTXL-AOA antenna evaluation board will no longer be available for purchase after September 30, 2021.
For SDK 5.20 and later, in conformity with Bluetooth Low Energy specifications, RTLS examples only support “raw I/Q data” mode. I/Q data can be used for the development of algorithms that will need to be specific to your end product implementation.
For SDK 5.20 and later, support for Angle of Arrival (AoA) has been removed from the RTLS visual demo.
The content of SimpleLink CC13X2 / CC26X2 SDK version 5.10 and earlier releases will remain accessible; however, limited E2E support for AoA will be provided in these earlier SDKs.
(1) Implementation incorporating AoA direction finding target capabilities do not require such advanced knowledge and can directly leverage the rtls_responder example provided in the SDK as described in the Bluetooth Low Energy Angle of Arrival (AoA) for target devices
Introduction#
This module is a study of the Real Time Localization System (RTLS) Toolbox provided within the SimpleLink Low Power F2 SDK. It is assumed that the reader has a basic knowledge of embedded C tool chains and general C and Python programming concepts.
This lab is based on the rtls_coordinator
(RTLS Coordinator role), rtls_responder
(RTLS Responder role)
and rtls_passive
(RTLS Passive role) projects that are part of
the SimpleLink Low Power F2 SDK.
First, the lab will cover an overview on how to get started with the RTLS projects. Subsequent tasks of this lab will guide the user on how to customize these projects.
Prerequisites#
Hardware required#
This module requires the following kits:
2x or 3x SimpleLink™ CC26x2R LaunchPad™
Recommended reading#
These chapters in the TI BLE5-Stack User’s Guide
TI BLE5-Stack Quick Start
The CC13XX or CC26XX SDK Platform
Application
BLE5-Stack (especially the sections dedicated to periodic advertising and periodic scanning)
RTLS Toolbox
Network Processor Interface (NPI)
Project readme files:
rtls_coordinator
Readme located in <SimpleLink CC13XX / CC26XX SDK> → examples → rtos → Board → ble5stack → rtls_coordinator folder within the CC13XX / CC26XX SDK.All relevant information to
rtls_responder
andrtls_passive
is contained in thertls_coordinator
readmertls_agent
Readme located in <SimpleLink CC13XX / CC26XX SDK> → tools → ble5stack → rtls_agent folder within the CC13XX / CC26XX SDK. This will be covered in detail in Task 2.
Software for desktop development#
Those listed under the Dependencies section of the CC13XX-CC26XX SDK Release Notes
Task 1 Prepare your environment#
At the end of this task you will have:
SimpleLink Low Power F2 SDK installed
Working Python environment
Install the Software#
Run the SimpleLink CC13XX / CC26XX SDK installer.
Install Python 3.7 from the Python Download page.
Setup the Python environment as described in the README.md in <SimpleLink CC13XX / CC26XX SDK> → tools → ble5stack → rtls_agent folder.
If a bash environment doesn’t exist on your system, install Git bash
This gives you:
The SDK with TI-RTOS included at
<SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR>
which defaults toC:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx
.Python 3.7 environment with all dependencies required by the RTLS Node Manager
Load the software#
Load Board #1 with
rtls_passive
project: <SimpleLink CC13XX / CC26XX SDK> → examples → rtos → CC26X2R1_LAUNCHXL → ble5stack → rtls_passiveLoad Board #2 with
rtls_responder
project: <SimpleLink CC13XX / CC26XX SDK> → examples → rtos → CC26X2R1_LAUNCHXL → ble5stack → rtls_responderLoad Board #3 with
rtls_coordinator
project: <SimpleLink CC13XX / CC26XX SDK> → examples → rtos → CC26X2R1_LAUNCHXL → ble5stack → rtls_coordinator
Task 2 Discover the RTLS Toolbox#
At the end of this task you will have:
A basic knowledge of the localization techniques
Used
rtls_example.py
script that sets up an RTLS network.Used the RTLS toolbox and the RTLS UI
Localization Techniques#
A Real Time Localization System can be defined as a system capable of determining the position of a target within a defined physical area in real time. The physical area is normally defined through deployment of reference/locator nodes.
There are two fundamentally different approaches to location finding:
Trilateration, where you know the distance between a reference node and a target node. RSSI based techniques are typical examples of trilateration.
![../../../_images/trilateration.png](../../../_images/trilateration.png)
Trilateration#
Triangulation, where you know the direction from a reference node to a target
node. Angle of Arrival
is a technique that can be used to measure the angle
from the receiver to the transmitter.
![../../../_images/triangulation.png](../../../_images/triangulation.png)
Triangulation#
Note
What is a node? A node in this case is referred to as a localization capable embedded device. For the demos in the SDK, nodes are LaunchPads
RTLS Toolbox Introduction#
In the previous section, we discussed how multiple nodes can combine angle information to perform triangulation and/or distance to perform trilateration. It is important to remember in the pictures above, it is not possible for one single node to localize an object using the TI sample applications. A single node only produces one angle and/or one distance. By nature, this is an ambiguous measurement. If there are at least two nodes providing AoA data, then localization can occur. Same for RSSI, if there are at least three nodes providing RSSI values, then localization can occur by combining the samples from the individual nodes and finding the intersection.
In addition, the previous section has not discussed the nature of the “link” between the locator(s) and the target(s). In this lab, two options - both Bluetooth 5.1 compliant - are presented. These are known as “connection” and “connectionless”. The connection-RTLS requires a Bluetooth LE connection between the locator and the target and optionally some passive nodes. While connectionless-RTLS allows the locator and the target to remain in scanning/advertising state. The main advantages of connection based RTLS systems are the Bluetooth Low Energy connection ensures the identity of the target device and bidirectional communication is available. On the other side, connectionless RTLS system has a reduced complexity (as there is no need for passive devices) and a large number of targets (several dozens) can be tracked simultaneously.
An overview of the topology is shown below. In the diagram below, the black, blue, and red boxes represent CC26x2R LaunchPads while the grey box is a PC. The locators are the RTLS coordinator and (for connection RTLS only) the RTLS passive. The target is the RTLS responder.
![../../../_images/network.png](../../../_images/network.png)
RTLS Network#
For a comprehensive presentation of the RTLS toolbox and its software components, please see the TI BLE5-Stack User’s Guide
RTLS Roles and Topology#
Each node in an RTLS network utilizes the software components listed above
in a different role to perform a specific task related to localization. There are
three examples: rtls_coordinator
, rtls_responder
, and rtls_passive
. The capabilities
of these examples are explained below.
Connection mode#
Note
RTLS Coordinator
The RTLS Coordinator runs a full BLE-Stack and acts as a Bluetooth LE Central device. It will scan and connect to the RTLS Responder over Bluetooth LE. Once a connection is established the RTLS Coordinator will do the following:
Share the connection parameters (access address, peripheral sleep clock accuracy, and CRC init) with the PC.
Use the BLE link to share RTLS parameters with the Responder device.
Measure the RSSI of the Bluetooth signals it receives
(Possibly) Receives packets with CTE and performs in-phase and quadrature component (IQ) sampling
The RTLS Coordinator does not send out AoA packets, but configures the Responder to do so.
Report RSSI and IQ data to the PC.
Hint
RTLS Responder
The RTLS Responder runs a full BLE-Stack and acts as a Bluetooth LE Peripheral device. This is the device that is to be located (often called”target”). The Responder device will advertise and enter a connection with the RTLS Coordinator.
Advertises special string to be detected by
rtls_coordinator
(covered in detail in Task 3)Sends data packets with AoA tone embedded using Constant Tone Extension (CTE). More information on CTE can be found in the Bluetooth Core Specification Version 5.2
Wireless/battery operated, not connected to PC
Warning
RTLS Passive
The RTLS Passive does not actively participate in the BLE connection between the RTLS Coordinator and Responder. Instead, it uses the Micro BLE-Stack in connection monitoring mode to follow the connection. To do this, the Passive device relies on the Coordinator to distribute the connection parameters once a connection is formed. The Passive node does the following:
Measures the RSSI of the Bluetooth signals sent by the RTLS Responder and RTLS Coordinator
Receives packets with CTE and performs in-phase and quadrature component (IQ) sampling
Uses Micro BLE-Stack in Connection Monitoring mode to follow connection between Coordinator and Responder
Note: The RTLS Passive can be used but is not necessary.
Error
PC/Central Processing Node
The PC node is responsible for controlling the embedded RTLS nodes by sending commands and processing events. In the SDK, this is realized by a combination of a Python layer that implements the UNPI Central role and a server that translates UNPI commands to a socket interface that is used by the User Interface (UI) application running in the browser. In a final product, these algorithms may be implemented on an embedded device or even perhaps the RTLS Coordinator node.
The PC implements the following functionality in the RTLS GUI:
Communicate with RTLS_Util to issue commands and extract received RTLS Data from devices
Graphing and logging data
Enumerate devices
Distribute connection parameters to Passive nodes
Connection-less mode#
Note
RTLS Coordinator
The RTLS Coordinator runs a full BLE-Stack and acts as a Bluetooth LE observer device. It will scan and synchronize to the RTLS Responder periodic advertisements. Once synchronized, the RTLS Coordinator will measure RSSI and receive packets with CTE to performs in-phase and quadrature component (IQ) sampling
Hint
RTLS Responder (CTE Transmitter)
The RTLS Responder runs a full BLE-Stack and acts as a Bluetooth LE broadcaster device. This is the device that is to be located (also called “target”). The Responder device will advertise periodic advertisements with a Constant Tone Extension (CTE) appended. More information on CTE can be found in the Bluetooth Core Specification Version 5.2
Error
PC/Central Processing Node
The PC node is responsible for controlling the embedded RTLS nodes by sending commands and processing events. In the SDK, this is realized by a combination of a Python layer that implements the UNPI Central role and a server that translates UNPI commands to a socket interface that is used by the User Interface (UI) application running in the browser. In a final product, these algorithms may be implemented on an embedded device or even perhaps the RTLS Coordinator node.
The PC implements the following functionality in the RTLS GUI:
Communicate via REST API’s with RTLS_Util to issue commands and extract received RTLS Data from devices
Graphing and logging data
Enumerate devices
Running the RTLS Visual Demo#
In this sub-part, we are going to use the UI (User Interface). This tool runs on a computer. You will find RTLS_UI in <SimpleLink CC13XX / CC26XX SDK> → tools → ble5stack → rtls_agent → rtls_ui folder.
Build the projects and flash the LaunchPads as described before.
Connect the Coordinator and Passive devices to the computer through USB. The Responder device must be powered but does not require to be connected to the computer.
Execute the program
rtls_ui.exe
This will open your default web-browser and connect you to a local server. If your default browser is not supported (typically if your default web browser is IE), you will have to copy-paste the address of the server in a supported web browser.
Review RTLS UI’s welcome page, then click on “Get Started!”
![../../../_images/rtls_ui_landpage.png](../../../_images/rtls_ui_landpage.png)
RTLS UI welcome page#
Select the mode to enable (Connection or Connectionless). Only one feature should be selected. Once done, click on “Continue”
![../../../_images/rtls_ui_feature_selection.png](../../../_images/rtls_ui_feature_selection.png)
RTLS UI welcome page#
The UI will then display the devices detected. The UI only detects the RTLS receivers (i.e. the Coordinator and Passive devices for connection mode, and the Coordinator device for connectionless mode). The UI will NOT display the Responder device(s) eventually connected to the computer.
Select the launchpad(s) to use. Only the Coordinator and/or Passive devices have to be selected. In the case of connectionless, only one Coordinator should be selected. Once done, click on “Continue”
![../../../_images/rtls_ui_launchpad_selection.png](../../../_images/rtls_ui_launchpad_selection.png)
Select the launchpad(s) to use#
The system is ready! Click on “Auto Play” to start the demo:
![../../../_images/rtls_ui_autoplay.png](../../../_images/rtls_ui_autoplay.png)
Click on Auto Play#
For connection mode, this will automatically:
launch a scan to detect the Responder device
connect the Responder device
enable continuous connection information monitoring (i.e. RSSI sampling)
For connectionless mode, this will automatically:
launch a scan to find the periodic advertisements sent by the RTLS Responder
synchronize with the periodic advertisements
enable RSSI and TX Power monitoring
Here is the screen obtained for connection-AoA:
![../../../_images/rtls_ui_autoplay_result.png](../../../_images/rtls_ui_autoplay_result.png)
CCI and AOA are displayed#
Here is the screen obtained for connectionless-AoA:
![../../../_images/rtls_ui_autoplay_result_CL_AoA.png](../../../_images/rtls_ui_autoplay_result_CL_AoA.png)
CCI and AOA are displayed#
The logs are stored by the RTLS UI in the folder rtls_ui\logs
. These logs
keep track of the UART messages sent by the RTLS UI and the nodes.
Note
Angle and IQ data display The out of the box RTLS Visual Demo does not enable IQ data sampling. The RTLS Non-Visual Demo presented below allows IQ data sampling and storage in a csv file.
Running the RTLS Non-Visual Demo#
In this sub-part we are going to use a Python script to directly interact with the nodes.
This gives power to the developer to define
custom behavior of the RTLS network and control the devices directly.
Specifically, this will cover setting up the required Python dependencies and
running the python scripts provided in the SDK.
For connection mode, we recommend to first use the script rtls_connected.py
.
For connectionless mode, use the script rtls_connectionless.py
.
Note
Before starting this task, the following is assumed
A command prompt supporting bash or Git bash is open and running.
Unix style slashes will be used throughout. If it is necessary to run these steps in the Windows Command Prompt (
cmd.exe
), then/
should be replaced with\
.Various command prompts will search your [System Path variable][1] to find Python. If you have a pre-existing Python version in your path this may be selected over the newly installed version. To prevent mixing the two up, we will use virtual environments.
We assume that Mac users don’t have another instance of Python 3 installed. If this is not the case, then based on the
PATH
variable an older version of Python may be selected with invoking thepython3
command. Be sure to invoke the correct version of Python.Here we re-hash some of the instructions from the rtls_agent/readme.html. Some steps may be redundant if you already followed this and have the python environment setup.
Please have a look to the README file stored in tools\ble5stack\rtls_agent\rtls_util
Install Python per steps in Getting started
Open a command prompt (Git Bash is recommended)
Create a Python virtual environment
Navigate to the SDK folder (e.g.
C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent
)Execute
py -3.7 -m venv .venv
(windows) orpython3 -m venv .venv
(mac). This will create a folder called.venv
in the current directory that includes a copy of the python interpreter and a sandbox for installing packages.Note: When using Python through Anaconda, the following extra command should be executed:
c:\Anaconda3\Scripts\activate base
Activate virtual environment using
source .venv/Scripts/activate
(bash) or.venv\Scripts\activate.bat
(Windows cmd)Observe that when a venv is activated
(.venv)
will appear before each cmd promptNotice that once the virtual environment is activated, the
python
command will use the local Python interpreter in the venv. See Virtual Environments for more info.
Install RTLS packages and required external Python dependencies
Make sure to review the content of the README file.
This step will use package.bat (for Windows) or package.sh (for Linux / Mac) to install the RTLS packages.
In Windows, run
winpty ./package.bat -c -b -u -i
(winpty must be omitted if you are using PowerShell or CMD terminal). In Linux / Mac runpackage.sh -c -b -u -i
Execute
python -m pip --proxy www.proxy.com install -r requirements.txt
Note that above
--proxy www.proxy.com
is only required if behind a proxy.www.proxy.com
is an example of a proxy. It should be replaced with the web address of your specific proxy if applicable.This will install the required external Python packages that are needed by the RTLS Python suite (these are listed in
requirements.txt
).
Open the python script (
examples/rtls_connected.py
orexamples/rtls_connectionless.py
, find and update the following lines.coordinator_comport="COM27", # "/dev/cu.usbmodemL1100KKT1", passive_comports=[], # ['COM19']
Make sure to list all the Coordinator and Passive LaunchPads used and to update properly the COM ports used. It is not required to add the Responder device to this list.
Note
Notes For connectionless-AoA, only one RTLS coordinator should be used.
Make sure all the functionalities you need are enabled
Verify both RSSI and IQ data collection is enabled.
For connection mode:
continues_connection_info=True,
angle_of_arrival=True,
For connectionless mode:
periodic_advertise_report=True,
angle_of_arrival=True,
Save the file and run.
For connection mode, run the command
python -u examples/rtls_connected.py
The script will scan for RTLS devices, connect, and then print continuous connection information (RSSI, channel) for 15 seconds.
See below for sample output snippet (note that the addresses and COM ports will be different).
The out-of-box demo only reports continuous connection information (CCI). The following sections will help you to leverage all the capabilities of the provided scripts.
Example Input Parameters
----------------------------------------------------------------------
Coordinator comport : COM27
Passive comports : []
Responder BD Address : []
Scan time : 10 Sec
Connection Interval : 100 mSec
Enable Continues Connection Interval : No
Enable Angle Of Arrival (AoA) : Yes
AoA Enable Filter : Yes
AoA Slot Duration : 2
AoA Sample Rate : 1
AoA Sample Size : 1
AoA CTE Length : 20
AoA CTE Interval : 2
Data Collection Duration : 30
Data Collection iteration : 1
Provide Post Analyze Function : Yes
Example Log Dir : C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connected_log
Example Log File Name : 10_27_2022_10_02_37_rtls_connected.log
----------------------------------------------------------------------
Devices Reset
Start scan for 10 sec
Scan Results:
{'addr': '80:6F:B0:1E:35:E1', 'addrType': 0, 'rssi': -36, 'advSID': 255, 'periodicAdvInt': 0}
Trying connect to 80:6F:B0:1E:35:E1
Connected to 80:6F:B0:1E:35:E1 with connection handle 0
========== Starting Loop 1 ==========
AOA Params Set
AOA Started
Example will now wait for result for 30 sec
[10:27:2022 10:02:53:866904] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_a gent\examples\rtls_connected_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 10:02:54:179892] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_a gent\examples\rtls_connected_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 10:02:54:421870] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_a gent\examples\rtls_connected_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
...
[10:27:2022 10:03:22:699925] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_a gent\examples\rtls_connected_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 10:03:23:322936] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_a gent\examples\rtls_connected_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 10:03:23:591923] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_a gent\examples\rtls_connected_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
Rename "rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv" into "10_27_2022_10_03_23_rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv"
Executing post analyze script on C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_conn ected_log\10_27_2022_10_03_23_rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
Analyzing file : C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connected_log\08_03_ 2021_10_03_23_rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
Return here output of your post-analyze algorithm
AOA Stopped
Coordinator disconnected from responder with conn handle 0
The python script also creates the folder rtls_connected_log
(in the examples
folder). The logs stored in this folder keep track of
the UART messages exchange by the python script with the nodes.
For connectionless-AoA, run the command
python -u examples/rtls_connectionless.py
The script will scan for the periodic advertisements of an RTLS device and synchronize with them.
After this it enables connectionless-CTE reception and prints RTLS information for 15 seconds.
See below for sample output snippet (note that the addresses and COM ports will be different).
Log obtained for connectionless-AoA
Example Input Parameters
----------------------------------------------------------------------
Coordinator comport : COM27
Responder BD Address : []
Scan time : 10 Sec
Sync Params :
Sync Skip : 0
Use Advertiser List : Yes
Start Periodic Advertise Report on Sync : No
Enable Periodic Advertise Report : No
Enable Angle Of Arrival (AoA) : Yes
AoA Enable Filter : Yes
AoA Slot Duration : 2
AoA Sample Rate : 1
AoA Sample Size : 1
Data Collection Duration : 30
Data Collection iteration : 1
Provide Post Analyze Function : Yes
Example Log Dir : C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log
Example Log File Name : 10_27_2022_09_56_52_rtls_connectionless.log
----------------------------------------------------------------------
Devices Reset
Start scan for 10 sec
Scan results:
{'addr': '80:6F:B0:1E:35:E1', 'addrType': 0, 'rssi': -34, 'advSID': 1, 'periodicAdvInt': 240}
Example will try sync with:
{'addr': '80:6F:B0:1E:35:E1', 'addrType': 0, 'rssi': -34, 'advSID': 1, 'periodicAdvInt': 240}
Using advertisers list to create sync
Responder 80:6F:B0:1E:35:E1 has been added to advertisers list
Starting attempt #1 to make sure that all required responder successfully connected
All required responders successfully connected !
========== Starting Loop 1 ==========
Connectionless AOA started for 80:6F:B0:1E:35:E1
Example will now wait for result for 30 sec
[10:27:2022 09:57:16:721232] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:17:029199] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:17:289245] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:17:524198] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:17:825218] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:18:080235] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:18:468200] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:18:773198] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:19:125200] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
...
[10:27:2022 09:57:44:552275] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:44:839260] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:45:083247] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:45:636250] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:45:890282] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
[10:27:2022 09:57:46:229251] : Added new set of IQ into C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
Rename rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv into 10_27_2022_09_57_46_rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
Executing post analyze script on C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\10_27_2022_09_57_46_rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
Analyzing file : C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\tools\ble5stack\rtls_agent\examples\rtls_connectionless_log\08_03_2021_09_57_46_rtls_raw_iq_samples_806fb01e55f7_0_loop1.csv
Return here output of your post-analyze algorithm
Connectionless AOA stoped for 80:6F:B0:1E:35:E1
Coordinator terminated sync from responder with sync handle 0
The python script also creates the folder rtls_connectionless_log
(in the examples
folder). The logs stored in this folder keep track of
the UART messages exchange by the python script with the nodes. This
folder also contains the raw IQ samples received from the rtls_coordinator
.
Task 3 Deep dive in the RTLS Python scripts#
With the environment setup, it is time for us to use Python directly to control the RTLS nodes. The goal of this task is to explain the RTLS PC software and to walk through setting up a RTLS network.
Note
You might want to revision or make a copy of the default rtls_connected.py so it is
preserved. Save it with another name like rtls_example_old.py
as a backup.
RTLS Node Manager Python Overview#
First, we will briefly discuss the important layers of the Python solution and their role.
/rtls_agent
/examples/
rtls_connected.py - Example to exercise rtls_util functionality
rtls_aoa_iq_with_rtls_util_export_into_csv.py - Example to store the IQ data (or AOA) to a file on your computer
rtls_aoa_multi_conn_example.py - Example to exercice the multi-connections capability of the RTLS devices
/rtls_util/
Main interface for examples. Class that abstracts RTLSManager and RTLSNode
functionality. Handles waiting for RTLS responses in order to provide synchronous
API's. Raises any unexpected functionality as an exception.
Please review the README file for details.
/rtls/
/rtls/
rtlsmanager.py - Class to manage multiple nodes in an RTLS network.
Subscribes to incoming data from the nodes, routes
outgoing data to each of the nodes. Distributes
connection parameters from Coordinator node to any
connected Passive nodes when an connection is
established. Handles messages from rtls_agent_cli server
if one is provided.
rtlsnode.py - Class that implements the basic functionality of a node
in an RTLS network. This class will query the embedded
device connected to it and determine its capabilities.
Essentially this assigns a role in an RTLS context to
a COM port.
ss_rtls.py Defines the commands in the RTLS UNPI subsystem.
This file will define builder classes for the various
UNPI commands that the RTLS subsystem supports.
/unpi/
serialnode.py - Thread that manages serial communication from COM ports.
to higher layers.
Queues up messages and sends them to parser.
unpiparser.py - Parser for Unified Network Processor Interface messages.
Implements UNPI frame format packing/unpacking.
It is recommended to build RTLS based Python applications on top of the
RtlsUtil
class within rtls_util.py. This class forms the RTLS API set. A call
to an RtlsUtil
method translates to a sequence of one or more RTLS UNPI commands
/ responses from ss_rtls.py. In this way, RtlsUtil
is an abstraction of both the
RTLS UNPI communication as well as the RTLSManager
which manages the various
RTLSNode
’s.
RTLS Python Program Template#
rtls_connected.py
and rtls_connectionless.py
from the previous task show how to perform basic initialization of RtlsUtil
as well
as how to set up the networking and collecting localization data.
The beginning of main()
has several configuration variables:
Here are for connection AoA:
example = RtlsConnectedExample(
coordinator_comport="COM27", # "/dev/cu.usbmodemL1100KKT1",
passive_comports=[], # ['COM19']
responder_bd_addrs=[], # ['80:6F:B0:1E:39:02', '80:6F:B0:1E:38:C3']
scan_time=10,
connection_interval=100,
angle_of_arrival=True,
angle_of_arrival_params={
'enable_filter': True,
'slot_duration': 2,
'sample_rate': 1,
'sample_size': 1,
'cte_length': 20,
'cte_interval': 2
},
data_collection_duration=30,
data_collection_iteration=1,
post_analyze_func=post_analyze_of_IQ_data
)
Here are for connectionless AoA:
example = RtlsConnectionlessExample(
coordinator_comport="COM27",
responder_bd_addrs=[], # ['80:6F:B0:1E:39:02', '80:6F:B0:1E:38:C3']
scan_time=10,
sync_params={
'sync_skip': 0
},
use_advertiser_list=True,
start_periodic_advertise_report_on_sync=False,
periodic_advertise_report=False,
angle_of_arrival=True,
angle_of_arrival_params={
'enable_filter': True,
'slot_duration': 2,
'sample_rate': 1,
'sample_size': 1,
},
data_collection_duration=30,
data_collection_iteration=1,
post_analyze_func=post_analyze_of_IQ_data
)
These allow the user to select:
the COM port used to communicate with the
rtls_coordinator
the COM port used to communicate with the
rtls_passive
(not used for connectionless AoA as this mode does not define the passive role)the addresses of the devices to connect/synchronize with. If left blank, all the devices found will be connected/synchronized.
the duration of the scanning phases (for connection/synchronization of the devices)
the connection interval (connection AoA only / not used for connectionless AoA as no connection is formed)
if IQ data collection for AoA is enabled (cf. boolean
angle_of_arrival
)the parameters used for AoA data collection
enable_filter, if set to true only the samples collected during sampling slots are reported. Otherwise, all the samples (including the ones sampled during switching slots are reported)
slot_duration, length of the sampling slots (1 or 2 us)
sample_rate, sampling rate (1, 2, 3 or 4 MHz)
sample_size, 1 or 2 bytes
cte_length, length in 16us units of the CTEs requested by the central locator (connection AOA only)
cte_interval, interval (in number of connection events) between two CTE requests (connection AOA only)
the duration of the IQ data collection before analysis
the number of data collections iterations to run
the function to trigger once the data collection is done
RtlsUtils initialization#
Parts of the initialization function are common to all modes. First, construct an instance of the RTLSUtil class to serve as the RTLS Node Manager interface. The first parameter is the file to log debug information to and the second parameter is the logging level.
rtlsUtil = RtlsUtil(logging_file, RtlsUtilLoggingLevel.INFO)
Next, create a dictionary of devices and pass this to RTLS.set_devices()
which
will create RTLSNode
’s for each device and an RTLSManager
class using these
nodes.
devices = [
{"com_port": coordinator_comport, "baud_rate": 460800, "name": "Coordinator"},
{"com_port": passive_comport, "baud_rate": 460800, "name": f"Passive {index}"},
]
Note
Note
The “name” field above does not affect the functionality. It is simply used for logging purposes and therefore it is not required to modify this if not desired.
RTLS.set_devices()
will send RTLS_CMD_IDENTIFY to each node to identify it’s capabilities
and set the relevant Coordinator / Passive(s).
Next, reset both nodes:
rtlsUtil.reset_devices()
The procedures above will appear, from a UNPI perspective, as the following:
![../../../_images/rtls_identify.png](../../../_images/rtls_identify.png)
RTLS Identify#
RTLS Network Setup Procedure#
At this point you should have a basic understanding of RTLS classes. Next we will cover the minimum commands required to setup an RTLS network. This procedure is slightly different for connection-AoA and connection-less AoA.
RTLS Network Setup Procedure for connection-AoA#
For connection-AoA a BLE connection is a prerequisite for performing localization.
The sequence diagram below shows the UNPI commands required to establish a connection between rtls_coordinator
and rtls_responder
.
![../../../_images/rtls_connect_diag.png](../../../_images/rtls_connect_diag.png)
RTLS Setup Sequence Diagram#
As covered in the BLE connections lab, before connecting, a scan must be
performed to see if the desired device is nearby. This is initiated by RtlsUtil.scan()
.
The scanning device will inspect the advertisement and optionally the scan response
data to determine if it wishes to connect to a given advertiser. Usually the
scanner is looking for a given token or string in the broadcast data of the advertiser.
The RTLS Coordinator will look for the string {'R','T','L','S','R','e','s','p','o','n','d','e','r',}
starting
at the 3rd byte of the Responder’s advertisement data. If the advertising device
matches the filter, then it will be reported to the PC/Node Manager as
RTLS_CMD_SCAN
responses which are returned from RtlsUtil.scan() as a list of
devices. If the advertising device does not match the filter, it will be discarded.
RtlsUtil.ble_connect()
can be used to form a connection to one of the devices in the
scan results. This will inform rtls_coordinator
to form a connection by issuing an
RTLS_CMD_CONNECT
along with the peer device’s address and address type.
The address information can be extracted from the RTLS_CMD_SCAN
responses
coming from the Coordinator node.
If the connection is successful, the RTLS_CMD_CONNECT
response will be
received with status of RTLS_SUCCESS
and RtlsUtil.ble_connect()
will return.
The RTLS examples do not consider a connection to be established between Coordinator
and Responder until the devices have paired and formed an L2CAP Connection Oriented
Channel (CoC). The L2CAP CoC is used to send RTLS sync related information
between Coordinator and Responder. This can include AoA parameters
or a command to enable AoA.
Immediately after the BLE connection is established
(i.e. GAP_LINK_ESTABLISHED_EVENT
received from the stack), the rtls_coordinator
will share the connection parameters with the PC/Node Manager via
RTLS_CMD_CONN_PARAMS
. This information is needed by the connection monitor
inside rtls_passive
in order to follow the connection between RTLS Coordinator
and Responder.
Note
Distributing Connection Parameters
The RTLSManager
Python class will immediately relay any connection
parameters received (RTLS_CMD_CONN_PARAMS
) to all of the Passive nodes
connected. This does not need to be done manually.
Note
RTLS Passive Connection Lost As its name suggests, the Passive device does not have an active role in the BLE connection. The Passive has only the capability to listen the link but is not able to require a retransmission if a packet is not properly received. As a result, and especially in noisy environments, the Passive can lose track of the connection. In that case, the Passive device needs to re-receive the (up to date) connection info to be able to listen the BLE link. This mechanism is not implemented in the out-of-the-box examples and you will be required to restart the demo if it happens.
RTLS Network Setup Procedure for connectionless mode#
For connectionless, the rtls_coordinator has to synchronize with the
periodic advertisements of the rtls_responder.
The sequence diagram below shows the UNPI commands required to synchronize the rtls_coordinator
and rtls_responder
.
![../../../_images/rtls_CL_AoA_sync_diag.png](../../../_images/rtls_CL_AoA_sync_diag.png)
RTLS Setup Sequence Diagram#
The way rtls_coordinator synchronizes with a periodic advertiser (rtls_responder) is detailed in the Generic Access Profile (GAP) section of the TI BLE5-Stack User’s Guide. A scan must first be performed in order to identify the devices sending periodic advertisements nearby. After this, the advertiser(s) to synchronize with is(are) selected. The periodic advertisers found can be filtered based on the type of CTE sent. Once synchronized with the periodic advertiser, the receiver can start sampling the CTE appended to the periodic advertisement packets and extract AoA information.
Setting up RTLS Network#
Now that we understand the basics behind the RTLS networks and how to set them up,
let’s review how the rtls_connected.py
and
rtls_connectionless.py
sample apps set up the RTLS networks.
Note that the scripts will do some additional processing after the network is setup. This is will be covered later in this lab.
Setting up RTLS Network in Python for connection-AoA#
The commands required to setup a network belong to the RTLS UNPI subsystem and
can be found in the ss_rtls.py
file. The sending and receiving of these commands
is abstracted through the RtlsUtil
class.
Scanning for Devices#
We will use the rtls_connected.py
as a starting point. From the sections
above, we know that after the nodes are identified, we want to tell the Coordinator
to scan. This is initiated as such:
scan_results = rtlsUtil.scan(scan_time_sec)
Alternatively, it is possible to only scan for a specific device address by passing a second “address” parameter as such:
scan_results = rtlsUtil.scan(scan_time_sec, responder_bd_addr)
After the scan completes (runs for scan_time_sec
), the results are returned in
scan_results
as a list of the following dictionaries:
{
"addr" : 6 byte address as string,
"addrType" : address type as int,
"rssi": int,
"advSID": int,
"periodicAdvInt": int (0 means this advertisement is not a periodic advertisement)
}
Note
Asynchronous vs Synchronous commands in UNPI
The following provides more information about the RTLS UNPI commands. As mentioned
above, all of this is abstracted through RtlsUtil
so can be skipped if desired.
You might have noticed that RTLS_CMD_SCAN
is used to tell the node to start
scanning, receive status, and receive scan results.
This is possible within UNPI because each message can be one of the following
types
Synchronous request
Synchronous response
Asynchronous request
In the case of RTLS_CMD_SCAN
the message that initiates the scan on the
rtls_coordinator
is a synchronous request. The message that returns the status
of the scan start call is a synchronous response, and the message that
returns scan results is an asynchronous request. See the NPI chapter
in the TI BLE5-Stack User’s Guide for more information.
Connecting to a Device#
Now, we have collected a list of scan results and are ready to connect. It is required to specify an address to connect to. The address can be hard-coded:
responder_bd_addr = "80:6F:B0:1E:38:C3"
rtlsUtil.ble_connect(responder_bd_addr, connect_interval_mSec)
If you don’t know the address, you can read it from the UART
display of the Responder device. Open a Serial terminal (like putty or Tera Term)
on the user/UART port of the rtls_responder
LaunchPad. Use 115200 baud, 8N1.
It should show the following text:
Initialized
Dev Addr: 0x806FB01E3A8B
Advertising
Alternatively, the address can be extracted from the scan results as such:
rtlsUtil.ble_connect(scan_results[0], connect_interval_mSec)
Note
Connection Interval
It is also necessary to pass a connection interval into RtlsUtil.ble_connect()
.
The ramifications of this parameter will be discussed in the various RTLS mode
documentation sections where relevant. The out-of-box example uses 100
milliseconds by default.
Remember, the rtls_coordinator
will automatically send the connection parameters
once a BLE connection is formed with the rtls_responder
. The RTLSManager
python
class will intercept this and distribute it to all rtls_passive
nodes so we
don’t have to do this in our program. Upon receiving the connection parameters,
the rtls_passive
connection monitor will begin following the connection between
Coordinator and Responder. Note that it may take some time to establish a connection as this
does include LE Secure Connections pairing as well as opening an L2CAP
Connection Oriented Channel.
Setting up RTLS Network in Python for connectionless mode#
As for connection mode, the commands required to setup a network belong to
the RTLS UNPI subsystem and can be found in the ss_rtls.py
file.
The sending and receiving of these commands is abstracted through the RtlsUtil
class.
Scanning for Devices (connectionless mode)#
Note
Synchronize with the devices in the Periodic Advertiser List When one wants to synchronize with the devices in the Periodic Advertiser List, there is no need to perform this initial scan and/or filter the advertiser list. In other words, you could directly refer to the section Create the synchronization with a periodic advertiser. However, we recommend you to go through all the steps in order to better understanding our offering.
We will use the rtls_connectionless.py
as a
starting point. From the sections above, we know that after the nodes are
identified, we want to tell the rtls_coordinator
to scan.
This is initiated as such:
scan_results = rtlsUtil.scan(scan_time_sec)
Alternatively, it is possible to only scan for a specific device address and advertising set ID (SID).
scan_results = rtlsUtil.scan(scan_time_sec, advertiser_addr, advertiser_advSID)
After the scan completes (runs for scan_time_sec
), the results are returned in
scan_results
as a list of the following dictionaries:
{
"addr" : 6 byte address as string,
"addrType" : address type as int,
"rssi": int,
"advSID": int,
"periodicAdvInt": int (0 means this advertisement is not a periodic advertisement)
}
If you look at the content of scan_results
, you will see that the rtls_responder
device is reported twice. The device is reported once as a periodic advertiser
(periodicAdvInt
value is not 0), and once as a legacy advertiser (periodicAdvInt
value is 0). This is because the out-of-the-box rtls_responder
project is
configured to send out several advertisement sets. The legacy advertisement
is used to establish the connection when using connection-AoA.
For connectionless-AoA the legacy should be filter out.
Scan results found: [{'addr': '80:6F:B0:1E:55:F7', 'addrType': 0, 'rssi': -58, 'advSID': 255, 'periodicAdvInt': 0}, {'addr': '80:6F:B0:1E:55:F7', 'addrType': 0, 'rssi': -63, 'advSID': 1, 'periodicAdvInt': 80}]
Select a periodic advertiser to synchronize with#
Now, we have collected a list of scan results. We are only interested in periodic advertisements. The other ones can be filtered out.
As said before, the field periodicAdvInt
of a periodic advertisement is
always superior to 0.
scan_results_for_cl_rtls = [scan_result for scan_result in scan_results if scan_result['periodicAdvInt'] > 0]
Note
Add the advertiser to the Periodic Advertiser List
advertiser = advertiser_list[0]
rtlsUtil.padv_add_device_to_periodic_adv_list(advertiser)
The advertiser passed to the function padv_add_device_to_periodic_adv_list
should be a periodic advertiser.
Other python procedures that may be useful:
periodicAdvLisSize = rtlsUtil.padv_read_periodic_adv_list_size()
advertiser = advertiser_list[0]
rtlsUtil.padv_remove_device_from_periodic_adv_list(advertiser)
rtlsUtil.padv_clear_periodic_adv_list()
The python procedure allows to read the content of the Periodic Advertiser List is not implemented. We recommend keeping a list within the python script of the devices added to the Periodic Advertiser List. In the out-of-the-box script, all the periodic advertisers found are added to the Periodic Advertiser List so no specific list is kept.
Create the synchronization with a periodic advertiser#
The function rtlsUtil.padv_create_sync()
is used to create the synchronization.
This functions requires five parameters that are described here:
advertiser
(calledResponder
). This parameter contains the description of the advertiser to synchronize with.
advertiser = advertiser_list[0]
# Dummy responder to send when using periodic advertise list for sync
dummy_responder = {'addr': 'FF:FF:FF:FF:FF:FF',
'addrType': 0,
'rssi': 0,
'advSID': 0,
'periodicAdvInt': 0
}
options
. There are two option to create the synchronization, one is using the Periodic Advertiser List and the other one is using the specified advertiser. In additon, one can choose if the periodic avertisements reports should be initially enabled or disabled.
# Options constants:
# Clear Bit 0 - Use the advSID, advAddrType, and advAddress parameters to determine which advertiser to listen to.
# Set Bit 0 - Use the Periodic Advertiser List to determine which advertiser to listen to.
# Clear Bit 1 - Reporting initially enabled.
# Set Bit 1 - Reporting initially disabled.
USE_GIVEN_ADDRESS_AND_REPORT_ENABLE = 0
USE_LIST_AND_REPORT_ENABLE = 1
USE_GIVEN_ADDRESS_AND_REPORT_DISABLE = 2
USE_LIST_AND_REPORT_DISABLE = 3
How to enable reports if they are not initially enabled?
The reports may not be enabled at the beginning to save some computation to the MCU. In that case the MCU keeps receiving the periodic advertisings but does not execute a callback at each reception.
If the reports are not enabled at synchronization creation, they can only be enabled after the synchronization is established:
rtlsUtil.padv_create_sync(advertiser,
USE_GIVEN_ADDRESS_AND_REPORT_DISABLE,
sync_skip,
sync_timeout,
sync_cte_type)
# Scan again for sync established event. scan again if not sync established event occurred
sync_est_status = scan_for_sync_est(scan_time_sec, rtlsUtil, advertiser, num_of_scan_retry)
# Enable periodic advertise reports
rtlsUtil.padv_periodic_receive_enable(rtlsUtil.padv_get_sync_handle_by_responder(advertiser))
skip
. This is the maximum number of periodic advertising events that can be skipped after a successful receive. This is mainly used for energy savings and can be kept to 0 for a first evaluation.
sync_skip = 0 # The maximum number of periodic advertising events that can be skipped after
# a successful receive (Range: 0x0000 to 0x01F3)
syncTimeout
. Maximum time allowed between the successfull reception of two periodic advertisements. Synchronization is considered as lost if this time expires. This is mainly used for energy savings and can be kept to 10 times the periodic advertisement interval for a first evaluation.
# Synchronization timeout for the periodic advertising train Range: 0x000A to 0x4000 Time = N*10 ms Time Range
# For this example, the timeout value set to be 10 times bigger then the periodic advertise interval.
sync_timeout = int((advertiser['periodicAdvInt'] * 1.25) * 10)
syncCteType
. This parameter allows to synchronize only with periodic advertisings containing a CTE. Here we want to synchronize with periodic advertising appended with an AoA CTEs only.
sync_cte_type = 0 # Clear All Bits(0) - Sync All
# Set Bit 0(1) - Do not sync to packets with an AoA CTE
# Set Bit 1(2) - Do not sync to packets with an AoD CTE with 1 us slots
# Set Bit 2(4) - Do not sync to packets with an AoD CTE with 2 us slots
# Set Bit 4(16) - Do not sync to packets without a CTE
Here is the way to call the function rtlsUtil.padv_create_sync()
:
rtlsUtil.padv_create_sync(advertiser,
USE_GIVEN_ADDRESS_AND_REPORT_DISABLE,
sync_skip,
sync_timeout,
sync_cte_type)
The synchronization is now created and ready to be established!
Establish the synchronization with a periodic advertiser#
This is done by launching a new scan.
In the cases where you want to synchronize with the device specified (not with the devices in the Periodic Advertiser List), the function
scan_for_sync_est
defined inrtls_connectionless.py
can be leveraged.
sync_advertiser_list = []
scan_time_sec = 10 # Scanning time duration in seconds
um_of_scan_retry = 5 # Number of scan retry in case sync established event didn't occurred
sync_est_status = scan_for_sync_est(scan_time_sec, rtlsUtil, advertiser, num_of_scan_retry)
if sync_est_status:
print(f"Sync established with: {advertiser}")
sync_advertiser_list.append(advertiser)
else:
print(f"Failed to establish sync with: {advertiser}")
In the cases where you want to synchronize with the devices in the Periodic Advertiser List, use directly
rtlsUtil.scan()
, and then verify if all the expected synchronizations have been established using the functionrtlsUtil.padv_get_sync_handle_by_responder()
. In our example, we added all the periodic advertisers we found during scanning to the Periodic Advertiser List (so we directly use theadvertiser_list
to verify if all the synchronizations have been established):
# Scan again for sync established event
rtlsUtil.scan(scan_time_sec)
time.sleep(3)
# verify if the sync handle is different from 0
synced_advertiser = None
for advertiser in advertiser_list:
if rtlsUtil.padv_get_sync_handle_by_responder(advertiser) == 0:
synced_advertiser = advertiser
print(f"Sync created with first advertiser on advertisers list: {synced_advertiser}. "
f"Periodic advertise report enabled automatically")
In summary…#
Connectionless mode requires synchronizing between the rtls_coordinator
device and
periodic advertisers. Periodic advertisers can be detected through a scanning
procedure. The scanning
procedure detects both periodic advertisers and legacy advertisers.
There are two ways to synchronize with periodic advertiser(s).
Synchronization with one advertiser. Based on the result of the scanning procedure, one periodic advertiser is selected. Synchronization is first created. Then synchronization is established.
Synchronization with all the periodic advertiser(s) in the Periodic Advertiser List of the
rtls_coordinator
device. To do so some periodic advertisers detected during the scanning procedure are selected then added to the Periodic Advertiser List. Once the Periodic Advertiser List is ready, the synchronization must be created then established.
Enabling data collection#
Enabling data collection with connection mode#
This section uses the rtls_connected.py
python script.
Enabling connection-AoA#
Now that the connection has been formed and the connection parameter information has been distributed, it is time to enable AoA.
aoa_params = {
"aoa_run_mode": "AOA_MODE_RAW",
"aoa_cc26x2": {
"aoa_slot_durations": self.angle_of_arrival_params.get('slot_duration', 2),
"aoa_sample_rate": self.angle_of_arrival_params.get('sample_rate', 1),
"aoa_sample_size": self.angle_of_arrival_params.get('sample_size', 1),
"aoa_sampling_control": int(
'0x10' if self.angle_of_arrival_params.get('enable_filter', True) else '0x11', 16),
"aoa_sampling_enable": 1,
"aoa_pattern_len": 36,
"aoa_ant_pattern": [0, 1, 2, 3, 4, 5, 0, 1, 2, 3, 4, 5, 0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 6, 7,
8, 9, 10, 11, 6, 7, 8, 9, 10, 11]
}
}
self.rtls_util.aoa_set_params(aoa_params)
print("AOA Params Set")
self.rtls_util.aoa_start(cte_length=self.angle_of_arrival_params.get('cte_length', 20),
cte_interval=self.angle_of_arrival_params.get('cte_interval', 2))
print("AOA Started\n")
Continuous Connection Information (to be used with connection-AoA)#
CCI is the default functionality of the out-of-box rtls_connected.py
. It is the
most simplistic method and only provides a received signal strength indicator (RSSI) and
frequency channel index for each BLE connection event.
CCI can be enabled on both the Coordinator and the Passive(s) by sending a RTLS_CMD_CONN_INFO
UNPI
request. This is abstracted and initiated from RtlsUtil
as such:
rtlsUtil.cci_start()
After being enabled, the respective node will send a RTLS_EVT_CONN_INFO
UNPI Asynchronous Response
after each Coordinator-Responder connection event. This response contains the RSSI and the channel of the
connection event. The Coordinator will send this after participating in the connection
event with the Responder and the Passive will send this after it observes the connection event.
RtlsUtil
will receive each response and append it to the RtlsUtil.conn_info_queue
. This queue
can then be processed as desired. The out-of-box example periodically reads and prints
from this queue in results_parsing()
in a separate thread.
This procedure is shown here:
![../../../_images/cci.png](../../../_images/cci.png)
Continuous Connection Information#
Stopping the Example#
After enabling the localization mode(s), rtls_connected.py
will
collect data for a given time (this time is given by the value of data_collection_duration
discussed set in the python script’s main()
), then
gracefully stop all ongoing over-the-air procedures and any spawned result-processing threads.
The parameter data_collection_duration
can be changed according to the data collection
time required.
self.rtls_util.cci_stop()
print("\nContinues Connection Information Stopped")
self.rtls_util.aoa_stop()
print("\nAOA Stopped")
Enabling data collection with connectionless mode#
This section uses the rtls_connectionless.py
python script.
Enabling connectionless-AoA#
Now that the device is synchronized with a periodic advertiser and that periodic advertising reports are enabled, we can enable connection-less AoA.
self.rtls_util.cl_aoa_start(aoa_params, responder)
print(f"Connectionless AOA started for {responder['addr']}\n")
Connetionless-AoA has to be started for each advertiser we are synchronized with.
Stopping the Example#
After enabling data connection, rtls_connectionless.py
will collect data for a given time, then gracefully stop.
The parameter data_collection_duration
can be changed
according to the data collection time required.
self.rtls_util.padv_periodic_receive_disable(sync_handle)
print(f"Periodic report disabled for {responder['addr']}")
self.rtls_util.cl_aoa_stop(aoa_params, responder)
print(f"\nConnectionless AOA stoped for {responder['addr']}")
This does not finish the synchronization(s) with the periodic advertisers.
If you desire to finish the synchronization with the periodic advertisers, you
need to use the funtion rtlsUtil.padv_terminate_sync()
.
for responder in self.all_sync_responders:
sync_handle = self.rtls_util.padv_get_sync_handle_by_responder(responder)
self.rtls_util.padv_terminate_sync(sync_handle)
print(f"Coordinator terminated sync from responder with sync handle {sync_handle}")
Task 4 Introduction to AoA theory#
Bluetooth Core Specification Version 5.1 introduces AoA/AoD which are
covered under Direction Finding Using Bluetooth Low Energy Device
section.
AoA is for receivers that have RF switches, multiple antennas, can switch antennas and capture I/Q samples when receiving direction finding packets.
AoD is for transmitters that have RF switches, multiple antennas and can switch antennas when transmitting direction finding packets. And receivers only have one antenna but can capture I/Q samples when receiving direction finding packets.
Direction Finding Method |
Transmitter |
Receiver |
---|---|---|
AoA |
Single antenna, transmit CTE |
Multiple antennas, RF switches, can switches antennas while capture I/Q data of the CTE |
AoD |
Multiple antennas, RF switches, transmit CTE while switching antennas |
Single antenna, can capture I/Q data of the CTE |
On top of that, the Bluetooth Core Specification version 5.1 specifies the following states can support sending direction finding packets:
Periodic advertising; also called
Connectionless CTE
Connection; also called
Connection CTE
The theory behind AoA/AoD and Connectionless/Connection CTE is the same, therefore in this SimpleLink Academy training, we will only focus on Connection CTE AoA.
We will explain the AoA theory first and the walk through our SimpleLink CC13XX / CC26XX SDK offering.
AoA measurement is typically a 3-step process:
Collect phase information by sampling the I/Q
Calculate the phase difference among the antennas
Convert the phase difference into Angle of Arrival
1. Collect phase information by sampling the I/Q#
When two (or more) antennas are placed at a given distance apart from each other, their received RF signals will have a phase difference that is proportional to the difference between their respective distances from the transmitter.
Typically, the signal from one antenna will be a delayed version of the signal from the other antenna. If they are sufficiently close (less than λ(wavelength)/2 between phase centers), you can always determine which is closest to the transmitter.
These path length differences will depend on the direction of the incoming RF waves relative to the antennas in the array. In order to measure the phase difference accurately, the radio wave packet must contain a section of constant tone with whitening (Data whitening is a process that avoids sending long sequences of 1s or 0s which can cause DC bias thus altering RF performance - Here we want a sequence of 1s, so datawhitening must be disabled.) disabled where there are no phase shifts caused by modulation.
Note
Constant Tone Extension (CTE) The constant tone extension is a section of consecutive 1’s without whitening, which is effectively a +250kHz wave on top of the carrier wave. In the Bluetooth Core Specification Version 5.1, both periodic advertising packets and connection packets can contain a constant tone extension (CTE) after the CRC. The CTE can only be sent using uncoded PHY.
![../../../_images/AoA_conversion_to_phase_shift.png](../../../_images/AoA_conversion_to_phase_shift.png)
AoA Conversion to Phase Shift#
2. Calculate the phase difference among the antennas#
Phase Difference (\(\phi\)) is measured by connecting at least two antennas to the same receiver sequentially (more antennas can be added).
![../../../_images/AoA_measure_phase.png](../../../_images/AoA_measure_phase.png)
AoA Measure the phase shift#
The picture shown below is a constellation diagram which illustrates signal vectors from 2 antennas. If all the antennas are positioned in line and with a fixed distance d, the phase difference \(\phi\) between adjacent antennas will be constant.
![../../../_images/AoA_constellation.png](../../../_images/AoA_constellation.png)
AoA Constellation diagram#
In order to get a good estimate of \(\phi\) (phase), all other intentional phase shifts in the signal should be removed. Connection CTE AoA solution achieves this by adding CTE at the end of packets.
![../../../_images/AoA_packetformat.png](../../../_images/AoA_packetformat.png)
Connection CTE Packet Format#
Note
Data Physical Packet format
The grey colored part of the packet shown above means
it’s optional. The Constant Tone Extension is only enabled when the CP
bit
in the Data Physical PDU header is set. The detail of the Constant Tone
Extension is then specified by the CTEInfo
field in the in the Data
Physical PDU.
This gives the receiver time to synchronize the demodulator first, and then store the I/Q samples from the CTE into radio RAM. The I/Q data is then extracted by the application layer.
I/Q samples are used to estimate phase difference among antennas. When the receiver gets AoA packets, the RF core will trigger an event that will lead to start of the antenna switching. The RF core will start sampling the I/Q data after the guard period of the CTE and the sampled data will be stored in the radio RAM.
By comparing the I/Q data collected from different antennas, users can get the relative phase difference among antennas.
3. Convert the phase difference into Angle of Arrival#
Last step is converting the phase shift (\(\phi\)) back to AoA (\(\theta\)).
If \(\phi\) is negative, this means that antenna 2 is ahead of antenna 1.
In this case \(\theta\) is negative too but this does not cause any
mathematical problem as sin()
and arcsin()
functions are defined
both for positive and negative numbers. To avoid any unnecessary complications,
we will consider here \(\phi\) to be positive.
The angle between the incident wave and antenna array is \(\theta\). Base on the picture below we know that the \(sin(\theta) = r/d\), and \(d\) is the distance between antenna 1 and antenna 2 which is known. Then all we need to find out is \(r\).
\(r\) is the distance to antenna 2 that the incident wave needs to travel after arriving at antenna 1. We have found that the phase difference between antenna 1 and antenna 2 is \(\phi\), so the extra distance \(r\) is equal to wavelength of the incoming signal * \(\phi/(2\pi)\).
\(r = \lambda * \phi/(2*\pi)\)
![../../../_images/AoA_converting_phase.png](../../../_images/AoA_converting_phase.png)
AoA convert the phase shift back to angle#
Therfore \(\theta\) can be represented as below:
![../../../_images/AoA_converted_angle.png](../../../_images/AoA_converted_angle.png)
AoA Angle#
Note
Note
The rtls_coordinator
and rtls_passive
can be used to sample
Bluetooth 5.1 compliant IQ data.
Angle calculation implementation depends on the characteristics of
the antenna board chosen.
Hint
That’s all folks! You earned a coffee ☕. Now make sure to review the labs showing how to develop an AoA-target and an AoA-locator.
References#
TI BLE5-Stack User’s Guide CC13XX-CC26XX SDK Release Notes SimpleLink Low Power F2 SDK Bluetooth Core Specification Version 5.2