Introduction
The rampgen can be used to generate a ramp signal of a desired frequency.
Features Supported
Rampgen module includes:
- setting of ISR freuency at which run fucntion is called.
- setting of frequency of ramp signal to be generated.
Features Not Supported
N/A
Benchmark Results
A benchmark on R5F core has been conducted to observe the following results when running the following functions:
| RAMPGEN Function | Cpu Cycles |
| RAMPGEN_reset | 15 |
| RAMPGEN_config | 16 |
| RAMPGEN_run | 30
|
- Ran with TI Clang Compiler v3.2.1.LTS, with -Os flag and functions force-inlined onto the benchmarking function placed in TCM memory. Obtained the average result from 500 consecutive loops of running rampgen functions with DPL CycleCountP, mimicking the usage of a control loop.
- Actual result may vary depending on provided datasets and memory configuration. For R5F, it is recommended for users to map control loops to TCM for the best performance.
Provided Examples
Additional References
N/A
API
RAMPGEN_API_MODULE