Please make sure the following tools are installed with at least the minimum recommended version.
| Tools | Minimum Recommended Version |
|---|---|
| Code Composer Studio (CCS) | 20.2.0 |
| TI C29-CGT (Compiler) | 2.0.0.STS |
| SysConfig | 1.24.0 |
Please refer to the Getting Started Guide in the F29x SDK available here. Please note that there are some prerequisites highlighted in the Build, Load and Run section.. Please make sure you have the correct version of Python and OpenSSL installed before proceeding.