F29x Motor Control SDK  1.00.00.00
Ramp Generator Library

Introduction

The rampgen can be used to generate a ramp signal of a desired frequency.

Features Supported

Rampgen module includes:

  • setting of ISR frequency at which run fucntion is called.
  • setting of frequency of ramp signal to be generated.

Features Not Supported

N/A

Provided Examples

Additional References

N/A

API

RAMPGEN_API_MODULE