3.4. Build Kernel#
During Linux development, the kernel source code may need to be modified and recompiled. For example, the kernel needs to be recompiled if:
Enabling features which are disabled in the kernel defconfig
Disabling features which are enabled in the kernel defconfig
Modifying kernel source code to port kernel to a custom board
Once the Processor SDK Linux package is installed, the kernel source code is
under <SDK_INSTALL_DIR>/board-support/linux-<version>/. Please refer to
Processor SDK Documentation Kernel User Guide
for how to compile the kernel for AM62x.