1.4. Device Comparison and PortingΒΆ

The below table summarizes the various AM62x variants and highlights the differences in their features:

REFERENCE NAME

Arm Cortex-A53

3D Graphics Engine

AM6254

Quad Core

Yes

AM6252

Dual Core

Yes

AM6251

Single Core

Yes

AM6234

Quad Core

No

AM6232

Dual Core

No

AM6231

Single Core

No

For more information, please refer to the following link.

If you would like to emulate one of the above variants, the below suggestions will configure the Linux on the AM62x SK EVM to use less resources than what are available on the super-set device. For example, the AM62x SK EVM has an AM6254 device and to model AM6232, we can disable the two A53 cores and turn off the GPU on the EVM.

  1. In order to modify the number of A53 CPU cores, choose one of the below methods:

  2. To disable the GPU, refer to the section: Porting GPU

  3. Miscellaneous: If you would like to modify the RAM size, choose one of the below methods: