4.2.3. Porting GPUΒΆ
The GPU is enabled in kernel device tree by default. In order to disable the GPU, add the following lines of code at the end of the k3-am625-sk.dts file:
&gpu {
status = "disabled";
};
Please keep in mind that the above change is only intended for emulating AM62x variants that do not have a GPU. With the above changes, GPU based applications will not run on the SK EVM.