|
AM62Px MCU+ SDK
10.00.00
|
|
Go to the documentation of this file.
62 #include <drivers/hw_include/cslr_mmcsd.h>
72 #define MMCSD_CARD_TYPE_SD (0U)
73 #define MMCSD_CARD_TYPE_EMMC (1U)
74 #define MMCSD_CARD_TYPE_MMC (2U)
77 #define MMCSD_CARD_TYPE_NO_DEVICE (3U)
82 #define MMCSD_BUS_WIDTH_4BIT (0x4U)
83 #define MMCSD_BUS_WIDTH_8BIT (0x8U)
84 #define MMCSD_BUS_WIDTH_1BIT (0x1U)
90 #define MMCSD_TRANSPEED_25MBPS (0x32U)
91 #define MMCSD_TRANSPEED_50MBPS (0x5AU)
92 #define MMCSD_TRANSPEED_DEFAULT (0x32U)
93 #define MMCSD_TRANSPEED_HS (0x5AU)
94 #define MMCSD_TRANSPEED_SDR12 (0x32U)
95 #define MMCSD_TRANSPEED_SDR25 (0x5AU)
96 #define MMCSD_TRANSPEED_SDR50 (0xBU)
97 #define MMCSD_TRANSPEED_SDR104 (0x2BU)
98 #define MMCSD_TRANSPEED_DDR50 (0x3BU)
99 #define MMCSD_TRANSPEED_HS200 (0x2BU)
100 #define MMCSD_TRANSPEED_HS400 (0x4BU)
104 #define MMCSD_BUS_VOLT_1_8V (0x5U)
105 #define MMCSD_BUS_VOLT_3_0V (0x6U)
106 #define MMCSD_BUS_VOLT_3_3V (0x7U)
111 #define MMCSD_CMD_TYPE_NORMAL (0U)
112 #define MMCSD_CMD_TYPE_BUS_SUSPEND (1U)
113 #define MMCSD_CMD_TYPE_FUNC_SEL (2U)
114 #define MMCSD_CMD_TYPE_IO_ABORT (3U)
119 #define MMCSD_CMD_RSP_TYPE_NORSP (0U)
120 #define MMCSD_CMD_RSP_TYPE_L136 (1U)
121 #define MMCSD_CMD_RSP_TYPE_L48 (2U)
122 #define MMCSD_CMD_RSP_TYPE_L48_BUSY (3U)
127 #define MMCSD_CMD_XFER_TYPE_WRITE (0U)
128 #define MMCSD_CMD_XFER_TYPE_READ (1U)
133 #define MMCSD_SUPPORT_MMC_DS (0x01U)
134 #define MMCSD_SUPPORT_MMC_HS_SDR (0x02U)
135 #define MMCSD_SUPPORT_MMC_HS_DDR (0x04U)
136 #define MMCSD_SUPPORT_MMC_HS200 (0x08U)
137 #define MMCSD_SUPPORT_MMC_HS400 (0x10U)
138 #define MMCSD_SUPPORT_MMC_ALL (0xFFU)
143 #define MMCSD_SUPPORT_SD_DS (0x01U)
144 #define MMCSD_SUPPORT_SD_HS (0x02U)
145 #define MMCSD_SUPPORT_SD_SDR50 (0x04U)
146 #define MMCSD_SUPPORT_SD_SDR104 (0x08U)
147 #define MMCSD_SUPPORT_SD_DDR50 (0x10U)
148 #define MMCSD_SUPPORT_SD_ALL (0xFFU)
153 #define MMCSD_PHY_TYPE_HW_PHY (0U)
154 #define MMCSD_PHY_TYPE_SW_PHY (1U)
155 #define MMCSD_PHY_TYPE_NO_PHY (2U)
160 #define MMCSD_PHY_TUNING_TYPE_AUTO (0U)
161 #define MMCSD_PHY_TUNING_TYPE_MANUAL (1U)
166 #define MMCSD_PHY_MODE_HS400 (1U)
167 #define MMCSD_PHY_MODE_HS200 (2U)
168 #define MMCSD_PHY_MODE_HSSDR50 (3U)
169 #define MMCSD_PHY_MODE_HSDDR50 (4U)
170 #define MMCSD_PHY_MODE_SDR104 (5U)
171 #define MMCSD_PHY_MODE_SDR50 (6U)
172 #define MMCSD_PHY_MODE_DDR50 (7U)
173 #define MMCSD_PHY_MODE_SDR25 (8U)
174 #define MMCSD_PHY_MODE_SDR12 (9U)
175 #define MMCSD_PHY_MODE_HS (10U)
176 #define MMCSD_PHY_MODE_DS (11U)
181 #define MMCSD_UHS_MODE_SDR12 (0U)
182 #define MMCSD_UHS_MODE_SDR25 (1U)
183 #define MMCSD_UHS_MODE_SDR50 (2U)
184 #define MMCSD_UHS_MODE_SDR104 (3U)
185 #define MMCSD_UHS_MODE_DDR50 (4U)
186 #define MMCSD_UHS_MODE_HS400 (5U)
187 #define MMCSD_UHS_MODE_UHS2 (7U)
342 uint32_t response[4];
uint8_t length
Definition: mmcsd/v0/mmcsd.h:547
uint32_t intrEnable
Definition: mmcsd/v0/mmcsd.h:368
MMCSD_Handle MMCSD_open(uint32_t index, const MMCSD_Params *openParams)
This function opens a given MMCSD peripheral.
MMCSD_EmmcDeviceData * emmcData
Definition: mmcsd/v0/mmcsd.h:415
uint32_t eventId
Definition: mmcsd/v0/mmcsd.h:374
uint32_t ocr
Definition: mmcsd/v0/mmcsd.h:267
uint8_t manuID
Definition: mmcsd/v0/mmcsd.h:282
uint32_t isHC
Definition: mmcsd/v0/mmcsd.h:430
SemaphoreP_Object dataCopyCompleteSemObj
Definition: mmcsd/v0/mmcsd.h:524
uint8_t transferSpeed
Definition: mmcsd/v0/mmcsd.h:295
uint32_t blockCount
Definition: mmcsd/v0/mmcsd.h:239
SD device properties.
Definition: mmcsd/v0/mmcsd.h:266
uint32_t dataBlockSize
Definition: mmcsd/v0/mmcsd.h:495
volatile uint32_t cmdEBError
Definition: mmcsd/v0/mmcsd.h:469
uint32_t busVoltage
Definition: mmcsd/v0/mmcsd.h:386
uint32_t isCmd23
Definition: mmcsd/v0/mmcsd.h:436
uint32_t cmd
Definition: mmcsd/v0/mmcsd.h:315
uint32_t rca
Definition: mmcsd/v0/mmcsd.h:217
uint16_t index
Definition: tisci_rm_proxy.h:3
volatile uint32_t cmdTimeout
Definition: mmcsd/v0/mmcsd.h:463
uint32_t blockSize
Definition: mmcsd/v0/mmcsd.h:327
bool impDsr
Definition: mmcsd/v0/mmcsd.h:248
SemaphoreP_Object xferMutex
Definition: mmcsd/v0/mmcsd.h:518
SemaphoreP_Object cmdCompleteSemObj
Definition: mmcsd/v0/mmcsd.h:521
uint8_t * writeBufIdx
Definition: mmcsd/v0/mmcsd.h:500
uint8_t specVersion
Definition: mmcsd/v0/mmcsd.h:289
uint32_t isTuning
Definition: mmcsd/v0/mmcsd.h:339
uint64_t blockCount
Definition: mmcsd/v0/mmcsd.h:448
uint32_t isSwitch1_8V
Definition: mmcsd/v0/mmcsd.h:442
uint32_t isManualTuning
Definition: mmcsd/v0/mmcsd.h:503
volatile uint32_t dataEBError
Definition: mmcsd/v0/mmcsd.h:478
uint8_t * tempDataBuf
Definition: mmcsd/v0/mmcsd.h:412
uint16_t dsr
Definition: mmcsd/v0/mmcsd.h:245
uint32_t busWidth
Definition: mmcsd/v0/mmcsd.h:424
uint8_t start
Definition: mmcsd/v0/mmcsd.h:545
SemaphoreP_Object xferCompleteSemObj
Definition: mmcsd/v0/mmcsd.h:527
uint64_t mediaSize
Definition: mmcsd/v0/mmcsd.h:451
uint32_t ssBaseAddr
Definition: mmcsd/v0/mmcsd.h:356
uint32_t inputClkFreq
Definition: mmcsd/v0/mmcsd.h:359
uint16_t maxReadBlockLen
Definition: mmcsd/v0/mmcsd.h:273
uint32_t uhsmode
Definition: mmcsd/v0/mmcsd.h:512
uint32_t isOpen
Definition: mmcsd/v0/mmcsd.h:506
MMCSD_Object * object
Definition: mmcsd/v0/mmcsd.h:539
uint32_t cardType
Definition: mmcsd/v0/mmcsd.h:409
void MMCSD_init(void)
This function initializes the MMCSD module.
uint32_t dir
Definition: mmcsd/v0/mmcsd.h:318
uint32_t busWidth
Definition: mmcsd/v0/mmcsd.h:380
This file contains the Register Desciptions for CSL types.
MMCSD_SdDeviceData * sdData
Definition: mmcsd/v0/mmcsd.h:418
MMCSD transaction.
Definition: mmcsd/v0/mmcsd.h:314
uint8_t eStrobeSupport
Definition: mmcsd/v0/mmcsd.h:254
const MMCSD_Attrs * attrs
Definition: mmcsd/v0/mmcsd.h:537
int32_t MMCSD_enableBootPartition(MMCSD_Handle handle, uint32_t partitionNum)
This function enables the boot partition if the connected media is eMMC.
uint8_t manuID
Definition: mmcsd/v0/mmcsd.h:229
uint32_t cardType
Definition: mmcsd/v0/mmcsd.h:377
uint32_t isCmd23
Definition: mmcsd/v0/mmcsd.h:298
uint8_t specVersion
Definition: mmcsd/v0/mmcsd.h:236
uint32_t MMCSD_getInputClk(MMCSD_Handle handle)
This function returns the input clk frequency MMCSD was programmed at.
uint32_t ocr
Definition: mmcsd/v0/mmcsd.h:214
volatile uint32_t cmdCRCError
Definition: mmcsd/v0/mmcsd.h:466
int32_t MMCSD_read(MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block reads from the MMC/SD media.
uint32_t gMmcsdConfigNum
Externally defined driver configuration array size.
uint32_t MMCSD_isHC(MMCSD_Handle handle)
This function returns if the media connected is High Capacity (> 2GB in size) or not.
uint32_t intrNum
Definition: mmcsd/v0/mmcsd.h:371
uint32_t isUHS
Definition: mmcsd/v0/mmcsd.h:433
uint32_t supportedModes
Definition: mmcsd/v0/mmcsd.h:383
HwiP_Object hwiObj
Definition: mmcsd/v0/mmcsd.h:530
volatile uint32_t cmdError
Definition: mmcsd/v0/mmcsd.h:481
uint32_t enableDma
Definition: mmcsd/v0/mmcsd.h:454
uint32_t MMCSD_getBlockCount(MMCSD_Handle handle)
This function returns the block count of User Data Area of the MMC/SD media connected to the MMCSD co...
uint32_t rca
Definition: mmcsd/v0/mmcsd.h:270
uint32_t is1_8V
Definition: mmcsd/v0/mmcsd.h:439
uint32_t phyType
Definition: mmcsd/v0/mmcsd.h:392
uint32_t ctrlBaseAddr
Definition: mmcsd/v0/mmcsd.h:353
uint8_t supportedModes
Definition: mmcsd/v0/mmcsd.h:251
uint8_t * dataBuf
Definition: mmcsd/v0/mmcsd.h:204
uint8_t * readBufIdx
Definition: mmcsd/v0/mmcsd.h:497
void * MMCSD_Handle
Definition: mmcsd/v0/mmcsd.h:189
volatile uint32_t xferInProgress
Definition: mmcsd/v0/mmcsd.h:484
MMCSD instance attributes - used during init time.
Definition: mmcsd/v0/mmcsd.h:200
uint32_t MMCSD_getBlockSize(MMCSD_Handle handle)
This function returns the block size of the MMC/SD media connected to the MMCSD controller.
uint32_t dataBlockCount
Definition: mmcsd/v0/mmcsd.h:494
eMMC device properties
Definition: mmcsd/v0/mmcsd.h:213
void MMCSD_deinit(void)
This function de-initializes the MMCSD module.
uint16_t maxReadBlockLen
Definition: mmcsd/v0/mmcsd.h:220
Definition: mmcsd/v0/mmcsd.h:544
MMCSD driver object.
Definition: mmcsd/v0/mmcsd.h:405
volatile uint32_t xferComp
Definition: mmcsd/v0/mmcsd.h:487
uint8_t transferSpeed
Definition: mmcsd/v0/mmcsd.h:242
uint32_t supportedDataWidths
Definition: mmcsd/v0/mmcsd.h:301
void MMCSD_Params_init(MMCSD_Params *mmcsdParams)
Initialize data structure with defaults.
void * dataBuf
Definition: mmcsd/v0/mmcsd.h:324
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:93
MMCSD_Handle handle
Definition: mmcsd/v0/mmcsd.h:406
uint32_t enableDma
Definition: mmcsd/v0/mmcsd.h:336
void * deviceData
Definition: mmcsd/v0/mmcsd.h:201
volatile uint32_t dataCRCError
Definition: mmcsd/v0/mmcsd.h:475
uint16_t maxWriteBlockLen
Definition: mmcsd/v0/mmcsd.h:223
uint32_t outputClkFreq
Definition: mmcsd/v0/mmcsd.h:362
volatile uint32_t cmdIndexError
Definition: mmcsd/v0/mmcsd.h:472
uint32_t arg
Definition: mmcsd/v0/mmcsd.h:321
uint8_t sdVer
Definition: mmcsd/v0/mmcsd.h:421
uint32_t transferSpeed
Definition: mmcsd/v0/mmcsd.h:427
Definition: mmcsd/v0/mmcsd.h:536
uint32_t blockCount
Definition: mmcsd/v0/mmcsd.h:330
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
uint32_t isHS
Definition: mmcsd/v0/mmcsd.h:389
MMCSD_Config gMmcsdConfig[]
Externally defined driver configuration array.
uint32_t enableDma
Definition: mmcsd/v0/mmcsd.h:365
MMCSD instance attributes - used during init time.
Definition: mmcsd/v0/mmcsd.h:352
uint32_t blockCount
Definition: mmcsd/v0/mmcsd.h:292
void MMCSD_close(MMCSD_Handle handle)
Function to close a MMCSD peripheral specified by the MMCSD handle.
uint32_t autoCmdEn
Definition: mmcsd/v0/mmcsd.h:333
SemaphoreP_Object cmdMutex
Definition: mmcsd/v0/mmcsd.h:515
volatile uint32_t xferTimeout
Definition: mmcsd/v0/mmcsd.h:490
int32_t MMCSD_disableBootPartition(MMCSD_Handle handle)
This function disables the boot partition if the connected media is eMMC.
uint32_t intrEnable
Definition: mmcsd/v0/mmcsd.h:457
uint32_t readBlockCount
Definition: mmcsd/v0/mmcsd.h:498
int32_t MMCSD_write(MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block writes to the MMC/SD media.
uint32_t xferHighSpeedEn
Definition: mmcsd/v0/mmcsd.h:509
volatile uint32_t cmdComp
Definition: mmcsd/v0/mmcsd.h:460
MMCSD_Handle MMCSD_getHandle(uint32_t index)
This function returns the handle of an open MMCSD Instance from the instance index.
uint8_t driveStrength
Definition: mmcsd/v0/mmcsd.h:257
uint8_t end
Definition: mmcsd/v0/mmcsd.h:546
uint8_t * dataBufIdx
Definition: mmcsd/v0/mmcsd.h:493
uint32_t writeBlockCount
Definition: mmcsd/v0/mmcsd.h:501
uint32_t tuningType
Definition: mmcsd/v0/mmcsd.h:395
uint32_t blockSize
Definition: mmcsd/v0/mmcsd.h:445
uint16_t maxWriteBlockLen
Definition: mmcsd/v0/mmcsd.h:276