MSPM0 Sensorless FOC Software User’s Guide¶
CCS Project setup¶
Go to Import CCS Projects as shown below.
Click Browse. Navigate to
C:\ti\mspm0_sdk_<SDK_Version>\examples\nortos\[LAUNCHPAD]\motor_control_bldc_sensorless_foc.Click Select Folder. Check the desired hardware board, and click Finish to import the project into your workspace.
2.1 Setting the Motor Parameters¶
The motor parameter can be found in the motor_params.h file. These are the motor parameters required for Sensorless FOC:
Stator resistance, Rs (ohm)
Stator inductance, Ls (H)
Number of motor poles (optional)
Back Emf constant in V/Hz
Base maximum Frequency of the motor (Hz)
Fig. 1 Locate motor_params.h file¶
These parameters are defined using an #elif statement for a motor. To define these parameters for a custom motor, modify the #define statements for MOTOR_PARA_RS, MOTOR_PARA_LS, MOTOR_PARA_POLES, and MOTOR_PARA_MAX_FREQ for USER_MOTOR. To add another motor, copy and paste the #elif statement below and rename USER_MOTOR to another name.
#elif (USER_MOTOR)
/* Define the electrical motor parameters (User motor) */
/* @brief Stator resistance (ohm) */
#define MOTOR_PARA_RS 8
/* @brief Stator inductance (H) */
#define MOTOR_PARA_LS 0.0032
/* @brief Number of poles */
#define MOTOR_PARA_POLES 6
/* @brief Back Emf constant in V/Hz */
#define MOTOR_PARA_KE 0.1
/* @brief Maximum Frequency */
#define MOTOR_PARA_MAX_FREQ 125
To select a motor defined in motor_params.h, click Project -> Properties in the toolbar. In the Properties window, go to Build -> Arm Compiler -> Predefined Symbols. The pre-defined motor name is LVSERVOMTR=1. To change the pre-defined motor name, click “Edit” and change LVSERVOMTR to another defined motor in motor_params.h, such as LVBLDCMTR or USER_MOTOR.
Fig. 2 LVSERVOMTR=1 symbol¶
Adding Initial Parameters (optional)¶
In the Project Explorer, open the project drop down menu and open “param_[motor driver].h”.
Fig. 3 Locate param_[motor driver].h file¶
In the “param_[motor driver].h” file change any of the “GUI_DEFAULT_xxxx” defines to some pre-defined parameters in the following folders, or the value inside of the parentheses.
“foc_types.h” (sensorless_foc -> foc)
“motor_params.h” (motor)
“drvxxxx.h” (motor_driver -> drv83xx) The parameters that can be initially defined are below.
Parameter |
Definition |
|---|---|
USER_DEFAULT_FOC_VOLT_RATIO |
Voltage divider ratio for th DC bus voltage input |
USER_DEFAULT_DRV_RSHUNT |
DRV shunt resistor in Ω |
DRV_CSA_GAIN_MAP_0 |
DRV gain mapped to FOC_CSA_GAIN_0 |
DRV_CSA_GAIN_MAP_1 |
DRV gain mapped to FOC_CSA_GAIN_1 |
DRV_CSA_GAIN_MAP_2 |
DRV gain mapped to FOC_CSA_GAIN_2 |
DRV_CSA_GAIN_MAP_3 |
DRV gain mapped to FOC_CSA_GAIN_3 |
USER_DEFAULT_CSA_GAIN |
Selected CSA gain settings |
USER_DEFAULT_ENABLE_GAIN_CHANGE |
FLAG used to enable DRV GAIN CHANGE while program runs |
DRV_setCsaGain |
Links to the DRV set gain function, need to be set if USER_DEFAULT_ENABLE_GAIN_CHANGE is defined |
DRV_HANDLE |
Links to the DRV instance, need to be set if USER_DEFAULT_ENABLE_GAIN_CHANGE is defined |
DRV_CSA_GAIN |
Links to the DRV CSA gain enumeration, need to be set if USER_DEFAULT_ENABLE_GAIN_CHANGE is defined |
USER_DEFAULT_ENABLE_FAULT_INPUT_CHECK |
FLAG used to enable checking External fault input |
FAULT_INPUT_STATUS |
Links to the API to poll for fault status, should return 1 to report external fault condition |
FAULT_INPUT_CLEAR |
Links to the API to clear external fault condition |
USER_DEFAULT_FOC_RS |
Motor stator resistance in Ω |
USER_DEFAULT_FOC_LS |
Motor stator inductance in H |
USER_DEFAULT_FOC_KE |
Motor back emf phase to phase in V/Hz |
USER_DEFAULT_FOC_MAX_FREQ |
Motor maximum frequency to command, speed reference upper limit is limited to this value |
USER_DEFAULT_FOC_PWMFREQ |
PWM frequency selection, can enter value in enum of FOC_PWM_FREQ |
USER_DEFAULT_FOC_DEADBAND |
Deadband to set in nanoseconds |
USER_DEFAULT_FOC_STARTUP_METHOD |
Startup method selection, can enter value in enum of FOC_STARTUP |
USER_DEFAULT_FOC_SLOW_FIRST_CYC_FREQ |
Slow first cycle frequency in Hz |
USER_DEFAULT_FOC_RAMPUP_CURRENT |
Current settings in rampup phase in Ampere |
USER_DEFAULT_FOC_RAMPUP_TARGET |
Target frequenct in ramp phase in Hz |
USER_DEFAULT_FOC_ALIGN_TIME |
Time spend in align in seconds |
USER_DEFAULT_FOC_ALIGN_CURRENT |
Align or first cycle current |
USER_DEFAULT_IPD_THRESHOLD_COUNT |
Value between 1-100, higher the value higher the peak current in IPD, can enter value in enum of FOC_IPD_THRES_COUNT |
USER_DEFAULT_FOC_IPD_FREQ |
IPD frequency enum, can enter value in enum of FOC_IPD_FREQ |
USER_DEFAULT_FOC_SPEED_REF_RAMP_RATE |
Ramp rate for PI speed reference in Hz/s |
USER_DEFAULT_FOC_PISPD_KP |
Proportional constant for PI speed |
USER_DEFAULT_FOC_PISPD_KI |
Integral constant for PI speed |
USER_DEFAULT_FOC_PISPD_DIV |
PI speed loop execution divider, can enter value in enum of FOC_SPD_DIV |
USER_DEFAULT_FOC_PIIQ_KP |
Proportional constant for PI IQ |
USER_DEFAULT_FOC_PIIQ_KI |
Integral constant for PI IQ |
USER_DEFAULT_FOC_PIID_KP |
Proportional constant for PI ID |
USER_DEFAULT_FOC_PIID_KI |
Integral constant for PI ID |
USER_DEFAULT_FOC_OUTER_LOOP |
Selection for outerloop speed or current, can enter value in enum of FOC_OUTER_LOOP |
USER_DEFAULT_FOC_DIRECTION_REVERSAL |
Set the motor direction, can enter value in enum of FOC_DIRECTION |
USER_DEFAULT_FOC_PWMADCSAMPLE |
Number of PWM cycles to be spend in adc sampling, ie, if 40 and PWM clock is 80Mhz then 1us is available for current sampling |
USER_DEFAULT_FOC_ADC_SETTLE_DELAY |
ADC value rise time delay in PWM cycles, defines the delay to wait before ADC input voltage is stabilized before sampling |
USER_DEFAULT_FOC_OVER_VOLT |
DC Bus voltage Over voltage threshold |
USER_DEFAULT_FOC_UNDER_VOLT |
DC Bus voltage Under voltage threshold |
USER_DEFAULT_FOC_OVER_CURRENT |
Phase Over current threshold |
Starting the Project¶
Connect the hardware and turn on the power supply. There should be no more than 50mA on the power supply.
Click on the Build button.
Project should build with no errors.Click on the Debug button.

Open the Expressions window and add the following global structures and expressions. The expressions below in the userVar structure controls the motor system and has control parameters defined in it.
The userVar structure has 3 structures:
controlRegs which holds the variables to control the motor
statusRegs which holds the status variables
userParams which holds the parameters for the foc
controlRegs components
Description
cntri1.clearFault
If set 1 clears all the faults
cntri1.flashAccessKey
Stores the flash access key. Need to be set value in define FOC_FLASH_ACCESSKEY to do flashWrite, flashRead, or dafultRead
cntri1.flashWrite
If set 1 and flashAccessKey matches then values in userParams are saved to flash
cntri1.flashRead
If set 1 and flashAccessKey matches then values in flash are loaded into userParams
cntri1.defaultRead
If set 1 and flashAccessKey matches then default values or initial parameters in flash are loaded into userParams
cntri1.disCL
If set 1 disables the closed loop transition after rampup phase is completed
cntri1.enableMotor
If set 1 starts to run motor, if set 0 stops the motor
speedRef
If outer loop is speed this is set as reference to PI speed. Value is set in IQ20 and positive values are only used. User should not enter negative values.
iqRef
If outer loop is current this is set as reference to PI IQ controller.Value is set in IQ20
idRef
If outer loop is current this is set as reference to PI ID controller.Value is set in IQ20
statusRegs components
Description
faultStatus.bits.extFaultIn
Shows the External fault input status, Set to 1 when falling edge on fault input pin
faultStatus.bits.uvlo
Shows the undervoltage fault status, Set to 1 when dc bus voltage is lower than underVoltageLimit parameter
faultStatus.bits.ovlo
Shows the undervoltage fault status, Set to 1 when dc bus voltage is higher than overVoltageLimit parameter
faultStatus.bits.ocp
Shows the overcurrent fault status, Set to 1 when motor phase current is greater than overCurrentLimit parameter
motorState
Shows the state of the foc control. Refer enum MOTOR.
vdc
DC bus current in IQ20
speedFbk
Estimated motor speed in IQ(20)
speedRef
Reference input for PI speed in IQ(20)
iqCurr
Feedback input to PI IQ in IQ(20)
iqCurrRef
Reference input for PI ID in IQ(20)
idCurr
Feedback input to PI ID in IQ(20)
idCurrRef
Reference input for PI ID in IQ(20)
userParams are initialized with the parameters saved in the flash in init time.
userParams components
Description
rs
Stator resistance in IQ(20)
ls
Stator inductance in IQ(20)
ke
Motor back emf constant in IQ(20)
maxFreq
Maximum motor frequency
PWMFreq
Selection of PWM frequency. Refer enum FOC_PWM_FREQ
deadband
Deadband in nanoseconds
CSAGain
Selection of CSA GAIN. Refer enum FOC_CSA_GAIN
outerLoop
Selection of Outer loop. Refer enum FOC_OUTER_LOOP
directionReversal
Selection of direction. Refer enum FOC_DIRECTION
startupMethod
Startup method selection. Refer enum FOC_STARTUP
slowCycFreq
Slow first cycle frequency in Hz. Value in IQ(20)
alignCur
Align current in Ampere in IQ(20)
alignTime
Align time in seconds in IQ(20)
IPDCurrThresh
Value between 1-100, higher the value higher the peak current. Refer enum FOC_IPD_THRES_COUNT
IPDFreq
IPD frequency selection. Refer enum FOC_IPD_FREQ
rampupCur
Rampup current in Ampere in IQ(20)
rampupRate
Ramp up rate in Hz/s in IQ(20)
rampupTarget
Ramp up target in Hz in IQ(20)
speedRefRampRate
Speed reference ramp rate in Hz/s in IQ(20)
piSpdKp
PI speed proportionality constant in IQ(20)
piSpdKi
PI speed Ki in IQ(20)
piSpdDiv
PI speed execution rate divider
piIdKp
PI ID proportionality constant in IQ(20)
piIdKi
PI ID integral constant in IQ(20)
piIqKp
PI IQ proportionality constant in IQ(20)
piIqKi
PI IQ integral constant in IQ(20)
overVoltageLimit
Overvoltage limit in IQ(20)
underVoltageLimit
Undervoltage limit in IQ(20)
overCurrentLimit
Overcurrent limit in IQ(20)
Note: Some of the variables are in IQ20 format. In order to be displayed and updated properly during debug, you should switch them to IQ(20) format in the CCS expressions window by right clicking the expression, select Q-Values, then click “Select Q-Value”.
Fig. 4 Select IQ value¶
For devices with SPI support only, you can add the guiSPI structure for SPI Configuration and controlling SPI reads/writes during runtime. The expressions below in the gui_spi structure configure the SPI configuration and use expressions during run time.
gui_spi
structure that contains the SPI variables below
writeBitfieldRegFlag
Writes writeBitfieldRegData to bitfieldRegPosData of writeBitfieldRegAddr when set to 1
writeBitfieldRegAddr
Set to address of a bitfield register write operation
bitfieldRegPosData
Bitfield position of a bitfield write operation to writeBitfieldRegAddr
bitfieldRegMaskData
Mask value of a bitfield write operation to writeBitfieldRegAddr
writeBitfieldRegData
Data value of a bitfield write register operation to writeBitfieldRegAddr
writeRegFlag
Writes writeRegData to writeRegData of writeRegAddr when set to 1
writeRegAddr
Set to address of a register write operation
writeRegData
Data value of a write register operation to writeRegAddr
readRegFlag
Reads data of readRegAddr and stores into to readRegData when set to 1
readRegAddr
Set to address of a register read operation
readRegData
Data value read from read operation of readRegAddr
Press Play
to start the code.Enable “Continuous Refresh” in the Expressions window.

Running the Project¶
Open userVar. Set outerloop to FOC_OUTER_LOOP_SPEED to select outer speed loop. Set speedRef to 100 to spin the motor at 100Hz and set enableMotor to 1 to start the motor. The motor starts spinning.
set enableMotor to 0 to stop the motor. Set directionReversal to FOC_DIRECTION_CCW to reverse the motor direction. Set enableMotor to 1 and observe motor spinning in opposite direction.
Stop the motor by setting enableMotor to 0. Change PWMFreq to FOC_PWM_FREQ_15000 to select 15Khz PWM frequency. Enable the motor again and observe the PWM outputs.
Change deadband to 500 to change the MCU deadband to 500 ns. Observe in waveforms.
Change speedRefRampRate to change the acceleration and deceleration rate of the motor when speedRef is modified.
Set overVoltageLimit to a low value and increase the DC bus voltage beyond it and observe faultStatus.bits.ovlo is set to 1, and the motor stops spinning. Reduce the voltage below the limit and set cntrl1.clearFault = 1 to clear the latched fault and enable the motor again to spin it.
Create an undervoltage fault by decreasing the voltage below underVoltageLimit. Observe faultStatus.bits.uvlo is set and the motor stops spinning. Increase the voltage above the limit and set cntrl1.clearFault = 1 to clear the latched fault and enable the motor again to spin it.
If the device has SPI registers, use the gui_spi variables to perform a bitfield write, register write, or register read, or read all operation.
To perform a bitfield write operation:
Select the drop-down register in writeBitfieldRegAddr
Enter the bitfield position in bitfieldRegPosData
Enter the mask of the setting in that bitfield position in bitfieldRegMaskData (for example, a 3-bit setting has mask 0x7)
Write the bitfield data in writeBitfieldRegData
Set the writeBitfieldRegFlag to 1. It will automatically clear to 0.
To perform a register write operation:
Select the drop-down register in writeRegAddr
Write the data in writeRegData
Set the writeRegFlag to 1. It will automatically clear to 0.
To perform a register read operation:
Select the drop-down register in readRegAddr
Set the readRegFlag to 1. It will automatically clear to 0.
Read the data in readRegData
Fig. 5 gui_spi variables¶
2.7 Logging the variables¶
The user can add the __ENABLE_LOG predefined symbol to enable logging. The user can set the log index and variable as shown in the below code:
FOC_addVarToLog(FOC_LOG_IDX_0, phaseVolt.Valpha);
To see the logged data as a graph, the user can add the variable cssLog[X], where X is the index. Right click the variable and select “Graph”.
Fig. 6 Image of graph¶
Select “Continuous Refresh” mode to see continuous data.
Fig. 7 Image of graph¶
Note: the software consumes 24KB extra space in SRAM to store the values when logging is enabled.
3. API Guide¶
4. Known Issues¶
Function implicit declaration warning for IQrepeat function while compiling.
Current solution supports power up to 100W. Applying high torque at low speeds can cause motor to spin backwards with high rpm.
5. Supported Devices¶
DRV8323RS¶
Supported MSPM0 Launchpads
Links