Readme
Example Summary
The following example configures configures TimerG in one shot mode, toggles an LED for 5 seconds, and then turns off the LED. The peripheral interrupt is disabled and then the device is put to SLEEP. This example demonstrates the best approach to disable interrupts.
Note: Example requires Rev E3 or later of the MSPM0C1104 LaunchPad.
Peripherals & Pin Assignments
| Peripheral | Pin | Function |
|---|---|---|
| GPIOA | PA22 | Standard Output |
| GPIOA | PA2 | Standard Output |
| SYSCTL | ||
| TIMG14 | ||
| EVENT | ||
| DEBUGSS | PA20 | Debug Clock |
| DEBUGSS | PA19 | Debug Data In Out |
BoosterPacks, Board Resources & Jumper Settings
Visit LP_MSPM0C1104 for LaunchPad information, including user guide and hardware files.
| Pin | Peripheral | Function | LaunchPad Pin | LaunchPad Settings |
|---|---|---|---|---|
| PA22 | GPIOA | PA22 | J1_8 | N/A |
| PA2 | GPIOA | PA2 | J2_13 | N/A |
| PA20 | DEBUGSS | SWCLK | J2_11 |
|
| PA19 | DEBUGSS | SWDIO | J2_17 |
|
Device Migration Recommendations
This project was developed for a superset device included in the LP_MSPM0C1104 LaunchPad. Please visit the CCS User’s Guide for information about migrating to other MSPM0 devices.
Low-Power Recommendations
TI recommends to terminate unused pins by setting the corresponding functions to GPIO and configure the pins to output low or input with internal pullup/pulldown resistor.
SysConfig allows developers to easily configure unused pins by selecting Board→Configure Unused Pins.
For more information about jumper configuration to achieve low-power using the MSPM0 LaunchPad, please visit the LP-MSPM0C1104 User’s Guide.
Example Usage
Compile, load and run the example. LED1 will toggle on and off for 5 seconds. After 5 seconds, the LED will turn off and the device will go to SLEEP.
Application Design Details
When disabling interrupts, the best approach is to disable the peripheral interrupts instead of just disabling the NVIC. If just the NVIC is disabled and the peripheral interrupt is left enabled, then the device will still wake up the power domain to check the interrupt status.