EVM Setup Operational Modes
Table of Contents
Overview
This guide is intended for users with a TI mmWave sensor evaluation module (EVM). The guide will walk through setting up the boards into either Flashing Mode or Functional Mode. In flashing mode, a program may be loaded onto the device’s external flash. In functional mode, the EVM boots automatically from flash and begins executing the image stored there.
This guide supports several different EVM’s so be sure to follow the steps that apply to your device.
mmWaveICBoost Initial Configuration
This section is only necessary if the EVM is being attached to an mmWaveICBoost carrier board and the carrier board has not been configured for flashing or functional mode previously.
Set S1 Switches
Set the S1 switch combination as shown in the image below. This puts the mmWaveICBoost in its standalone operation as opposed to in development mode for use with a DCA1000.
ISK, ISK-ODS, and L EVM’s
This section applies to the following boards:
ISK Style Standalone Mode
- This section describes setting an ISK, ISK-ODS, or LEVM to Flashing or Functional mode when used without a mmWaveICBoost carrier board.
- Only ISK Rev C or later and ISK-ODS Rev B or later can be used in standalone mode.
- CCS Debug mode does NOT work in standalone mode.
Hardware Requirements for Standalone ISK Style
- ISK, ISK-ODS, or LEVM Antenna Module Board
- Micro USB Cable
Flashing Mode for Standalone ISK Style EVM’s
1. Switch Configuration
Set the mux switches as shown in the image below. The same switch orientation is used for both ISK and ISK-ODS.
2. Hardware Configuration
Connect the micro-USB cable to the EVM at the connector shown and then to a PC. Note that a separate power supply is not needed as the modules get power from the USB connection itself. LEDs on the EVM should turn on.
3. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
Functional Mode for Standalone ISK Style EVM’s
1. Switch Configuration
Set the mux switches as shown in the image below. The same switch orientation is used for both ISK and ISK-ODS.
2. Hardware Configuration
Connect the micro-USB cable to the EVM at the connector shown and then to a PC. Note that a separate power supply is not needed as the modules get power from the USB connection itself. LEDs on the EVM should turn on.
3. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
ISK Style With mmWaveICBoost Attached
This section describes setting an ISK style EVM to either Flashing or Functional mode when attached to an mmWaveICBoost carrier board.
Hardware Requirements for ISK + Carrier
- MMWAVEICBOOST Carrier Board
- ISK, ISK-ODS, or LEVM Antenna Module Board
- Micro USB Cable
- Power Supply 5V, 3A with 2.1-mm barrel jack (center positive)
Initial Configuration for ISK Style EVM + Carrier
1. Configure mmWaveIcBoost
If the mmWaveICBoost carrier board has not been used previously, then follow the steps to perform initial configuration of the carrier board.
2. Configure Antenna Module
On newer EVM’s (ISK Rev C or later and ISK-ODS Rev B or Later) that have not been previously used in conjunction with the carrier board, set the S1 Switches according to the following image.
3. Mount EVM
- If using an older revision of the ISK or ODS module, both 60Pin connectors will be used.
- If using a newer revision of the ISK or ISK-ODS module, only the right connector closer to the micro-usb connectors will be connected.
4. Connect cables
- Connect the micro-USB to the carrier board at the connector shown and to the PC. Note that the micro-USB is connected to the lower XDS110 USB (and not the FTDI USB).
- Connect the 5V/3A power supply to the power source and then to the carrier board. LEDs on the carrier board should turn on.
Flashing Mode for ISK Style EVM + Carrier
1. Switch Configuration
Set SOP mode jumpers according to the following image to configure the carrier board for flashing mode.
2. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
Functional Mode for ISK Style EVM + Carrier
1. Switch Configuration
Set SOP mode jumpers according to the following image to configure the carrier board for functional mode.
2. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
AOP EVM’s
This section applies to the following boards:
AOP Standalone Mode
- Section applies to setting an AOP EVM to Flashing or Functional mode when used without an mmWaveICBoost carrier board.
- An AOP EVM can no longer be flashed if the board has been split at the pre-made snap point.
- CCS Debug mode does NOT work in standalone mode.
Hardware Requirements for Standalone AOP
- AOP Antenna Module Board
- Micro USB Cable
Initial Configuration for Standalone AOP
If the device was previously used in standalone mode, this step may be skipped. Otherwise, configure the S1 switches to match the following image.
Flashing Mode for Standalone AOP
1. Switch Configuration
Set the mux switches as described in the image below
2. Hardware Configuration
Connect the micro-USB cable to the EVM at the connector shown and then to a PC. Note that a separate power supply is not needed as the AOP modules get power from the USB connection itself. LEDs on the EVM should turn on.
3. Power State
Toggle the NRST button to assert a device reset
Functional Mode for Standalone AOP
1. Switch Configuration
Set the mux switches as described in the image below
2. Hardware Configuration
Connect the micro-USB cable to the EVM at the connector shown and then to a PC. Note that a separate power supply is not needed as the AOP modules get power from the USB connection itself. LEDs on the EVM should turn on.
3. Power State
Toggle the NRST button to assert a device reset
AOP With mmWaveICBoost Attached
This section applies to setting an AOP EVM to Flashing or Functional mode when attached to an mmWaveICBoost carrier board. Please note, an AOP EVM cannot be attached to an mmWaveICBoost carrier board once the board has been snapped at the pre-made break point
Hardware Requirements for AOP + Carrier
- MMWAVEICBOOST Carrier Board
- AOP Antenna Module Board
- Micro USB Cable
- Power Supply 5V, 3A with 2.1-mm barrel jack (center positive)
Initial Configuration for AOP + Carrier
1. Configure mmWaveIcBoost
If the mmWaveICBoost carrier board has not been used previously, then follow the steps to perform initial configuration of the carrier board.
2. Configure Switches on Front of EVM
Set the S1 and S2 Switches on the front of the AOP EVM according to the following image
3. Configure Switch on Back of EVM
Set the S3 Switch on the back of the AOP EVM according to the following image
4. Mount EVM
Attach the EVM to the carrier board. The 60 pin connector on the AOP EVM will connect to the connector on the carrier that is closer to the two micro-USB connectors
5. Connect cables
- Connect the micro-USB to the carrier board at the connector shown and to the PC. Note that the micro-USB is connected to the lower XDS110 USB (and not the FTDI USB).
- Connect the 5V/3A power supply to the power source and then to the carrier board. LEDs on the carrier board should turn on.
6. Flashing Mode for AOP + Carrier
Set SOP mode jumpers according to the following image to configure the carrier board for flashing mode.
6a. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
7. Functional Mode for AOP + Carrier
Set SOP mode jumpers according to the following image to configure the carrier board for functional mode.
7a. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
xWRL6432BOOST Low Power EVM’s
This section applies to the following boards:
Hardware Requirements for xWRL6432BOOST
- xWRL6432BOOST Antenna Module Board
- Micro USB Cable
- (For Debug ONLY) Power Supply 5V, 3A with 2.1-mm barrel jack (center positive)
Flashing Mode for xWRL6432BOOST EVM’s
1. Connect Cables
- Connect the micro-USB to the PC and to the connector on the board shown in the photo below.
- (For Debug ONLY) Connect the 5V/3A power supply to the power source and then to the board. LEDs on the board should turn on.
2. Set SOP Mode
- Enable flashing mode by setting the mux switches as seen below.
3. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
Functional Mode for xWRL6432BOOST EVM’s
1. Connect Cables
- Connect the micro-USB to the PC and to the connector on the board shown in the photo below.
- (For Debug ONLY) Connect the 5V/3A power supply to the power source and then to the board. LEDs on the board should turn on.
2. Set SOP Mode
- Enable functional mode by setting the mux switches as seen below.
3. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below.
xWRxxxxBOOST EVM’s
This section applies to the following boards:
Hardware Requirements for BOOST EVM’s
- BOOST EVM
- Micro USB Cable
- Power Supply 5V, 3A with 2.1-mm barrel jack (center positive)
Flashing Mode for BOOST EVM’s
1. Connect Cables
- Connect the micro-USB to the PC and to the connector on the board shown in the photo below.
- Connect the 5V/3A power supply to the power source and then to the board. LEDs on the board should turn on.
2. Set SOP Mode
- Enable flashing mode by setting SOP2:0 to 101 as shown below. Depending on the EVM, the board may have jumpers or switches to set the SOP Mode - refer to the image corresponding to your EVM type.
3. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below. The yellow DS4 LED below should toggle OFF and ON when the switch is depressed then released.
Functional Mode for BOOST EVM’s
1. Connect Cables
- Connect the micro-USB to the PC and to the connector on the board shown in the photo below.
- Connect the 5V/3A power supply to the power source and then to the board. LEDs on the board should turn on.
2. Set SOP Mode
- Enable flashing mode by setting SOP2:0 to 101 as shown below. Depending on the EVM, the board may have jumpers or switches to set the SOP Mode - refer to the image corresponding to your EVM type.
3. Toggle NRST
- To ensure that the correct SOP mode is latched once power has been applied, power cycle by pressing and releasing the NRST switch identified below. The yellow DS4 LED below should toggle OFF and ON when the switch is depressed then released.
Need More Help?
- Consult the mmWaveICBoost and Antenna Module User’s Guide
- Search for your issue or post a new question on the mmWave E2E forum